This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0188 [28 Nov 2017 04:40] Trisha Cabildo update |
resources:eval:user-guides:circuits-from-the-lab:cn0188 [30 Jul 2021 07:14] Victor Calinao, Jr |
||
---|---|---|---|
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] | * [[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] | ||
- | * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp://ftp.analog.com/pub/cftl/CN0188/|CN0188 Evaluation Software]] | * [[ftp://ftp.analog.com/pub/cftl/CN0188/|CN0188 Evaluation Software]] | ||
* Power Supply | * Power Supply | ||
Line 29: | Line 29: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:11-2-2017_2-20-01_pm.png?nolink&600 |}}\\ | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:11-2-2017_2-20-01_pm.png?nolink&600 |}}\\ | ||
- | * The [[http://www.analog.com/EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]] **(CN-0188 Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector | + | * The [[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]] **(CN-0188 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **J2** is the +6 V barrel connector for wall wart supply input | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
* Terminal block **J3** is the test point for 6 V DC output | * Terminal block **J3** is the test point for 6 V DC output | ||
Line 39: | Line 39: | ||
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:11-2-2017_2-30-58_pm.png?nolink&600 |}}\\ | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:11-2-2017_2-30-58_pm.png?nolink&600 |}}\\ | ||
- | - Connect the 120-pin connector on the [[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board | + | - Connect the 120-pin connector on the [[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board |
- Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | ||
- With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
Line 73: | Line 73: | ||
- **Shunt Voltage Input** - Determines input shunt voltage level in millivolts | - **Shunt Voltage Input** - Determines input shunt voltage level in millivolts | ||
- **Temperature** - Temperature level test conditions of input signal | - **Temperature** - Temperature level test conditions of input signal | ||
- | - **Data Acquisition** Controls \\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:9.png?nolink&600 |}} | + | - **Data Acquisition** Controls \\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:11.png?nolink&600 |}} |
* **Sample Data** - Start acquisition of measurement data | * **Sample Data** - Start acquisition of measurement data | ||
* **Remove Data Point** - Remove a data point from samples | * **Remove Data Point** - Remove a data point from samples | ||
* **Save Data** - Save measurement data to file | * **Save Data** - Save measurement data to file | ||
* **Clear Data** - Clear the current measurement data | * **Clear Data** - Clear the current measurement data | ||
- | - **Sample Data Graph** Tab - Shows the XY plot of ADC code and output error (%) with respect to the shunt voltage\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:9.png?nolink&600 |}} | + | - **Sample Data Graph** Tab - Shows the XY plot of ADC code and output error (%) with respect to the shunt voltage\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:12.png?nolink&600 |}} |
+ | * **ADC Code Plot** Enable - Show or hide the ADC Code plot | ||
+ | * **Error Plot** Enable - Show or hide the Error plot | ||
+ | * **Converted Shunt Voltage** - Shunt voltage value from the ADC | ||
+ | * **Over/Under Voltage** Indicator - Indicates over or under voltage conditions | ||
* **Plot Options** - Edit plot display and options like interpolation and color of output waveform | * **Plot Options** - Edit plot display and options like interpolation and color of output waveform | ||
- **Administration** Tab \\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:10.png?nolink&600 |}} | - **Administration** Tab \\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0188:10.png?nolink&600 |}} | ||
Line 86: | Line 90: | ||
\\ | \\ | ||
+ | ==== Running the System ==== | ||
+ | -Open the CN0188.exe application from the default installation location | ||
+ | -Set the correct connector and click the Connect Button | ||
+ | -Upon successful connection, set the desired input signal parameters such as shunt voltage and temperature | ||
+ | -Start and control data acquisition through the data acquisition control buttons | ||
+ | -Output data will be shown in the graph. Edit graph through plot options and check boxes provided | ||
+ | -Click Disconnect if finished | ||
+ | -Click Quit to exit the program | ||
+ | |||
+ | \\ | ||
---- | ---- | ||
Line 91: | Line 105: | ||
* [[ftp://ftp.analog.com/pub/cftl/CN0188/|CN0188 Evaluation Software]] | * [[ftp://ftp.analog.com/pub/cftl/CN0188/|CN0188 Evaluation Software]] | ||
* [[ADI>CN0188|CN0188 Circuit Note Page]] | * [[ADI>CN0188|CN0188 Circuit Note Page]] | ||
- | * [[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0188-DesignSupport.zip|CN0188 Design Support Package]] | + | * [[adi>media/en/reference-design-documentation/design-integration-files/CN0188-DesignSupport.zip|CN0188 Design Support Package]] |
* [[ADI>AD7171|AD7171 Product Page]] | * [[ADI>AD7171|AD7171 Product Page]] | ||
Line 101: | Line 115: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0188-DesignSupport.zip|EVAL-CN0188-SDPZ Design & Integration Files]] | + | [[adi>media/en/reference-design-documentation/design-integration-files/CN0188-DesignSupport.zip|EVAL-CN0188-SDPZ Design & Integration Files]] |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 107: | Line 121: | ||
* PADS project | * PADS project | ||
</WRAP> | </WRAP> | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0188-SDPZ?&v=Rev C|Register]] to receive all these great benefits and more!</WRAP> | ||
//End of Document// | //End of Document// | ||