Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Last revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0188 [04 Dec 2017 10:50]
Trisha Cabildo update
resources:eval:user-guides:circuits-from-the-lab:cn0188 [03 Jan 2021 21:55]
Robin Getz fix links
Line 15: Line 15:
 ===== Required Equipment ===== ===== Required Equipment =====
   * [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]]   * [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]]
-  * [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)+  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)
   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]
   * Power Supply   * Power Supply
Line 29: Line 29:
 ==== Block assignments ==== ==== Block assignments ====
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-20-01_pm.png?​nolink&​600 |}}\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-20-01_pm.png?​nolink&​600 |}}\\
-  * The [[http://​www.analog.com/​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]] **(CN-0188 Board)** connects to the [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector +  * The [[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]] **(CN-0188 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector 
-  * The [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.+  * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
   * Terminal block **J2** is the +6 V barrel connector for wall wart supply input   * Terminal block **J2** is the +6 V barrel connector for wall wart supply input
   * Terminal block **J3** is the test point for 6 V DC output   * Terminal block **J3** is the test point for 6 V DC output
Line 39: Line 39:
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-30-58_pm.png?​nolink&​600 |}}\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0188:​11-2-2017_2-30-58_pm.png?​nolink&​600 |}}\\
  
-  - Connect the 120-pin connector on the [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board+  - Connect the 120-pin connector on the [[adi>​EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board
   - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above   - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above
   - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board   - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board
Line 105: Line 105:
   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]   * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0188/​|CN0188 Evaluation Software]]
   * [[ADI>​CN0188|CN0188 Circuit Note Page]]   * [[ADI>​CN0188|CN0188 Circuit Note Page]]
-  * [[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|CN0188 Design Support Package]]+  * [[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|CN0188 Design Support Package]]
  
   * [[ADI>​AD7171|AD7171 Product Page]]   * [[ADI>​AD7171|AD7171 Product Page]]
Line 115: Line 115:
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|EVAL-CN0188-SDPZ Design & Integration Files]]+[[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0188-DesignSupport.zip|EVAL-CN0188-SDPZ Design & Integration Files]]
   * Schematics ​   * Schematics ​
   * PCB Layout ​   * PCB Layout ​
resources/eval/user-guides/circuits-from-the-lab/cn0188.txt · Last modified: 30 Jul 2021 07:14 by Victor Calinao, Jr