This is an old revision of the document!
CN0172 Software Evaluation User Guide
Overview
The function of the CN0172 is to provide a high accuracy multi-channel thermocouple measurement solution. Achieving a precision thermocouple measurement requires a signal chain of precision components that will amplify the small thermocouple voltage, remove noise, correct non-linearity, and provide accurate reference junction compensation. The AD7793 24-bit sigma-delta ADC is used to measure thermocouple voltages while the ADT7320 precision 16-bit digital temperature sensor is used to provide and provide reference junction compensation at ±0.25°C accuracy.
General Setup
Minimum PC/System Requirements
How to Install the Evaluation Software
-
Extract the files within the file
CN0172 SDP Eval Software.zip and open the file
setup.exe. It is recommended that you install the CN0172 SDP Evaluation Software to the default directory path
C:\Program Files\Analog Devices\CN0172\ and all National Instruments products to
C:\Program Files\National Instruments\
Press
“Next”.

Press
“Next”.

Upon completion of the installation of the
CN0172 SDP Eval Software, the installer for the
ADI SDP Drivers will execute. Follow the on-screen prompts to install the drivers. It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer. It is recommended that you install the drivers to the default directory path
C:\Program Files\Analog Devices\SDP\Drivers\
Press
“Next”
Press “Finish” to install the Drivers and complete the installation of all software necessary to evaluate the EVAL-CN0172-SDPZ
Step by Step Instruction for Connecting the Hardware
Ensure that the Breakout board and the EVAL-CN0172-SDPZ are wired up correctly. Connect the
EVAL-SDP-CB1Z and the Multi-Channel
breakout board using both 120 pin male and female connectors found on the respective boards.

Mount the SDP Board onto the breakout board.

Plug 3
K-type thermocouple wires into the thermocouple connector as shown.

Plug the mini end of the
USB cable into connector J1 of the
EVAL-SDP-CB1Z and connect the other end of the
USB cable into the Laptop or PC.
Wait for found new hardware wizard to appear and finish installation of SPD driver before opening the software.
Opening and Enabling the Evaluation Software
Launch the software which will be located in the analog devices folder in all programs.

After starting the application the user must click the “Board Setup” button. The user has the option to edit one or more of the following options:
Thermocouple type – User selects the correct thermocouple being used
Temperature Unit – Select temperature unit required
Samples/reading – changes the data acquisition rate
AD7793 Gain – Gain factor from 1 to 64 for the thermocouple output
ADT7320 Resolution – Choose between 13 or 16 bit resolution for cold junction reference
ADT7320 calibration – enables user to calibrate the ADT7320 temperature for greater accuracy
Data logging status – Enable to record temperature in location specified in save data to folder directory
Save Data in Folder – Directory for data storage
Once the Board Setup is complete the user can obtain data by clicking the
“Start Data Acquisition” button.