Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0172 [11 Oct 2012 16:41]
Brandon Bushey created
resources:eval:user-guides:circuits-from-the-lab:cn0172 [31 Dec 2020 06:37] (current)
Robin Getz fix link
Line 1: Line 1:
-====== ​CIRCUIT NOTE TITLE (CN0172======+====== CN0172 ​Software Evaluation User Guide ======
  
 ===== Overview ===== ===== Overview =====
  
-The function of the [[http://​www.analog.com/​CN0172|CN0172]] is to provide a high accuracy multi-channel thermocouple measurement solution. Achieving a precision thermocouple measurement requires a signal chain of precision components that will amplify the small thermocouple voltage, remove noise, correct non-linearity,​ and provide accurate reference junction compensation. The [[http://​www.analog.com/​AD7793|AD7793]] 24-bit sigma-delta ADC is used to measure thermocouple voltages while the [[http://​www.analog.com/​ADT7320|ADT7320]] precision 16-bit digital temperature sensor is used to provide and provide reference junction compensation at ±0.25°C accuracy. ​+The function of the [[adi>CN0172|CN0172]] is to provide a high accuracy multi-channel thermocouple measurement solution. Achieving a precision thermocouple measurement requires a signal chain of precision components that will amplify the small thermocouple voltage, remove noise, correct non-linearity,​ and provide accurate reference junction compensation. The [[adi>AD7793|AD7793]] 24-bit sigma-delta ADC is used to measure thermocouple voltages while the [[adi>ADT7320|ADT7320]] precision 16-bit digital temperature sensor is used to provide and provide reference junction compensation at ±0.25°C accuracy. ​
  
 ===== General Setup ===== ===== General Setup =====
  
-  * 1x [[http://​www.analog.com/​EVAL-CN0172-SDPZ|EVAL-CN0172-SDPZ]] Circuit Evaluation board +  * 1x [[adi>EVAL-CN0172-SDPZ|EVAL-CN0172-SDPZ]] Circuit Evaluation board 
-  * 1x [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller board+  * 1x [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller board
   * 1x SDP Breakout Board   * 1x SDP Breakout Board
   * 3x K-type thermocouples   * 3x K-type thermocouples
Line 14: Line 14:
   * 1 USB Type-A plug to USB Mini-B plug cable   * 1 USB Type-A plug to USB Mini-B plug cable
   * 1x PC running Windows XP or higher   * 1x PC running Windows XP or higher
- 
- 
-{{ Circuit Set-up Block Diagram |}} 
  
 ===== Minimum PC/System Requirements ===== ===== Minimum PC/System Requirements =====
Line 29: Line 26:
  
   - Download [[ftp://​ftp.analog.com/​pub/​cftl/​CN0172|CN0172 Evaluation Software]]. ​ Do not plug in the SDP until the drivers have been installed   - Download [[ftp://​ftp.analog.com/​pub/​cftl/​CN0172|CN0172 Evaluation Software]]. ​ Do not plug in the SDP until the drivers have been installed
-  - Extract the files within the file **CN0172 SDP Eval Software.zip** and open the file **setup.exe**. ​ It is recommended that you install the CN0172 SDP Evaluation Software to the default directory path **C:​\Program Files\Analog Devices\CN0172\** and all National Instruments products to **C:​\Program Files\National Instruments\**{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_evaluation_software_driver_install.jpg?​300 |}} +  - Extract the files within the file **CN0172 SDP Eval Software.zip** and open the file **setup.exe**. ​ It is recommended that you install the CN0172 SDP Evaluation Software to the default directory path **C:​\Program Files\Analog Devices\CN0172\** and all National Instruments products to **C:​\Program Files\National Instruments\**{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_evaluation_software_driver_install.jpg?​300 |}} 
-  - Press **“Next”**.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_evaluation_software_driver_install1.jpg?​300 |}} +  - Press **“Next”**.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_evaluation_software_driver_install1.jpg?​300 |}} 
-  - Press **“Next”**.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_evaluation_software_driver_install_complete.jpg?​300 |}} +  - Press **“Next”**.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_evaluation_software_driver_install_complete.jpg?​300 |}} 
-  - Upon completion of the installation of the **CN0172 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. ​ Follow the on-screen prompts to install the drivers. ​ It is recommended that you close all other applications before clicking “Next”. ​ This will make it possible to update relevant system files without having to reboot your computer. ​ It is recommended that you install the drivers to the default directory path **C:​\Program Files\Analog Devices\SDP\Drivers\**{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_sdp_driver_install.jpg?​300 |}} +  - Upon completion of the installation of the **CN0172 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. ​ Follow the on-screen prompts to install the drivers. ​ It is recommended that you close all other applications before clicking “Next”. ​ This will make it possible to update relevant system files without having to reboot your computer. ​ It is recommended that you install the drivers to the default directory path **C:​\Program Files\Analog Devices\SDP\Drivers\**{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_sdp_driver_install.jpg?​300 |}} 
-  - Press **“Next”**{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_sdp_driver_install_complete.jpg?​300 |}}+  - Press **“Next”**{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_sdp_driver_install_complete.jpg?​300 |}}
   - Press **“Finish”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0172-SDPZ**   - Press **“Finish”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0172-SDPZ**
- 
 ===== Step by Step Instruction for Connecting the Hardware ===== ===== Step by Step Instruction for Connecting the Hardware =====
  
-  - Ensure that the Breakout board and the EVAL-CN0172-SDPZ are wired up correctly. Connect the **EVAL-SDP-CB1Z** and the Multi-Channel **breakout board** using both 120 pin male and female connectors found on the respective boards.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_hardware_board_connection.jpg?​ |}} +  - Ensure that the Breakout board and the EVAL-CN0172-SDPZ are wired up correctly. Connect the **EVAL-SDP-CB1Z** and the Multi-Channel **breakout board** using both 120 pin male and female connectors found on the respective boards.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_hardware_board_connection.jpg?​ |}} 
-  - Mount the SDP Board onto the breakout board.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_hardware_board_connection1.jpg?​ |}} +  - Mount the SDP Board onto the breakout board.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_hardware_board_connection1.jpg?​ |}} 
-  - Plug 3 K-type thermocouple wires into the thermocouple connector as shown.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_hardware_board_connection2.jpg?​ |}}+  - Plug 3 K-type thermocouple wires into the thermocouple connector as shown.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_hardware_board_connection2.jpg?​ |}}
   - Plug the mini end of the USB cable into connector J1 of the **EVAL-SDP-CB1Z** and connect the other end of the USB cable into the Laptop or PC.   - Plug the mini end of the USB cable into connector J1 of the **EVAL-SDP-CB1Z** and connect the other end of the USB cable into the Laptop or PC.
   - Wait for found new hardware wizard to appear and finish installation of SPD driver before opening the software.   - Wait for found new hardware wizard to appear and finish installation of SPD driver before opening the software.
- 
 ===== Opening and Enabling the Evaluation Software ===== ===== Opening and Enabling the Evaluation Software =====
  
-  - Launch the software which will be located in the analog devices folder in all programs.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_evaluation_software_user_interface.jpg?​300 |}}+  - Launch the software which will be located in the analog devices folder in all programs.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_evaluation_software_user_interface.jpg?​300 |}}
   - After starting the application the user must click the **“Board Setup”** button. The user has the option to edit one or more of the following options:   - After starting the application the user must click the **“Board Setup”** button. The user has the option to edit one or more of the following options:
     - **Thermocouple type** – User selects the correct thermocouple being used     - **Thermocouple type** – User selects the correct thermocouple being used
Line 56: Line 51:
     - **Data logging status** – Enable to record temperature in location specified in save data to folder directory     - **Data logging status** – Enable to record temperature in location specified in save data to folder directory
     - **Save Data in Folder** – Directory for data storage     - **Save Data in Folder** – Directory for data storage
-  - Once the Board Setup is complete the user can obtain data by clicking the **“Start Data Acquisition”** button.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0172_evaluation_software_user_interface1.jpg?​300 |}} +  - Once the Board Setup is complete the user can obtain data by clicking the **“Start Data Acquisition”** button.{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0172:​cn0172_evaluation_software_user_interface1.jpg?​300 |}}
resources/eval/user-guides/circuits-from-the-lab/cn0172.1349966494.txt.gz · Last modified: 11 Oct 2012 16:41 by Brandon Bushey