resources:eval:user-guides:circuits-from-the-lab:cn0172 [29 Nov 2012 18:31]
James Fitzgerald [Opening and Enabling the Evaluation Software]
resources:eval:user-guides:circuits-from-the-lab:cn0172 [31 Dec 2020 06:37]
Robin Getz fix link
Line 1: Line 1:
-====== ​CIRCUIT NOTE TITLE (CN0172======+====== CN0172 ​Software Evaluation User Guide ======
  
 ===== Overview ===== ===== Overview =====
  
-The function of the [[http://​www.analog.com/​CN0172|CN0172]] is to provide a high accuracy multi-channel thermocouple measurement solution. Achieving a precision thermocouple measurement requires a signal chain of precision components that will amplify the small thermocouple voltage, remove noise, correct non-linearity,​ and provide accurate reference junction compensation. The [[http://​www.analog.com/​AD7793|AD7793]] 24-bit sigma-delta ADC is used to measure thermocouple voltages while the [[http://​www.analog.com/​ADT7320|ADT7320]] precision 16-bit digital temperature sensor is used to provide and provide reference junction compensation at ±0.25°C accuracy. ​+The function of the [[adi>CN0172|CN0172]] is to provide a high accuracy multi-channel thermocouple measurement solution. Achieving a precision thermocouple measurement requires a signal chain of precision components that will amplify the small thermocouple voltage, remove noise, correct non-linearity,​ and provide accurate reference junction compensation. The [[adi>AD7793|AD7793]] 24-bit sigma-delta ADC is used to measure thermocouple voltages while the [[adi>ADT7320|ADT7320]] precision 16-bit digital temperature sensor is used to provide and provide reference junction compensation at ±0.25°C accuracy. ​
  
 ===== General Setup ===== ===== General Setup =====
  
-  * 1x [[http://​www.analog.com/​EVAL-CN0172-SDPZ|EVAL-CN0172-SDPZ]] Circuit Evaluation board +  * 1x [[adi>EVAL-CN0172-SDPZ|EVAL-CN0172-SDPZ]] Circuit Evaluation board 
-  * 1x [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller board+  * 1x [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller board
   * 1x SDP Breakout Board   * 1x SDP Breakout Board
   * 3x K-type thermocouples   * 3x K-type thermocouples
resources/eval/user-guides/circuits-from-the-lab/cn0172.txt · Last modified: 31 Dec 2020 06:37 by Robin Getz