This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0150 [25 Oct 2017 04:05] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0150 [30 Jul 2021 07:10] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 5: | Line 5: | ||
The [[ADI> | The [[ADI> | ||
- | The [[ADI> | + | The [[ADI> |
The EVAL-CN0150-SDPZ board connects to ADI’s System Demonstration Platform (SDP) and is powered by a +6 V supply or +6 V “wall wart”. | The EVAL-CN0150-SDPZ board connects to ADI’s System Demonstration Platform (SDP) and is powered by a +6 V supply or +6 V “wall wart”. | ||
Line 13: | Line 13: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Power Supply | * Power Supply | ||
Line 20: | Line 20: | ||
* Windows 7 (32-bit), Windows Vista (32-bit) or Windows XP | * Windows 7 (32-bit), Windows Vista (32-bit) or Windows XP | ||
* USB interface | * USB interface | ||
- | * RF signal source | + | * RF signal source |
- | * //Rohde & Schwarz SMT-03 RF signal source// | + | |
* Coaxial RF cable with SMA connectors | * Coaxial RF cable with SMA connectors | ||
Line 27: | Line 26: | ||
===== General Setup ===== | ===== General Setup ===== | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
- | {{ : | + | {{ : |
- | * The [[http:// | + | * The [[adi>EVAL-CN0150-SDPZ|EVAL-CN0150-SDPZ]] **(CN-0150 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
- | * Terminal block **J2** is the +6 V power supply input | + | * Terminal block **J1** is the +6 V power supply |
+ | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
* Terminal block **J3** is the SMA connector for RF input | * Terminal block **J3** is the SMA connector for RF input | ||
\\ | \\ | ||
+ | ==== Test setup ==== | ||
+ | {{ : | ||
+ | - Connect the 120-pin connector on the [[adi> | ||
+ | - Connect the RF signal source to the [[adi> | ||
+ | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
+ | *//If available, a +6 V "wall wart" can be connected to the barrel connector on the board and used in place of the +6 V power supply// | ||
+ | - Connect the USB cable supplied with the SDP board to the USB port on the PC | ||
+ | - Apply power to the +6 V supply (or “wall wart”) connected to [[adi> | ||
+ | - Launch the evaluation software | ||
+ | - Connect the USB cable from the PC to the USB mini connector on the SDP board | ||
+ | \\ | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
Do **not** connect the USB cable to the Mini-USB connector on the SDP board before turning on the dc power supply for the **EVAL-CN0150-SDPZ**. | Do **not** connect the USB cable to the Mini-USB connector on the SDP board before turning on the dc power supply for the **EVAL-CN0150-SDPZ**. | ||
</ | </ | ||
+ | \\ | ||
+ | ==== Calibration ==== | ||
+ | Because the slope and intercept of the system vary from device to device, a system level calibration is **required**. | ||
+ | - Apply two known signal levels PIN_1 and PIN_2 close to the endpoints of the AD8318 linear input range. Note that it should be well within the linear operating range of the device (**-50 dBm to -10 dBm for this device**){{ : | ||
+ | - Measure the corresponding output codes CODE_1 and CODE_2 from the ADC | ||
+ | - Calculate SLOPE_ADC and INTERCEPT using the following equations: | ||
+ | * **SLOPE_ADC** = (CODE_2 - CODE_1)/ | ||
+ | * **INTERCEPT** = PIN_2 - (CODE_2/ | ||
+ | - These will be used to calculate the unknown input power level, PIN, when operation in the field using the equation | ||
+ | * **PIN** = (CODE_OUT/ | ||
+ | \\ | ||
---- | ---- | ||
+ | |||
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== | ||
- Extract the file **CN0150_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | - Extract the file **CN0150_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | ||
Line 51: | Line 74: | ||
---- | ---- | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
- | ====Test Setup Tab==== | + | ==== Main Window |
- | {{ : | + | {{ : |
- | | + | - **Connect** Button - Starts the connection between the [[ADI> |
+ | - **Reset and Disconnect** Button - Resets and ends the connection between the [[ADI> | ||
+ | - **Sample Data Graph** Tab - Shows the XY plot of ADC code and output error (%) versus input signal power. Also contains the plot options where you can edit plot display and options like interpolation and color of output waveform | ||
+ | - **Test Setup** Tab \\ {{ : | ||
+ | * **Data Acquisition** | ||
+ | * **Input Power** - Indicate input signal power level | ||
+ | * **Frequency** - Indicate input signal frequency | ||
+ | * **Temperature** - Temperature test level condition of the input signal | ||
+ | * **Acquire Data** - Start acquisition of measurement data | ||
+ | * **Clear Data** - Clear the current measurement data | ||
+ | * **Save Data to File** - Save measurement data to file | ||
+ | * **Increment Amount** - Increment value of input power level | ||
+ | * **Average Value** - Read only. ADC conversion value | ||
+ | * **Sample size** - Edit value to desired sampling size for ADC | ||
+ | * **Remove Last** - Remove last reading from the graph | ||
+ | * **Auto-increment** - Enable auto increment of input power level | ||
+ | * **Calibration** - insert calibration instructions here | ||
+ | * **PIN_1** - First known input power level close to endpoints of AD8318 linear input range | ||
+ | * **PIN_2** - Second known input power level close to endpoints of AD8318 linear input range | ||
+ | * **Slope (ADC Code/ dBm)** - Slope of the transfer curve of AD8318 (-24 mV/dB nominal) | ||
+ | * **Intercept (ADC Code)** - X-axis intercept with a unit of dBm | ||
+ | | ||
+ | * **SDP Connector** - Selects which 120-pin connection of the SDP-B Board to use | ||
+ | * **SCLK Frequency** - Sets the SPI clock frequency for the data transfers used by the evaluation board | ||
+ | * **AD7887 Voltage Reference** - Select between internal or external 2.5 volts voltage reference | ||
+ | * **SPI Byte to Write** - Buffer of unsigned 16-bit elements for SPI write transfer | ||
+ | * **Flash LED** - Flashes the LED on the SDP controller board | ||
+ | * **Read Firmware** - Reads the firmware of CN0150 Evaluation Board | ||
\\ | \\ | ||
+ | |||
+ | ==== Running the System ==== | ||
+ | -Open the CN0150.exe application from the default installation location | ||
+ | -Set the correct connector and click the Connect Button | ||
+ | -Upon successful connection, calibrate the device in the Test Setup tab | ||
+ | -After proper calibration, | ||
+ | -Start acquisition of measurement data through Acquire Data button | ||
+ | -To manipulate the data, other measurement data control buttons are available such as Clear Data and Save Data to file | ||
+ | -Click Reset and Disconnect if finished | ||
+ | \\ | ||
---- | ---- | ||
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== | ||
* [[ftp:// | * [[ftp:// | ||
- | * [[ADI> | + | * [[adi> |
- | * [[http:// | + | * [[adi> |
- | * [[ADI> | + | * [[adi> |
- | * [[ADI> | + | * [[adi> |
- | * [[ADI> | + | * [[adi> |
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 75: | Line 135: | ||
* PADS project | * PADS project | ||
</ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
//End of Document// | //End of Document// | ||