This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0150 [05 Dec 2017 04:39] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0150 [31 Dec 2020 06:36] – fix links Robin Getz | ||
---|---|---|---|
Line 13: | Line 13: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Power Supply | * Power Supply | ||
Line 27: | Line 27: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0150-SDPZ|EVAL-CN0150-SDPZ]] **(CN-0150 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **J1** is the +6 V power supply | * Terminal block **J1** is the +6 V power supply | ||
* Terminal block **J2** is the +6 V barrel connector for wall wart supply input | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
Line 36: | Line 36: | ||
==== Test setup ==== | ==== Test setup ==== | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[adi> | + | - Connect the 120-pin connector on the [[adi> |
- Connect the RF signal source to the [[adi> | - Connect the RF signal source to the [[adi> | ||
- With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
Line 120: | Line 120: | ||
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== | ||
* [[ftp:// | * [[ftp:// | ||
- | * [[ADI> | + | * [[adi> |
- | * [[http:// | + | * [[adi> |
- | * [[ADI> | + | * [[adi> |
- | * [[ADI> | + | * [[adi> |
- | * [[ADI> | + | * [[adi> |
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout |