Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:circuits-from-the-lab:cn-0583:start [15 Feb 2024 17:58] – Add programming the SOM section Ciprian Regusresources:eval:user-guides:circuits-from-the-lab:cn-0583:start [15 Feb 2024 17:59] (current) – . Ciprian Regus
Line 233: Line 233:
   - Download the {{ :resources:eval:user-guides:circuits-from-the-lab:cn0583:cn0583_firmware.zip | CN0583 Demo Hex File}} for the demo application. Alternatively, you may use you own hex file.   - Download the {{ :resources:eval:user-guides:circuits-from-the-lab:cn0583:cn0583_firmware.zip | CN0583 Demo Hex File}} for the demo application. Alternatively, you may use you own hex file.
   - Connect the EVAL-CN0583-CRR1 carrier board to your PC using an USB cable.   - Connect the EVAL-CN0583-CRR1 carrier board to your PC using an USB cable.
-  - Wait for the DAPLINK directory to appear.+  - Wait for the DAPLINK directory to appear on your PC's filesystem.
   - Copy the hex file to the DAPLINK directory.   - Copy the hex file to the DAPLINK directory.
   - The hex file will now be written in the MAX32660's flash memory (this should take a few seconds). After that, the DAPLINK directory will be deleted.   - The hex file will now be written in the MAX32660's flash memory (this should take a few seconds). After that, the DAPLINK directory will be deleted.
resources/eval/user-guides/circuits-from-the-lab/cn-0583/start.txt · Last modified: 15 Feb 2024 17:59 by Ciprian Regus