This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:adf7242-pmod [01 Apr 2015 11:49] – Paul Cercueil | resources:eval:user-guides:circuits-from-the-lab:adf7242-pmod [01 Apr 2015 14:34] – [2.4GHz Wireless Transceiver PMOD] Walt Kester | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== 2.4GHz Wireless Transceiver PMOD ====== | ||
+ | ====== 2.4GHz Wireless Transceiver PMOD ====== | ||
+ | [[ADI> | ||
===== Product Details ===== | ===== Product Details ===== | ||
- | The low cost and small profile RF solution 2.4GHz, 802.15.4/ | + | The low cost and small profile RF solution 2.4GHz, 802.15.4/ |
The Wireless Transceiver PMOD board uses mini 2.4Ghz Chip Antennas. In conjunction with the impedance-matched (complex differential impedance value) filter balun, reduces the RF front end count. This PMOD board supports polarization diversity that uses two chip antennas which can greatly improve performance under multipath fading conditions. | The Wireless Transceiver PMOD board uses mini 2.4Ghz Chip Antennas. In conjunction with the impedance-matched (complex differential impedance value) filter balun, reduces the RF front end count. This PMOD board supports polarization diversity that uses two chip antennas which can greatly improve performance under multipath fading conditions. |