Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:arduino-uno:reference_designs:demo_cn0429 [07 Jan 2019 15:04] – [Obtaining the Source Code] Andrei Drimbareanresources:eval:user-guides:arduino-uno:reference_designs:demo_cn0429 [03 Jan 2021 22:04] (current) – fix links Robin Getz
Line 28: Line 28:
   * Hardware   * Hardware
     * Arduino Uno     * Arduino Uno
-    * [[https://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/CN0429.html|EVAL-CN0429-EBZ Gas Sensor Daughter Board loaded with firmware.]] (up to 4) +    * [[adi>en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/CN0429.html|EVAL-CN0429-EBZ Gas Sensor Daughter Board loaded with firmware.]] (up to 4) 
-    * [[https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-M355-ARDZ-INT.html|EVAL-M355-ARDZ-INT Arduino-compatible platform.]]+    * [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-M355-ARDZ-INT.html|EVAL-M355-ARDZ-INT Arduino-compatible platform.]]
     * Type B to Type A USB cable     * Type B to Type A USB cable
     * PC or Laptop with a USB port     * PC or Laptop with a USB port
Line 40: Line 40:
 ===== Setting up the Hardware ===== ===== Setting up the Hardware =====
  
-  - Plug in the **EVAL-CN0429-EBZ** ([[https://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/CN0429.html|CN0429]] Shield board) to the [[https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-M355-ARDZ-INT.html|EVAL-M355-ARDZ-INT]] interposer board+  - Plug in the **EVAL-CN0429-EBZ** ([[adi>en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/CN0429.html|CN0429]] Shield board) to the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-M355-ARDZ-INT.html|EVAL-M355-ARDZ-INT]] interposer board
   - Connect the system to the Arduino connectors DIGITAL (PWM~), POWER, ANALOG IN and ICSP of the Arduino Uno board.   - Connect the system to the Arduino connectors DIGITAL (PWM~), POWER, ANALOG IN and ICSP of the Arduino Uno board.
     * Note, the boards should only plug together one way, preventing reverse connections.     * Note, the boards should only plug together one way, preventing reverse connections.
   - Connect the system to the PC using USB cable   - Connect the system to the PC using USB cable
-  - Connect the sensors to the dedicated connectors on the **EVAL-CN0429-EBZ**. The [[https://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/CN0429.html|CN0429]] is compatible with electrochemical gas sensors in “4-series” form factor. 2-, 3- and 4-electrode sensors are supported. See the drawing below for form factor dimensions. +  - Connect the sensors to the dedicated connectors on the **EVAL-CN0429-EBZ**. The [[adi>en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/CN0429.html|CN0429]] is compatible with electrochemical gas sensors in “4-series” form factor. 2-, 3- and 4-electrode sensors are supported. See the drawing below for form factor dimensions. 
  
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0429:cn0429_gas_sensor_dimensions.png?600 |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0429:cn0429_gas_sensor_dimensions.png?600 |}}
resources/eval/user-guides/arduino-uno/reference_designs/demo_cn0429.txt · Last modified: 03 Jan 2021 22:04 by Robin Getz