This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:arduino-uno:reference_designs:demo_adxl372 [18 Jan 2018 09:52] – [Setting up the Hardware] Mircea Caprioru | resources:eval:user-guides:arduino-uno:reference_designs:demo_adxl372 [22 Jan 2018 08:46] – [Project Structure] Mircea Caprioru | ||
---|---|---|---|
Line 9: | Line 9: | ||
The **ADXL372** is an ultralow power, 3-axis, **±200 g** MEMS accelerometer. | The **ADXL372** is an ultralow power, 3-axis, **±200 g** MEMS accelerometer. | ||
+ | <note important> | ||
===== Demo Requirements ===== | ===== Demo Requirements ===== | ||
Line 43: | Line 44: | ||
===== Project Structure===== | ===== Project Structure===== | ||
- | {{ : | + | {{ : |
The Arduino Sketch is used to load the example into Arduino IDE. The project is composed of three main parts: | The Arduino Sketch is used to load the example into Arduino IDE. The project is composed of three main parts: |