Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:adum770x [04 Apr 2019 17:04]
Istvan Csomortani [Overview] Applications should be a title
resources:eval:user-guides:adum770x [22 Jul 2021 17:51] (current)
Elliott Potter Corrected link to sinc filter on github
Line 32: Line 32:
 User can configure the corresponding interface type, by setting the **adc_port_type** Tcl variable in the system_project.tcl file. Note that this variable should be set before generating any bit file.  User can configure the corresponding interface type, by setting the **adc_port_type** Tcl variable in the system_project.tcl file. Note that this variable should be set before generating any bit file. 
  
-The output of the device is a continuous digital bit stream, to reconstruct the original input signal information,​ this output bit stream needs to be digitally filtered and decimated. A simple {{https://​github.com/​analogdevicesinc/​hdl/​blob/​adum7701/​library/​common/​util_dec256sinc24b.v|sinc filter}} is recommended to reconstruct the original input signal information received from the ADuM7701. The following equation describes the transfer function of the sinc filter: ​+The output of the device is a continuous digital bit stream, to reconstruct the original input signal information,​ this output bit stream needs to be digitally filtered and decimated. A simple {{https://​github.com/​analogdevicesinc/​hdl/​blob/​master/​library/​common/​util_dec256sinc24b.v|sinc filter}} is recommended to reconstruct the original input signal information received from the ADuM7701. The following equation describes the transfer function of the sinc filter: ​
  
 <​m>​H(z) = (1/DR (1-Z^-DR)/​(1 - Z^-1))^N</​m>​ <​m>​H(z) = (1/DR (1-Z^-DR)/​(1 - Z^-1))^N</​m>​
resources/eval/user-guides/adum770x.txt · Last modified: 22 Jul 2021 17:51 by Elliott Potter