Wiki

This version (01 Mar 2023 13:55) was approved by Paul Pop.The Previously approved version (16 Dec 2021 15:19) is available.Diff

ADRV9371x Arria 10 GX Quick Start Guide

arria10-fpga_adrv9371.jpg

NOTE:
Support for the A10GX carrier is discontinued and will not be supported in future releases. Last pre-build images can be found at Nios2 Linux on the Altera FPGA Development Boards page.

This guide provides some quick instructions on how to setup the ADRV9371x on A10GX

Prerequisites

Required Hardware

Required Software

  • You need a Host PC (Windows)
  • Intel Quartus 21.2
  • Bitfile and Linux ELF image
  • IIO Scope Download

Setting up the hardware (A10GX)

You will need to: arria10-fpga-kit.jpg

  1. Get the A10GX board.
  2. Connect the ADRV9371x FMC board to the FPGA carrier FMC1 socket(J1).
  3. Connect the USB JTAG J3 (Micro USB) to your Host PC.
  4. Connect the Ethernet cable.
  5. Plug the Power Supply into 12V Power input connector (DC Input).
  6. Turn it on.

All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.

Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.

Programming the FPGA

Nios II Command Shell is used to program the FPGA. To run Nios II Command Shell navigate to C:\intelFPGA_pro\21.2\nios2eds and start Nios II Command Shell.bat. Windows Subsystem for Linux (WSL) needs to be installed in order to run Nios II Command Shell.

After starting the Command Shell, navigate to the path where the pre-build images are saved. For example:

ceshu@LADACE-L02:/mnt/c/intelFPGA_pro/21.2/nios2eds$ cd /mnt/c/Users/ladace/Downloads/adrv9371x_a10gx

Programming FPGA bitfiled image

To flash the bitfield pre-build image, nios2-configure-sof command is used. For example:

ceshu@LADACE-L02:/mnt/c/Users/ladace/Downloads/adrv9371x_a10gx$ nios2-configure-sof adrv9371x_a10gx.sof
Searching for SOF file:
in .
  adrv9371x_a10gx.sof

Info: *******************************************************************
Info: Running Quartus Prime Programmer
Info: Command: quartus_pgm --no_banner --mode=jtag -o p;./adrv9371x_a10gx.sof
Info (213045): Using programming cable "USB-BlasterII [USB-1]"
Info (213011): Using programming file ./adrv9371x_a10gx.sof with checksum 0x30E16FA7 for device 10AX115S2F45@1
Info (209060): Started Programmer operation at Thu Dec 16 11:14:04 2021
Info (209016): Configuring device index 1
Info (209017): Device 1 contains JTAG ID code 0x02E060DD
Info (209007): Configuration succeeded -- 1 device(s) configured
Info (209011): Successfully performed operation(s)
Info (209061): Ended Programmer operation at Thu Dec 16 11:14:19 2021
Info: Quartus Prime Programmer was successful. 0 errors, 0 warnings
    Info: Peak virtual memory: 1778 megabytes
    Info: Processing ended: Thu Dec 16 11:14:19 2021
    Info: Elapsed time: 00:00:24
    Info: System process ID: 8172

Programming Linux image

To flash the Linux pre-build image, nios2-download command is used. For example:

ceshu@LADACE-L02:/mnt/c/Users/ladace/Downloads/adrv9371x_a10gx$ nios2-download -g zImage
Using cable "USB-BlasterII [USB-1]", device 1, instance 0x00
Pausing target processor: OK
Initializing CPU cache (if present)
OK
Downloaded 5468KB in 6.0s (911.3KB/s)
Verified OK
Starting processor at address 0xC4000000

Nios II Terminal

To start the Nios II Terminal use the following nios2-terminal.exe command. Example of console:

Complete kernel boot log (Click to expand)

Complete kernel boot log (Click to expand)

ceshu@LADACE-L02:/mnt/c/Users/ladace/Downloads/adrv9371x_a10gx$ nios2-terminal.exe
nios2-terminal: connected to hardware target using JTAG UART on cable
nios2-terminal: "USB-BlasterII [USB-1]", device 1, instance 0
nios2-terminal: (Use the IDE stop button or Ctrl-C to terminate)

Linux version 4.9.0-04235-g4db1e6cb5208 (sandu@saturn) (gcc versiLinux version 4.19.0-g17f4223 (jenkins@romlxbuild1.adlk
.analog.com) (gcc version 8.3.1 20190416 (Altera 19.3 Build 222)) #1875 Tue Jul 27 14:46:07 IST 2021
On node 0 totalpages: 65536
  Normal zone: 512 pages used for memmap
  Normal zone: 0 pages reserved
  Normal zone: 65536 pages, LIFO batch:15
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists, mobility grouping on.  Total pages: 65024
Kernel command line: debug console=ttyJ0,115200
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Sorting __ex_table...
Memory: 247920K/262144K available (3795K kernel code, 469K rwdata, 4372K rodata, 3160K init, 106K bss, 14224K reserved,
0K cma-reserved)
NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
clocksource: nios2-clksrc: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns
Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
devtmpfs: initialized
random: get_random_u32 called from bucket_table_alloc.isra.6+0x98/0x1e8 with crng_init=0
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
futex hash table entries: 256 (order: -1, 3072 bytes)
NET: Registered protocol family 16
jesd204: found 0 devices and 0 topologies
clocksource: Switched to clocksource nios2-clksrc
NET: Registered protocol family 2
tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
random: fast init done
workingset: timestamp_bits=30 max_order=16 bucket_order=0
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
101814f0.serial: ttyJ0 at MMIO 0x101814f0 (irq = 2, base_baud = 0) is a Altera JTAG UART
console [ttyJ0] enabled
loop: module loaded
spi_altera 10181400.spi: base (ptrval), irq 8
libphy: Fixed MDIO Bus: probed
libphy: altera_tse: probed
altera_tse 10181000.ethernet (unnamed net_device) (uninitialized): MDIO bus altera_tse-0: created
altera_tse 10181000.ethernet: Altera TSE MAC version 19.3 at 0x10181000 irq 1/3
ad9371 spi0.1: ad9371_probe : enter
altera-a10-fpll 10045000.altera-a10-fpll: FPLL PLL calibration OK (1400 us)
altera-a10-fpll 10035000.altera-a10-fpll: FPLL PLL calibration OK (1400 us)
altera-a10-fpll 10025000.altera-a10-fpll: FPLL PLL calibration OK (1400 us)
altera_adxcvr 10024000.axi-ad9371-tx-xcvr: ATX PLL calibration OK (20 ms)
altera_adxcvr 10024000.axi-ad9371-tx-xcvr: Lane 0 TX termination and VOD calibration OK (400 us)
altera_adxcvr 10024000.axi-ad9371-tx-xcvr: Lane 1 TX termination and VOD calibration OK (400 us)
altera_adxcvr 10024000.axi-ad9371-tx-xcvr: Lane 2 TX termination and VOD calibration OK (500 us)
altera_adxcvr 10024000.axi-ad9371-tx-xcvr: Lane 3 TX termination and VOD calibration OK (500 us)
altera_adxcvr 10024000.axi-ad9371-tx-xcvr: Altera ADXCVR (17.01.a) probed
altera_adxcvr 10034000.axi-ad9371-rx-xcvr: Lane 0 CDR/CMU PLL & RX offset calibration OK (400 us)
altera_adxcvr 10034000.axi-ad9371-rx-xcvr: Lane 1 CDR/CMU PLL & RX offset calibration OK (500 us)
altera_adxcvr 10034000.axi-ad9371-rx-xcvr: Altera ADXCVR (17.01.a) probed
altera_adxcvr 10044000.axi-ad9371-rx-os-xcvr: Lane 0 CDR/CMU PLL & RX offset calibration OK (600 us)
altera_adxcvr 10044000.axi-ad9371-rx-os-xcvr: Lane 1 CDR/CMU PLL & RX offset calibration OK (500 us)
altera_adxcvr 10044000.axi-ad9371-rx-os-xcvr: Altera ADXCVR (17.01.a) probed
NET: Registered protocol family 17
altera_adxcvr 10024000.axi-ad9371-tx-xcvr: Setting link rate to 122880000 (lane rate: 4915200)
altera_adxcvr 10034000.axi-ad9371-rx-xcvr: Setting link rate to 122880000 (lane rate: 4915200)
altera_adxcvr 10044000.axi-ad9371-rx-os-xcvr: Setting link rate to 122880000 (lane rate: 4915200)
ad9371 spi0.1: ad9371_probe : enter
ad9371 spi0.1: ad9371_probe : enter
random: crng init done
ad9371 spi0.1: framerStatus (0x20)
ad9371 spi0.1: AD9371 Rev 3, Firmware 5.2.2 API version: 1.5.2.3566 successfully initialized
cf_axi_dds 10054000.axi-ad9371-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x10054000 mapped to 0x03281b71,
 probed DDS AD9371
cf_axi_adc 10050000.axi-ad9371-rx-hpc: ADI AIM (10.01.b) at 0x10050000 mapped to 0x78806569, probed ADC AD9371 as MASTER
Freeing unused kernel memory: 3160K
This architecture does not have kernel memory protection.
Run /init as init process
Starting logging: OK
Initializing random number generator... done.
Starting network: OK
altera_tse 10181000.ethernet eth0: device MAC address b2:94:3d:6e:11:8f
altera_tse 10181000.ethernet eth0: TSE revision 1303
altera_tse 10181000.ethernet eth0: PCS PHY ID: 0x00000000
altera_tse 10181000.ethernet eth0: SGMII PCS block initialised OK
altera_tse 10181000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
Network cable is plugged
udhcpc: started, v1.25.0
udhcpc: sending discover
udhcpc: sending select for 10.48.65.123
udhcpc: lease of 10.48.65.123 obtained, lease time 21600
deleting routers
adding dns 10.32.51.110
adding dns 10.64.53.110
          inet addr:10.48.65.123  Bcast:10.48.65.255  Mask:255.255.255.0
Starting dropbear sshd: OK
Starting IIO Server Daemon

Welcome to Buildroot
buildroot login:

IIO Oscilloscope

To connect the board to IIO Scope start the IIO Oscilloscope application and go to Settings menu and then press Connect. From Select or Discover libIIO Context select Manual and enter the URI in the following format ip:<your_board_ip> Press the Refresh button and then Connect.

To determine the IP of the board, in Nios II Command Shell login using root and password analog. Then run the ifconfig command. For example:

# ifconfig
eth0      Link encap:Ethernet  HWaddr B2:94:3D:6E:11:8F
          inet addr:10.48.65.123  Bcast:10.48.65.255  Mask:255.255.255.0
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:17056 errors:0 dropped:1586 overruns:0 frame:0
          TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:3509856 (3.3 MiB)  TX bytes:684 (684.0 B)
          Memory:10181000-101813ff

lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

#

iioscope_connect.jpg

To plot the captured waveforms go to File menu then click New Plot. Select the channels to plot and then click Capture / Stop button.

iioscope_newplot.jpg

More Information

Support

Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.

resources/eval/user-guides/adrv9371x/quickstart/a10gx.txt · Last modified: 01 Mar 2023 10:26 by Paul Pop