Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

resources:eval:user-guides:adrv936x_rfsom:tutorials:loopback_delay_estimation [12 Feb 2020 16:30]
Srikanth Pagadarai created
resources:eval:user-guides:adrv936x_rfsom:tutorials:loopback_delay_estimation [14 Jan 2021 05:12]
Robin Getz user interwiki links
Line 5: Line 5:
 Requirements:​ Requirements:​
   - MATLAB, Simulink, HDL Coder   - MATLAB, Simulink, HDL Coder
-  - [[https://​www.mathworks.com/​help/​supportpkg/​xilinxzynqbasedradio/​index.html|Communications Toolbox Support Package for Xilinx Zynq-Based Radio]] ​+  - [[mw>help/​supportpkg/​xilinxzynqbasedradio/​index.html|Communications Toolbox Support Package for Xilinx Zynq-Based Radio]] ​
   - Xilinx Vivado (Tested 2018.2)   - Xilinx Vivado (Tested 2018.2)
-  - [[https://​wiki.analog.com/​resources/​eval/​user-guides/​adrv936x_rfsom|ADI AD9361 System on Module (SOM) SDR]] +  - [[/​resources/​eval/​user-guides/​adrv936x_rfsom|ADI AD9361 System on Module (SOM) SDR]] 
   - A loopback cable with UFL female ports on both ends   - A loopback cable with UFL female ports on both ends
  
 To build and run the demo: To build and run the demo:
-  - Create a MathWorks HSP compatible SD card by running the [[https://​www.mathworks.com/​help/​supportpkg/​xilinxzynqbasedradio/​ug/​guided-host-radio-hardware-setup.html|Guided Host-Radio Hardware Setup]] from within MATLAB. ​+  - Create a MathWorks HSP compatible SD card by running the [[mw>help/​supportpkg/​xilinxzynqbasedradio/​ug/​guided-host-radio-hardware-setup.html|Guided Host-Radio Hardware Setup]] from within MATLAB. ​
   - Build the image for the design from MATLAB using the provided [[https://​github.com/​analogdevicesinc/​TransceiverToolbox/​blob/​master/​trx_examples/​targeting/​loopback-delay-estimation/​hdlworkflow.m|hdlworkflow]] script   - Build the image for the design from MATLAB using the provided [[https://​github.com/​analogdevicesinc/​TransceiverToolbox/​blob/​master/​trx_examples/​targeting/​loopback-delay-estimation/​hdlworkflow.m|hdlworkflow]] script
   - Download the generated image onto the SD card.   - Download the generated image onto the SD card.
resources/eval/user-guides/adrv936x_rfsom/tutorials/loopback_delay_estimation.txt · Last modified: 14 Jan 2021 05:12 by Robin Getz