This is an old revision of the document!
This article will explain an example design that utilizes the frequency hopping features of the AD9361 transceiver through the use of its built-in fastlock profiles under external pin control. Since this example focuses on features that are generally used in tightly time-constrained applications, the design will be done primarily built around logic for the FPGA fabric and software control interfaces. The following topics will be discussed:
The AD9361 transceiver has a massive LO tuning range from 70 MHz to 6 GHz in roughly ~4 Hz steps. Allowing for support of many different applications for the transceiver. However, move the LO across this range has strict requirements, specifically for the internal VCXO driving the RX or TX paths. Whenever an LO change of 100 MHz is required from a calibrated frequency, the VCXO must be first moved and re-calibrated. This is automatically performed by the driver, and monitoring the PLL lock settings will show the TX or RX PLL unlocking during this frequency change and re-calibration phase. During this process, a series of values are written into the VCXO calibration registers that are unique for that LO frequency. The during of the re-calibration can vary depending on the divider ratio used to generate the LO in question. This will normally range from X to Y. During this phase data receiver or transmitted is invalid, and only will become valid once the related PLL is locked.
In order to increase this LO transition rate, it is possible to save these calibrations on-chip for future need LO switches. These extra registers are called fastlock registers or fastlock profiles, and a maximum of 8 are provided on-chip. If more are needed, calibration information can be pulled off-chip then loaded from the baseband processor in the future. When using these fastlock profiles, a user can simply recall a fastlock profile from the desired register set and the LO will move to the frequency associated with that profile and the LO will lock-in with ~15-25us depending on configuration and LO frequency. The selection of profiles can be done over SPI, or more commonly, over direct external pins provided at the CTRL_IN interfaces of the transceiver. The pin control interface will be used in this design since it is the fastest and most deterministic.
Frequency Hopper Controller Reference Design Interfaces
For this design, an HDL Coder workflow will be used to both generate the additional controlling IP, but also to stitch the generated IP into a custom reference design. The diagram above outlines the connections of the Hop Controller which is responsible for selecting specific fastlock profiles, as well as managing receive DMA to only capture data during the dwell period after the AD9361 has transitioned between frequencies.
The custom HDL reference design will be adapted from the standard design provided for the ADRV9361-Z7035 RF-SOM with FMC carrier board. From the original design, two main changes are made to support this frequency hopping use case. These changes are:
These are accomplished by modifying two files. The main system wrapper (system_top.v) to unbundle the desired ports:
output [ 3:0] gpio_ctl, input [ 7:0] gpio_status, output spi_csn, output spi_clk, output spi_mosi, input spi_miso); ... ad_iobuf #(.DATA_WIDTH(2)) i_iobuf_ad9361 ( .dio_t ({gpio_t[46:45]}), .dio_i ({gpio_o[46:45]}), .dio_o ({gpio_i[46:45]}), .dio_p ({ gpio_resetb, // 46:46 gpio_sync })); // 45:45 ... .up_txnrx (gpio_o[48]), .gpio_en_agc (gpio_en_agc), .gpio_status (gpio_status), .gpio_ctl (gpio_ctl));
and the main Tcl file used to build the project itself (system_bd.tcl):
ad_ip_parameter axi_ad9361 CONFIG.ADC_INIT_DELAY 29 # Add external pin for EN_AGC create_bd_port -dir O gpio_en_agc # Add external pins for CTRL_IN create_bd_port -from 0 -to 7 -dir I gpio_status # Add external pins for CTRL_OUT create_bd_port -from 0 -to 3 -dir O gpio_ctl
Back in MATLAB, a new interface definition file set is created. This simply requires modifying the add_rx_tx_io.m file, which is responsible for defining possible interfaces of generated IP. To separate this design as well, separate targets were made for this design with a specific namespace. MATLAB performs namespace separation using plus folders which you will find in the frequency-hopping folder of the ADI BSP.
tcollins@winston:/tmp/TransceiverToolbox$ ls -A trx_examples/targeting/frequency-hopping/ |grep -v /$ adi_build.tcl +AnalogDevicesDemo <--- MATLAB API to reference design build_kernel.sh ccfmc_lvds_hop <--- Verilog and tcl for reference design devicetree.dtb devicetree.dts fastlock.m FrequencyHopper.m frequency_hopping.slx hdlcoder_board_customization.m <--- Registration for HDL Workflow Advisor hdlworkflow.m hopper.patch hop_result.bmp
The Hop Controller has two main modes, hop enabled and hop disabled. In the hop disabled mode, the controller will use the current index last provided by the internal state machine. If the HOPPER_MANUAL_PROFILE_ENABLE register is set, the profile used will be based on the HOPPER_MANUAL_PROFILE register.
In hopping mode, when the HOPPER_MANUAL_PROFILE_ENABLE register is not set, the controller will rotate through profiles 0-7 in order. When 7 is reached the internal counter rolls back to start at 0 again. It will remain at the profile for 20+N samples where N is the value provided in the HOPPER_DWELL_SAMPLES register.
Register map:
Name | Register | Range | Purpose |
---|---|---|---|
HOPPER_DWELL_SAMPLES | 0x100 | 32 bits | Number of samples to remain a profile index when HOPPER_ENABLE_HOPPING is set |
HOPPER_ENABLE_HOPPING | 0x104 | 1 bit | Enables automatic profile rotation |
HOPPER_FORCE_OUT_ENABLE | 0x108 | 1 bit | Latches DMA enables high when set |
HOPPER_MANUAL_PROFILE | 0x120 | 3 bit | Index of profile to select. Only applicable when HOPPER_MANUAL_PROFILE_ENABLE is set |
HOPPER_MANUAL_PROFILE_ENABLE | 0x124 | 1 bit | Select profile index based on HOPPER_MANUAL_PROFILE instead of internal controller state |
To provide configuration to the Hop Controller IP an IIO driver was implemented, which must be built into the Linux kernel on the target platform. The source of this driver is provided as a patch to the ADI kernel. The Hop Controller IIO driver is a platform driver and can currently only be instantiated via devicetree.
Required devicetree properties:
Example
axi-hopper@43c00000 { compatible = "adi,axi-hopper-1.00"; reg = <0x43c00000 0xffff>; };
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every one of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
root@analog:/sys/bus/iio/devices/iio:device5# ls -l total 0 -rw-rw-rw- 1 root root 4096 Jan 1 00:00 dev -rw-rw-rw- 1 root root 4096 Jan 1 00:00 dwell_samples -rw-rw-rw- 1 root root 4096 Jan 1 00:00 forced_enable -rw-rw-rw- 1 root root 4096 Jan 1 00:00 hopping_enable -rw-rw-rw- 1 root root 4096 Jan 1 00:00 manual_profile_enable -rw-rw-rw- 1 root root 4096 Jan 1 00:00 manual_profile_indx -rw-rw-rw- 1 root root 4096 Jan 1 00:00 name lrwxrwxrwx 1 root root 0 Jan 1 00:03 of_node -> ../../../../../firmware/devicetree/base/fpga-axi@0/axi-hopper@43c00000 drwxrwxrwx 2 root root 0 Jan 1 00:00 power lrwxrwxrwx 1 root root 0 Jan 1 00:03 subsystem -> ../../../../../bus/iio -rw-rw-rw- 1 root root 4096 Jan 1 00:00 uevent
Using the IIO tools we can see the axi-hopper device in the IIO device list.
root@analog:~# iio_attr -a -d Using auto-detected IIO context at URI "local:" IIO context has 7 devices: iio:device3: ad9517-3, found 0 device attributes iio:device1: ad9361-phy, found 18 device attributes iio:device6: cf-ad9361-lpc, found 0 device attributes iio:device4: cf-ad9361-dds-core-lpc, found 0 device attributes iio:device2: xadc, found 1 device attributes iio:device0: ad7291, found 0 device attributes iio:device5: axi-hopper, found 5 device attributes
Since there is an IIO driver for the Hop Controller it can be controlled remotely from MATLAB. A system object called FrequencyHopper was created using the IIO binding provided in the ADI BSP to access the IIO driver. The example provided in the BSP will load profiles for 8 LO frequencies 1 MHz apart so they the receiver can view the entire hopping range. Next, the Hop Controller is configured and hopping is initiated. The script will show a frequency versus time plot similar to below.
Requirements:
To build and run the demo:
Now the ADRV9361-Z7035 can be booted from the built SD card, the fastlock.m example can be run from MATLAB. Note you may need to update the URI at the top of the example to reflect the IP address of your ADRV9361-Z7035.