This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:adrv936x_rfsom:hardware [14 Jan 2021 05:12] – user interwiki links Robin Getz | resources:eval:user-guides:adrv936x_rfsom:hardware [07 Dec 2023 14:49] (current) – Removed Board File Link Mike Jones | ||
---|---|---|---|
Line 24: | Line 24: | ||
* Carrier Card Connector Dimensions: | * Carrier Card Connector Dimensions: | ||
* {{: | * {{: | ||
+ | * ADRV9361-Z7035 Step file: {{ : | ||
</ | </ | ||
Line 36: | Line 37: | ||
===== ADRV9361-Z7035 Hardware ===== | ===== ADRV9361-Z7035 Hardware ===== | ||
- | ==== Revision F (WIP) ==== | + | ==== Revision F ==== |
- | Still under review. | + | This is the current shipping version. |
<WRAP round download> | <WRAP round download> | ||
- | * {{: | + | * {{: |
+ | * {{ : | ||
</ | </ | ||
+ | * Changes from Rev E to Rev F: | ||
+ | * The schematic did not change. We only made an adjustment to the layout. | ||
+ | * The RF traces were modified to improve the insertion loss and the return loss as well as the EVM. | ||
+ | * This resulted in some layout changes for discrete capacitors | ||
+ | * On the SOM the revision is shown as " | ||
+ | * The reset button moved position | ||
+ | |||
==== Revision E ==== | ==== Revision E ==== | ||
- | This is the current shipping version. | ||
<WRAP round download> | <WRAP round download> | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
- | * {{: | ||
</ | </ | ||
- | === Why do a Rev F? === | ||
- | * The schematic did not change. We only made an adjustment to the layout. | ||
- | * The RF traces were modified to improve the insertion loss and the return loss as well as the EVM. | ||
- | * Rev E has high attenuation on TX above 4.5 GHz | ||
==== Revision C (First publicly available revision) ==== | ==== Revision C (First publicly available revision) ==== | ||
Line 86: | Line 89: | ||
* This has the notation error described above. | * This has the notation error described above. | ||
* {{: | * {{: | ||
- | * {{ : | ||
</ | </ | ||