This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:adrv936x_rfsom:hardware [28 Jan 2021 19:57] – update arrow links after their web site update Robin Getz | resources:eval:user-guides:adrv936x_rfsom:hardware [15 Mar 2021 10:58] – Brian OLoughlin | ||
---|---|---|---|
Line 36: | Line 36: | ||
===== ADRV9361-Z7035 Hardware ===== | ===== ADRV9361-Z7035 Hardware ===== | ||
- | ==== Revision F (WIP) ==== | + | ==== Revision F ==== |
- | Still under review. | + | This is the current shipping version. |
<WRAP round download> | <WRAP round download> | ||
- | * {{: | + | * {{: |
+ | * {{ : | ||
+ | * {{ : | ||
</ | </ | ||
+ | * Changes from Rev E to Rev F: | ||
+ | * The schematic did not change. We only made an adjustment to the layout. | ||
+ | * The RF traces were modified to improve the insertion loss and the return loss as well as the EVM. | ||
+ | * This resulted in some layout changes for discrete capacitors | ||
+ | * On the SOM the revision is shown as " | ||
+ | * The reset button moved position | ||
+ | |||
==== Revision E ==== | ==== Revision E ==== | ||
- | This is the current shipping version. | ||
<WRAP round download> | <WRAP round download> | ||
Line 53: | Line 61: | ||
</ | </ | ||
- | === Why do a Rev F? === | ||
- | * The schematic did not change. We only made an adjustment to the layout. | ||
- | * The RF traces were modified to improve the insertion loss and the return loss as well as the EVM. | ||
- | * Rev E has high attenuation on TX above 4.5 GHz | ||
==== Revision C (First publicly available revision) ==== | ==== Revision C (First publicly available revision) ==== |