Wiki

This version (20 May 2024 11:18) was approved by Andrei Dragomir.The Previously approved version (14 May 2024 14:34) is available.Diff

ADRV904x Quick Start Guides

The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the ADRV904x-HB/PCBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program, or boot a Linux distribution.

Supported Carriers

The ADRV904x-HB/PCBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:

Board ADRV904x-HB/PCBZ
ZCU102
Arria 10 SoC WIP

Supported Environments

The supported OS are:

Board HDL Linux Software No-OS Software
ZCU102
Arria 10 SoC WIP WIP WIP

Hardware Setup

The ADRV904x-HB/PCBZ boards connects to the HPC2 connector (unless otherwise noted). The carrier setup requires power (12VDC 3A MAX), UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.

ZCU102 + EVAL

Unboxing guide

Detailed description of the setup procedure for ADRV9009 (similar procedure for ADRV904x):

Detailed unboxing guide

resources/eval/user-guides/adrv904x/quickstart.txt · Last modified: 20 May 2024 11:18 by Andrei Dragomir