This is an old revision of the document!
ADRV9029 DPD EVALUATION PRE-REQUISITES
EQUIPMENT NEEDED
-
-
1x Signal Generator for generating clock to the ADRV9029 Evaluation Board
1x Host Computer and an ethernet cable to connect the Host Computer to ADS9 Evaluation Platfrom
1x 5 Watt or lower RF Power Amplifier for evaluation
DC Power Supply and Cables for the RF power amplifier
1x 30dB fixed RF attenuator (Mini-Circuits BW-S30W20+ or equivalent)
1x 6dB fixed RF attenuator (Mini-Circuits VAT-6W2+ or equivalent)
1x Coupler (Mini-Circuits ZFBDC16-63HP-S+ or equivalent)
SMA connectors and RF cables to connect various components as shown in the figure below. Please note that the Observation Receiver (ORx) is on the bottom side of the ADRV9029 evaluation board.
SOFTWARE REQUIREMENTS
Operating System: Windows-10 64-bit
-
OTHER REQUIREMENTS
A wideband OFDM test signal such as LTE5/LTE10/LTE20 or NR100 signal sampled at a Tx IQ rate of 245.76
MSPS in
tab separated IQ format for evaluating DPD. Ensure that the Peak power level of the OFDM signal does not exceed -4dBFS to provide sufficient head-room for DPD gain expansion.
Typically, an OFDM signal with -14dBFS
rms and 8dB Peak-To-Average-Power Ratio is used for DPD evaluation.
-