Wiki

This version (21 Mar 2021 20:11) was approved by Anand Kumar.The Previously approved version (17 Mar 2021 04:52) is available.Diff

ADRV9029 DPD EVALUATION PRE-REQUISITES

EQUIPMENT NEEDED

  1. 1x Signal Generator for generating clock to the ADRV9029 Evaluation Board
  2. 1x Host Computer and an ethernet cable to connect the Host Computer to ADS9 Evaluation Platfrom
  3. 1x 5 Watt or lower RF Power Amplifier for evaluation
  4. DC Power Supply and Cables for the RF power amplifier
  5. 1x 30dB fixed RF attenuator (Mini-Circuits BW-S30W20+ or equivalent)
  6. 1x 6dB fixed RF attenuator (Mini-Circuits VAT-6W2+ or equivalent)
  7. 1x Coupler (Mini-Circuits ZFBDC16-63HP-S+ or equivalent)
  8. SMA connectors and RF cables to connect various components as shown in the figure below. Please note that the Observation Receiver (ORx) is on the bottom side of the ADRV9029 evaluation board.


SOFTWARE REQUIREMENTS

  1. Operating System: Windows-10 64-bit

OTHER REQUIREMENTS

  • A wideband OFDM test signal such as LTE5/LTE10/LTE20 or NR100 signal sampled at a Tx IQ rate of 245.76 MSPS in tab separated IQ format for evaluating DPD. Ensure that the Peak power level of the OFDM signal does not exceed -4dBFS to provide sufficient head-room for DPD gain expansion.
    • Typically, an OFDM signal with -14dBFS rms and 8dB Peak-To-Average-Power Ratio is used for DPD evaluation.
    • Third party vector signal generation tools such as Keysight Signal Studio, Matlab Vector Generation can be used for generating wideband OFDM signals.

Navigation - ADRV9029 DPD USER GUIDE

resources/eval/user-guides/adrv9029/prerequisites.txt · Last modified: 21 Mar 2021 20:11 by Anand Kumar