This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:adrv9029:dpd_model_optimization [08 Apr 2021 01:02] – Added additional steps Anand Kumar | resources:eval:user-guides:adrv9029:dpd_model_optimization [25 Mar 2024 06:46] (current) – [DPD Model Generation] Ramarao Bitra | ||
---|---|---|---|
Line 7: | Line 7: | ||
ADI provides a library of 140 pre-defined DPD models that are optimized for good performance on ADRV9029 with various types of Power Amplifiers that can be downloaded at this {{ : | ADI provides a library of 140 pre-defined DPD models that are optimized for good performance on ADRV9029 with various types of Power Amplifiers that can be downloaded at this {{ : | ||
+ | For 190 coefficient model files, {{ : | ||
In order to identify a DPD model for that is optimum for a Power Amplifier, the following procedure is recommended | In order to identify a DPD model for that is optimum for a Power Amplifier, the following procedure is recommended |