ADRV9029 DPD Model
DPD Model is a fundamental building block of ADRV9029 DPD that defines the GMP polynomial(memory terms and polynomial degree) for modeling a Power Amplifier in the baseband. Good modeling of the PA is critical for achieving good DPD performance. An example DPD Model descriptor is shown below
DPD Model Generation
ADI provides a library of 140 pre-defined DPD models that are optimized for good performance on ADRV9029 with various types of Power Amplifiers that can be downloaded at this link
In order to identify a DPD model for that is optimum for a Power Amplifier, the following procedure is recommended
-
-
After verifying that DPD bringup is successful on the ADRV9029 platform, browse to the location
C:\Program Files\Analog Devices\ADRV902x Transceiver Evaluation Software_x64_FULL\Resources\DpdModels/ on your PC and ensure that DPD model library is available. In case the DPD model library is not installed in the above mentioned location, the user can download the DPD model library at this
link and manually install the DPD library at the location
C:\Program Files\Analog Devices\ADRV902x Transceiver Evaluation Software_x64_FULL\Resources\DpdModels on your PC.
At this stage the user can download the DPD model sweep script provided by
ADI at
this link. The model sweep script automates the process of picking the most suitable model for the PA by iterating through the DPD model library and picking the DPD model that produces the least amount of error between pre-DPD actuator Tx and post PA observed ORx data.
Load the script downloaded in Step 4 into the Iron Python tab of the ADRV9029 TES
GUI by clicking on
File→Load in the Iron Python tab of the ADRV9029
GUI as shown in the figure below and browsing to the location where you have stored the script on your PC.
6. After loading the script, execute the script by clicking Build→Run in the Iron Python tab of ADRV9029 TES GUI
7. At the end of execution of this script, the DPD model producing the least amount of error will be logged as C:\Program Files\Analog Devices\ADRV9025 Transceiver Evaluation Software_x64_FULL\Resources\DpdModels\DpdModelOptimized.txt.
The DPD model sweep script is configured to run on transmitter Tx1 by default. Please ensure that the PA gain line up is connected to Tx1 in the ADRV9029 Evaluation System
Once the DpdModelOptimized.txt is obtained from the script, user can continue DPD evaluation by loading this DPD model as described in ADRV9029 DPD Evaluation through TES GUI