This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:adrv9009-zu11eg:testing [13 Dec 2022 02:23] – updates Alexandra Trifan | resources:eval:user-guides:adrv9009-zu11eg:testing [08 Mar 2023 13:40] (current) – [Required Software] Monica Constandachi | ||
---|---|---|---|
Line 38: | Line 38: | ||
=== ADRV9009-ZU11EG SD card === | === ADRV9009-ZU11EG SD card === | ||
The SD card image used for production testing is based on official release of Zynq images and can be downloaded from : | The SD card image used for production testing is based on official release of Zynq images and can be downloaded from : | ||
+ | <WRAP hi round download 80%> | ||
+ | * **15 December 2022 release ** | ||
+ | * [[https:// | ||
+ | * Checksum '' | ||
+ | </ | ||
<WRAP hi round download 80%> | <WRAP hi round download 80%> | ||
Line 59: | Line 64: | ||
=== Raspberry PI SD card === | === Raspberry PI SD card === | ||
The SD image used is based on Raspbian with desktop. On top of that are installed the testing scripts. The image can be created starting from vanilla Raspbian or downloaded from: | The SD image used is based on Raspbian with desktop. On top of that are installed the testing scripts. The image can be created starting from vanilla Raspbian or downloaded from: | ||
+ | |||
+ | <WRAP hi round download 80%> | ||
+ | * **15 December 2022 release ** | ||
+ | * [[https:// | ||
+ | * Checksum '' | ||
+ | </ | ||
<WRAP hi round download 80%> | <WRAP hi round download 80%> |