This is an old revision of the document!
….
There is no over-voltage or reverse polarity protection
Connect a 5V 1A power supply to TP17(GND) and TP14(VCC)
The following changes need to be made on the evaluation board:
The following connections between connectors P25(carrier) and J1(clk) need to be done.
P25 | J1 | Function |
---|---|---|
2 | 12 | GND |
3 | 20 | CS |
4 | 16 | MOSI |
5 | 18 | MISO |
6 | 14 | CLK |
There are two domains of synchronization that are considered in this configuration, the ADRV9009 transceivers and the FPGAs. Synchronization for the transceivers is provided by the clocking tree of HMC7044s and the JESD protocol. In the diagram several HMC7044s are cascade from a parent, or what we call external HMC7044, who is responsible for general system reference (sysref) control. These reference signals feed the clock chips on the individual SOMs and FPGAs.
During multi-chip synchronization (MCS), which is a feature of the ADRV9009s, all baseband data from the converters is synchronized across transceiver chips. This requires specific sysrefs to be captured at each of the transceiver simultaneously. This will also create deterministic phase differences between transceivers, when RFPLL sync is enabled, as well. The individual API rights to the transceivers, clock chips, and their sequences are detailed in the rx method of the python class adrv9009_zu11eg_multi.py.
For more information on:
Please visit the JESD204 (FSM) Interface Linux Kernel Framework page
examples/adrv9009_som_multi.py
michael@mhenneri-D06:~/devel/git/pyadi-iio$ python3 examples/adrv9009_som_multi.py --Connecting to devices Iteration# 0 ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage1> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage1> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage2> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage2> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage3> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage3> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <link_setup> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <link_setup> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage1> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage1> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage2> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage2> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage3> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage3> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage4> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage4> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage5> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage5> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clocks_enable> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clocks_enable> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <link_enable> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <link_enable> with status <0> HMC7044s CAP bank select: [14, 14, 14, 13, 13, 14, 13] JESD Link status: DATA (84a50000.axi-jesd204-rx) JESD Link status: DATA (84a30000.axi-jesd204-tx) JESD Link status: DATA (84a70000.axi-jesd204-rx) JESD Link status: DATA (84a50000.axi-jesd204-rx) JESD Link status: DATA (84a30000.axi-jesd204-tx) JESD Link status: DATA (84a70000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a50000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a30000.axi-jesd204-tx) JESD SYSREF captured: Yes (84a70000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a50000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a30000.axi-jesd204-tx) JESD SYSREF captured: Yes (84a70000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a50000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a30000.axi-jesd204-tx) JESD SYSREF alignment error: No (84a70000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a50000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a30000.axi-jesd204-tx) JESD SYSREF alignment error: No (84a70000.axi-jesd204-rx) JESD 84a50000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a70000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a50000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a70000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes ########### Across Chip (A): 16.733179 Across FMC8 (A): 174.713495 Across Chip (B): 8.009678 Across FMC8 (B): -162.783896 Across SoM (AB): 40.307809 ########### Iteration# 1 ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage1> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage1> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage2> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage2> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage3> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage3> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <link_setup> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <link_setup> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage1> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage1> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage2> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage2> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage3> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage3> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage4> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage4> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage5> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage5> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clocks_enable> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clocks_enable> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <link_enable> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <link_enable> with status <0> HMC7044s CAP bank select: [14, 14, 14, 13, 13, 14, 13] JESD Link status: DATA (84a50000.axi-jesd204-rx) JESD Link status: DATA (84a30000.axi-jesd204-tx) JESD Link status: DATA (84a70000.axi-jesd204-rx) JESD Link status: DATA (84a50000.axi-jesd204-rx) JESD Link status: DATA (84a30000.axi-jesd204-tx) JESD Link status: DATA (84a70000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a50000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a30000.axi-jesd204-tx) JESD SYSREF captured: Yes (84a70000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a50000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a30000.axi-jesd204-tx) JESD SYSREF captured: Yes (84a70000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a50000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a30000.axi-jesd204-tx) JESD SYSREF alignment error: No (84a70000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a50000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a30000.axi-jesd204-tx) JESD SYSREF alignment error: No (84a70000.axi-jesd204-rx) JESD 84a50000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a70000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a50000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a70000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes ########### Across Chip (A): 16.754098 Across FMC8 (A): 174.305087 Across Chip (B): 7.621835 Across FMC8 (B): -163.603793 Across SoM (AB): 40.224082 ########### Iteration# 2 ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage1> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage1> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage2> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage2> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clk_sync_stage3> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clk_sync_stage3> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <link_setup> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <link_setup> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage1> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage1> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage2> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage2> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage3> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage3> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage4> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage4> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <opt_setup_stage5> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <opt_setup_stage5> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <clocks_enable> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <clocks_enable> with status <0> ip:10.44.3.53: DEVICE0: Is <Paused> in state <link_enable> with status <0> ip:10.44.3.39: DEVICE1: Is <Paused> in state <link_enable> with status <0> HMC7044s CAP bank select: [14, 14, 14, 13, 13, 14, 13] JESD Link status: DATA (84a50000.axi-jesd204-rx) JESD Link status: DATA (84a30000.axi-jesd204-tx) JESD Link status: DATA (84a70000.axi-jesd204-rx) JESD Link status: DATA (84a50000.axi-jesd204-rx) JESD Link status: DATA (84a30000.axi-jesd204-tx) JESD Link status: DATA (84a70000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a50000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a30000.axi-jesd204-tx) JESD SYSREF captured: Yes (84a70000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a50000.axi-jesd204-rx) JESD SYSREF captured: Yes (84a30000.axi-jesd204-tx) JESD SYSREF captured: Yes (84a70000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a50000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a30000.axi-jesd204-tx) JESD SYSREF alignment error: No (84a70000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a50000.axi-jesd204-rx) JESD SYSREF alignment error: No (84a30000.axi-jesd204-tx) JESD SYSREF alignment error: No (84a70000.axi-jesd204-rx) JESD 84a50000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a70000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a50000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a70000.axi-jesd204-rx: 0 0 0 0 0 0 0 0 JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a50000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes JESD 84a70000.axi-jesd204-rx: Yes Yes Yes Yes Yes Yes Yes Yes ########### Across Chip (A): 16.590096 Across FMC8 (A): 173.989377 Across Chip (B): 7.867138 Across FMC8 (B): -164.080114 Across SoM (AB): 39.479836 ###########
On the primary setup check the status of the external clockchip.
This chip reporting status Unsynchronized
is expected, since this chip is only frequency locked against
a 30.720MHz reference clock.
This specifies any shell prompt running on the target
root@analog:~# iio_attr -D hmc7044-ext status
--- PLL1 ---
Status: Locked
Using: CLKIN1 @ 30720000 Hz
PFD: 3840 kHz
--- PLL2 ---
Status: Locked (Unsynchronized)
Frequency: 2949120000 Hz (Autocal cap bank value: 13)
SYSREF Status: Valid & Locked
SYNC Status: Unsynchronized
Lock Status: PLL1 & PLL2 Locked
root@analog:~#
On the primary and secondary setup check the status of all clockchips in the topology.
This specifies any shell prompt running on the target
root@analog:~# iio_attr -D hmc7044-car status --- PLL1 --- Status: Locked Using: CLKIN1 @ 30720000 Hz PFD: 7680 kHz --- PLL2 --- Status: Locked (Synchronized) Frequency: 2949120000 Hz (Autocal cap bank value: 14) SYSREF Status: Valid & Locked SYNC Status: Synchronized Lock Status: PLL1 & PLL2 Locked root@analog:~# iio_attr -D hmc7044 status --- PLL1 --- Status: Locked Using: CLKIN1 @ 30720000 Hz PFD: 30720 kHz --- PLL2 --- Status: Locked (Synchronized) Frequency: 2949120000 Hz (Autocal cap bank value: 14) SYSREF Status: Valid & Locked SYNC Status: Synchronized Lock Status: PLL1 & PLL2 Locked root@analog:~# iio_attr -D hmc7044-fmc status --- PLL1 --- Status: Locked Using: CLKIN1 @ 30720000 Hz PFD: 30720 kHz --- PLL2 --- Status: Locked (Synchronized) Frequency: 2949120000 Hz (Autocal cap bank value: 14) SYSREF Status: Valid & Locked SYNC Status: Synchronized Lock Status: PLL1 & PLL2 Locked root@analog:~#