This is an old revision of the document!
This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the ADRV9009-ZU11EG on:
Instructions on how to build the ZynqMP / MPSoC Linux kernel and devicetrees from source can be found here:
The project will be release as part of 2019_r1 release.Before then, the SD image for 2018_r2 can be used.
Details on how to write the SD card can be found here: Zynq & Altera SoC Quick Start Guide including the 2018_R2 image.
After writing the image, on the boot partition ADRV9009-ZU11EG specific files can be added from
http://swdownloads.analog.com/cse/share/ADRV9009-ZU11EG-14-06-2019.zip
ADRV9009-ZU11EG
System on Module to the ADRV2CRR-FMC
carrier board.P11
P8
(Micro USB) to your host PC.P9
P15
.S13
, S14
, S15
, S16
. See picture below.ADRV2CRR-FMC
for SD BOOT from carrier using S9
. See picture below.S12
.All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.
Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.
This specifies any shell prompt running on the target
Xilinx Zynq MP First Stage Boot Loader Release 2018.3 Jun 14 2019 - 10:06:14 U-Boot 2018.01-21435-g099c929 (May 28 2019 - 08:42:11 +0000) Analog Devices Inc. ADR9009-ZU11EG I2C: ready DRAM: 4 GiB EL Level: EL2 Chip ID: zu11eg MMC: sdhci@ff170000: 0 (SD) *** Warning - bad CRC, using default environment In: serial@ff010000 Out: serial@ff010000 Err: serial@ff010000 Bootmode: LVL_SHFT_SD_MODE1 Net: ZYNQ GEM: ff0b0000, phyaddr 1, interface sgmii i2c_mux_set: could not set mux: id: 5 chip: 74 channel: 0 I2C EEPROM MAC address read failed Warning: ethernet@ff0b0000 (eth1) using random MAC address - da:3c:6d:34:48:50 eth1: ethernet@ff0b0000ZYNQ GEM: ff0e0000, phyaddr 0, interface rgmii-id I2C EEPROM MAC address read failed Warning: ethernet@ff0e0000 (eth0) using random MAC address - 1e:d5:da:08:37:fe , eth0: ethernet@ff0e0000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device Device: sdhci@ff170000 Manufacturer ID: 3 OEM: 5344 Name: SU08G Tran Speed: 50000000 Rd Block Len: 512 SD version 3.0 High Capacity: Yes Capacity: 7.4 GiB Bus Width: 4-bit Erase Group Size: 512 Bytes reading uEnv.txt 376 bytes read in 16 ms (22.5 KiB/s) Loaded environment from uEnv.txt Importing environment from SD ... Running uenvcmd ... Copying Linux from SD to RAM... ** No boot file defined ** reading system.dtb 62255 bytes read in 19 ms (3.1 MiB/s) reading Image 16228864 bytes read in 1045 ms (14.8 MiB/s) ## Flattened Device Tree blob at 04000000 Booting using the fdt blob at 0x4000000 Loading Device Tree to 000000000ffed000, end 000000000ffff32e ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.0-12222-g6598c88 (michael@mhenneri-D06) (gcc version 6.2.1 20161114 (Linaro GCC Snapshot 6.2-2016.11)) #2783 SMP Fri Jun 14 15:35:26 CEST 2019 [ 0.000000] Boot CPU: AArch64 Processor [410fd034] [ 0.000000] Machine model: Analog Devices ADRV9009-ZU11EG [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8') [ 0.000000] bootconsole [cdns0] enabled [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 256 MiB at 0x0000000070000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] random: fast init done [ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff56000 s45080 r8192 d32744 u86016 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: enabling workaround for ARM erratum 845719 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1034240 [ 0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait root=/dev/mmcblk0p2 rw rootwait [ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes) [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes) [ 0.000000] software IO TLB [mem 0x6bfff000-0x6ffff000] (64MB) mapped at [ffffffc06bfff000-ffffffc06fffefff] [ 0.000000] Memory: 3783916K/4194304K available (10108K kernel code, 744K rwdata, 4432K rodata, 512K init, 2156K bss, 148244K reserved, 262144K cma-reserved) [ 0.000000] Virtual kernel memory layout: [ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB) [ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB) [ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008a60000 ( 10112 KB) [ 0.000000] .rodata : 0xffffff8008a60000 - 0xffffff8008ec0000 ( 4480 KB) [ 0.000000] .init : 0xffffff8008ec0000 - 0xffffff8008f40000 ( 512 KB) [ 0.000000] .data : 0xffffff8008f40000 - 0xffffff8008ffa200 ( 745 KB) [ 0.000000] .bss : 0xffffff8008ffa200 - 0xffffff8009215430 ( 2157 KB) [ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB) [ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB) [ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum) [ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual) [ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB) [ 0.000000] Hierarchical RCU implementation. [ 0.000000] RCU event tracing is enabled. [ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] arch_timer: cp15 timer(s) running at 33.33MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x7b0074340, max_idle_ns: 440795202884 ns [ 0.000003] sched_clock: 56 bits at 33MHz, resolution 30ns, wraps every 2199023255543ns [ 0.008323] Console: colour dummy device 80x25 [ 0.012388] Calibrating delay loop (skipped), value calculated using timer frequency.. 66.66 BogoMIPS (lpj=133332) [ 0.022669] pid_max: default: 32768 minimum: 301 [ 0.027357] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes) [ 0.033923] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes) [ 0.041603] ASID allocator initialised with 65536 entries [ 0.046417] Hierarchical SRCU implementation. [ 0.051074] EFI services will not be available. [ 0.055220] zynqmp_plat_init Platform Management API v1.1 [ 0.060557] zynqmp_plat_init Trustzone version v1.0 [ 0.065496] smp: Bringing up secondary CPUs ... [ 0.070160] Detected VIPT I-cache on CPU1 [ 0.070191] CPU1: Booted secondary processor [410fd034] [ 0.070481] Detected VIPT I-cache on CPU2 [ 0.070501] CPU2: Booted secondary processor [410fd034] [ 0.070781] Detected VIPT I-cache on CPU3 [ 0.070801] CPU3: Booted secondary processor [410fd034] [ 0.070847] smp: Brought up 1 node, 4 CPUs [ 0.101470] SMP: Total of 4 processors activated. [ 0.106143] CPU features: detected feature: 32-bit EL0 Support [ 0.111941] CPU: All CPU(s) started at EL2 [ 0.116012] alternatives: patching kernel code [ 0.121177] devtmpfs: initialized [ 0.130834] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.134930] futex hash table entries: 1024 (order: 5, 131072 bytes) [ 0.147153] xor: measuring software checksum speed [ 0.185224] 8regs : 2047.000 MB/sec [ 0.225258] 8regs_prefetch: 1825.000 MB/sec [ 0.265293] 32regs : 2516.000 MB/sec [ 0.305326] 32regs_prefetch: 2114.000 MB/sec [ 0.305355] xor: using function: 32regs (2516.000 MB/sec) [ 0.309731] pinctrl core: initialized pinctrl subsystem [ 0.315353] NET: Registered protocol family 16 [ 0.320133] cpuidle: using governor menu [ 0.323806] vdso: 2 pages (1 code @ ffffff8008a66000, 1 data @ ffffff8008f44000) [ 0.330523] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.337760] DMA: preallocated 256 KiB pool for atomic allocations [ 0.367510] zynqmp-pinctrl pinctrl: zynqmp pinctrl initialized [ 0.368562] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed [ 0.375283] ARM CCI_400_r1 PMU driver probed [ 0.385206] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.455137] raid6: int64x1 gen() 363 MB/s [ 0.523090] raid6: int64x1 xor() 396 MB/s [ 0.591184] raid6: int64x2 gen() 602 MB/s [ 0.659196] raid6: int64x2 xor() 536 MB/s [ 0.727208] raid6: int64x4 gen() 877 MB/s [ 0.795263] raid6: int64x4 xor() 659 MB/s [ 0.863307] raid6: int64x8 gen() 1021 MB/s [ 0.931367] raid6: int64x8 xor() 664 MB/s [ 0.999412] raid6: neonx1 gen() 644 MB/s [ 1.067476] raid6: neonx1 xor() 756 MB/s [ 1.135536] raid6: neonx2 gen() 1039 MB/s [ 1.203602] raid6: neonx2 xor() 1073 MB/s [ 1.271669] raid6: neonx4 gen() 1341 MB/s [ 1.339706] raid6: neonx4 xor() 1281 MB/s [ 1.407775] raid6: neonx8 gen() 1410 MB/s [ 1.475796] raid6: neonx8 xor() 1336 MB/s [ 1.475823] raid6: using algorithm neonx8 gen() 1410 MB/s [ 1.479791] raid6: .... xor() 1336 MB/s, rmw enabled [ 1.484722] raid6: using neon recovery algorithm [ 1.490628] SCSI subsystem initialized [ 1.493184] usbcore: registered new interface driver usbfs [ 1.498512] usbcore: registered new interface driver hub [ 1.503784] usbcore: registered new device driver usb [ 1.508827] media: Linux media interface: v0.10 [ 1.513287] Linux video capture interface: v2.00 [ 1.517883] pps_core: LinuxPPS API ver. 1 registered [ 1.522783] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 1.531875] PTP clock support registered [ 1.536000] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver. [ 1.542718] FPGA manager framework [ 1.546063] fpga-region fpga-full: FPGA Region probed [ 1.551065] Advanced Linux Sound Architecture Driver Initialized. [ 1.557291] Bluetooth: Core ver 2.22 [ 1.560596] NET: Registered protocol family 31 [ 1.564997] Bluetooth: HCI device and connection manager initialized [ 1.571313] Bluetooth: HCI socket layer initialized [ 1.576155] Bluetooth: L2CAP socket layer initialized [ 1.581186] Bluetooth: SCO socket layer initialized [ 1.586633] clocksource: Switched to clocksource arch_sys_counter [ 1.592151] VFS: Disk quotas dquot_6.6.0 [ 1.596010] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 1.607024] NET: Registered protocol family 2 [ 1.607416] TCP established hash table entries: 32768 (order: 6, 262144 bytes) [ 1.614527] TCP bind hash table entries: 32768 (order: 7, 524288 bytes) [ 1.621359] TCP: Hash tables configured (established 32768 bind 32768) [ 1.627426] UDP hash table entries: 2048 (order: 4, 65536 bytes) [ 1.633413] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes) [ 1.639895] NET: Registered protocol family 1 [ 1.644249] RPC: Registered named UNIX socket transport module. [ 1.649945] RPC: Registered udp transport module. [ 1.654611] RPC: Registered tcp transport module. [ 1.659281] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 1.666213] hw perfevents: no interrupt-affinity property for /pmu, guessing. [ 1.672962] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 1.681095] audit: initializing netlink subsys (disabled) [ 1.685914] audit: type=2000 audit(1.631:1): state=initialized audit_enabled=0 res=1 [ 1.686317] workingset: timestamp_bits=62 max_order=20 bucket_order=0 [ 1.700657] NFS: Registering the id_resolver key type [ 1.704971] Key type id_resolver registered [ 1.709106] Key type id_legacy registered [ 1.713090] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 1.719758] jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc. [ 1.753319] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247) [ 1.755070] io scheduler noop registered [ 1.758968] io scheduler deadline registered [ 1.763211] io scheduler cfq registered (default) [ 1.767867] io scheduler mq-deadline registered [ 1.772364] io scheduler kyber registered [ 1.778180] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed [ 1.811060] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled [ 1.814439] cacheinfo: Unable to detect cache hierarchy for CPU 0 [ 1.822332] brd: module loaded [ 1.825796] loop: module loaded [ 1.826457] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.832536] libphy: Fixed MDIO Bus: probed [ 1.835518] tun: Universal TUN/TAP device driver, 1.6 [ 1.839638] CAN device driver interface [ 1.843839] macb ff0b0000.ethernet: Not enabling partial store and forward [ 1.875869] macb ff0e0000.ethernet: Not enabling partial store and forward [ 1.903460] usbcore: registered new interface driver asix [ 1.903535] usbcore: registered new interface driver ax88179_178a [ 1.909297] usbcore: registered new interface driver cdc_ether [ 1.915092] usbcore: registered new interface driver net1080 [ 1.920710] usbcore: registered new interface driver cdc_subset [ 1.926592] usbcore: registered new interface driver zaurus [ 1.932137] usbcore: registered new interface driver cdc_ncm [ 1.937967] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM [ 1.945448] usbcore: registered new interface driver uas [ 1.949269] usbcore: registered new interface driver usb-storage [ 1.955497] i2c /dev entries driver [ 1.959608] IR NEC protocol handler initialized [ 1.963162] IR RC5(x/sz) protocol handler initialized [ 1.968176] IR RC6 protocol handler initialized [ 1.972676] IR JVC protocol handler initialized [ 1.977171] IR Sony protocol handler initialized [ 1.981756] IR SANYO protocol handler initialized [ 1.986427] IR Sharp protocol handler initialized [ 1.991098] IR MCE Keyboard/mouse protocol handler initialized [ 1.996894] IR XMP protocol handler initialized [ 2.002058] usbcore: registered new interface driver uvcvideo [ 2.007103] USB Video Class driver (1.1.1) [ 2.011309] axi_fan_control_driver 80000000.axi-fan-control: Re-mapped from 0x80000000 to ffffff800b6d0000 [ 2.020776] axi_fan_control_driver 80000000.axi-fan-control: Major version mismatch. Expected 1.00.a, Reported 0.01. [ 2.031736] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff800921e000 with timeout 60s [ 2.040410] Bluetooth: HCI UART driver ver 2.3 [ 2.044647] Bluetooth: HCI UART protocol H4 registered [ 2.049747] Bluetooth: HCI UART protocol BCSP registered [ 2.055023] Bluetooth: HCI UART protocol ATH3K registered [ 2.060385] Bluetooth: HCI UART protocol Three-wire (H5) registered [ 2.066657] Bluetooth: HCI UART protocol Intel registered [ 2.071977] Bluetooth: HCI UART protocol QCA registered [ 2.077196] usbcore: registered new interface driver bcm203x [ 2.082816] usbcore: registered new interface driver bpa10x [ 2.088353] usbcore: registered new interface driver bfusb [ 2.093804] usbcore: registered new interface driver btusb [ 2.099226] Bluetooth: Generic Bluetooth SDIO driver ver 0.1 [ 2.104890] usbcore: registered new interface driver ath3k [ 2.110751] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1066666 KHz [ 2.117695] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz [ 2.126504] sdhci: Secure Digital Host Controller Interface driver [ 2.132269] sdhci: Copyright(c) Pierre Ossman [ 2.136593] sdhci-pltfm: SDHCI platform and OF driver helper [ 2.143439] ledtrig-cpu: registered to indicate activity on CPUs [ 2.148321] usbcore: registered new interface driver usbhid [ 2.153722] usbhid: USB HID core driver [ 2.206546] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered [ 2.208080] pktgen: Packet Generator for packet performance testing. Version: 2.75 [ 2.215060] Netfilter messages via NETLINK v0.30. [ 2.219659] ip_tables: (C) 2000-2006 Netfilter Core Team [ 2.224955] Initializing XFRM netlink socket [ 2.229113] NET: Registered protocol family 10 [ 2.233830] Segment Routing with IPv6 [ 2.237141] ip6_tables: (C) 2000-2006 Netfilter Core Team [ 2.242594] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 2.248661] NET: Registered protocol family 17 [ 2.252766] NET: Registered protocol family 15 [ 2.257180] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this. [ 2.270056] Ebtables v2.0 registered [ 2.273682] can: controller area network core (rev 20170425 abi 9) [ 2.279769] NET: Registered protocol family 29 [ 2.284157] can: raw protocol (rev 20170425) [ 2.288393] can: broadcast manager protocol (rev 20170425 t) [ 2.294018] can: netlink gateway (rev 20170425) max_hops=1 [ 2.299519] Bluetooth: RFCOMM TTY layer initialized [ 2.304315] Bluetooth: RFCOMM socket layer initialized [ 2.309420] Bluetooth: RFCOMM ver 1.11 [ 2.313136] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 2.318409] Bluetooth: BNEP filters: protocol multicast [ 2.323604] Bluetooth: BNEP socket layer initialized [ 2.328530] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 2.334413] Bluetooth: HIDP socket layer initialized [ 2.339445] 9pnet: Installing 9P2000 support [ 2.343595] Key type dns_resolver registered [ 2.348279] registered taskstats version 1 [ 2.352220] Btrfs loaded, crc32c=crc32c-generic �ہ 2.370929] console [ttyPS0] enabledat MMIO 0xff010000 (irq = 22, base_baud = 6249999) is a xuartps [ 2.370929] console [ttyPS0] enabled [ 2.374506] bootconsole [cdns0] disabled [ 2.374506] bootconsole [cdns0] disabled [ 2.382895] GPIO line 13 (ulpi-phy-reset) hogged as output/high [ 2.392770] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:8 protocol:4 pll_locked:yes [ 2.400962] PLL: shutdown [ 2.404926] zynqmp_pll_set_rate() set divider failed for dpll_int, ret = -13 [ 2.412016] zynqmp_clk_divider_set_rate() set divider failed for gpu_ref_div1, ret = -13 [ 2.421593] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Failed to get required clock freq [ 2.431694] xilinx-dp-snd-codec: probe of fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0 failed with error -22 [ 2.441756] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed [ 2.449813] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed [ 2.457888] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 2.467957] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000 [ 2.474991] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 2.481600] [drm] No driver support for vblank timestamp query. [ 2.487557] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008b11f30) [ 2.519821] PLL: enable [ 2.649238] Console: switching to colour frame buffer device 240x67 [ 2.674637] zynqmp-display fd4a0000.zynqmp-display: fb0: frame buffer device [ 2.681970] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0 [ 2.690077] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed [ 2.699142] macb ff0b0000.ethernet: Not enabling partial store and forward [ 2.706553] libphy: MACB_mii_bus: probed [ 2.740068] macb ff0e0000.ethernet: Not enabling partial store and forward [ 2.747391] libphy: MACB_mii_bus: probed [ 2.822746] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 14 (1e:d5:da:08:37:fe) [ 2.832574] Marvell 88E1510 ff0e0000.ethernet-ffffffff:00: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:00, irq=POLL) [ 2.848331] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:0 protocol:3 pll_locked:yes [ 2.858414] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 2.863909] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 2.871802] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010 [ 2.880522] xhci-hcd xhci-hcd.0.auto: irq 34, io mem 0xfe200000 [ 2.886556] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 2.893344] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 2.900561] usb usb1: Product: xHCI Host Controller [ 2.905430] usb usb1: Manufacturer: Linux 4.14.0-12222-g6598c88 xhci-hcd [ 2.912122] usb usb1: SerialNumber: xhci-hcd.0.auto [ 2.917295] hub 1-0:1.0: USB hub found [ 2.921056] hub 1-0:1.0: 1 port detected [ 2.925157] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 2.930646] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 2.938339] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 2.946513] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003 [ 2.953294] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 2.960504] usb usb2: Product: xHCI Host Controller [ 2.965375] usb usb2: Manufacturer: Linux 4.14.0-12222-g6598c88 xhci-hcd [ 2.972066] usb usb2: SerialNumber: xhci-hcd.0.auto [ 2.977185] hub 2-0:1.0: USB hub found [ 2.980948] hub 2-0:1.0: 1 port detected [ 2.987163] at24 0-002c: 2048 byte 24c16 EEPROM, writable, 1 bytes/write [ 2.993894] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 16 [ 3.258646] usb 1-1: new full-speed USB device number 2 using xhci-hcd [ 3.412784] usb 1-1: New USB device found, idVendor=046d, idProduct=c52b [ 3.419485] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0 [ 3.426618] usb 1-1: Product: USB Receiver [ 3.430704] usb 1-1: Manufacturer: Logitech [ 3.444263] input: Logitech USB Receiver as /devices/platform/amba/ff9d0000.usb0/fe200000.dwc3/xhci-hcd.0.auto/usb1/1-1/1-1:1.0/0003:046D:C52B.0001/input/input0 [ 3.515005] hid-generic 0003:046D:C52B.0001: input: USB HID v1.11 Keyboard [Logitech USB Receiver] on usb-xhci-hcd.0.auto-1/input0 [ 3.530419] input: Logitech USB Receiver as /devices/platform/amba/ff9d0000.usb0/fe200000.dwc3/xhci-hcd.0.auto/usb1/1-1/1-1:1.1/0003:046D:C52B.0002/input/input1 [ 3.602770] hid-generic 0003:046D:C52B.0002: input: USB HID v1.11 Mouse [Logitech USB Receiver] on usb-xhci-hcd.0.auto-1/input1 [ 3.616926] hid-generic 0003:046D:C52B.0003: device has no listeners, quitting [ 4.018649] cdns-i2c ff030000.i2c: timeout waiting on completion [ 4.024653] pca954x 1-0070: probe failed [ 4.028626] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 17 [ 4.078646] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit [ 4.092758] adrv9009 spi1.0: adrv9009_probe : enter [ 4.097840] adrv9009 spi1.1: adrv9009_probe : enter [ 4.157557] axi_adxcvr 84a40000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x84A40000 mapped to 0xffffff8009375000. Number of lanes: 4. [ 4.172340] axi_adxcvr 84a60000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x84A60000 mapped to 0xffffff800937d000. Number of lanes: 4. [ 4.186326] axi_adxcvr 84a20000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using GTH4 at 0x84A20000 mapped to 0xffffff8009385000. Number of lanes: 8. [ 4.201026] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 4.211374] macb ff0b0000.ethernet: Not enabling partial store and forward [ 4.218802] libphy: MACB_mii_bus: probed [ 4.235694] mmc0: new high speed SDHC card at address aaaa [ 4.241355] mmcblk0: mmc0:aaaa SU08G 7.40 GiB [ 4.246924] mmcblk0: p1 p2 p3 [ 4.294737] macb ff0b0000.ethernet eth1: Cadence GEM rev 0x50070106 at 0xff0b0000 irq 13 (da:3c:6d:34:48:50) [ 4.304563] Marvell 88E1510 ff0e0000.ethernet-ffffffff:01: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:01, irq=POLL) [ 4.318901] adrv9009 spi1.0: adrv9009_probe : enter [ 4.326803] adrv9009 spi1.0: ADIHAL_resetHw at index [ 4.799975] random: crng init done [ 11.866079] adrv9009 spi1.0: TAL_DEFRAMER_A deframerStatus 0x12 [ 11.872090] adrv9009 spi1.0: TAL_FRAMER_A framerStatus 0x21 [ 11.877752] adrv9009 spi1.0: TAL_FRAMER_B framerStatus 0x29 [ 11.987596] adrv9009 spi1.0: adrv9009_probe: adrv9009-x2 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized [ 11.999161] adrv9009 spi1.1: adrv9009_probe : enter [ 12.006907] adrv9009 spi1.1: ADIHAL_resetHw at index [ 12.690647] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 2 desynced (8 errors), restarting link [ 12.699342] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 3 desynced (12 errors), restarting link [ 12.808150] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 2 desynced (9 errors), restarting link [ 12.816842] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 3 desynced (631 errors), restarting link [ 19.576472] adrv9009 spi1.1: adrv9009_probe: adrv9009 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized [ 19.599339] cf_axi_dds 84a04000.axi-adrv9009-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A04000 mapped to 0xffffff800cb60000, probed DDS ADRV9009-X2 [ 19.614346] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 19.644911] cf_axi_adc 84a00000.axi-adrv9009-rx-hpc: ADI AIM (10.01.b) at 0x84A00000 mapped to 0xffffff800cb70000, probed ADC ADRV9009-X2 as MASTER [ 19.658310] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 19.669477] input: gpio_keys as /devices/platform/gpio_keys/input/input2 [ 19.676324] hctosys: unable to open rtc device (rtc0) [ 19.682504] ALSA device list: [ 19.685470] No soundcards found. [ 19.689366] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered [ 19.723364] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 19.731468] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 19.745864] devtmpfs: mounted [ 19.748945] Freeing unused kernel memory: 512K Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory [ 19.954655] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 2 desynced (50 errors), restarting link [ 19.963439] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 3 desynced (10 errors), restarting link [ 20.080717] init: hwclock main process (1789) terminated with status 1 [ 20.082654] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 2 desynced (9 errors), restarting link [ 20.082660] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 3 desynced (9 errors), restarting link [ OK ]ting up X socket directories... * STARTDISTCC is set to false in /etc/default/distcc * /usr/bin/distccd not starting [ OK ]rting IIO Daemon iiod Last login: Thu Jan 1 00:00:25 UTC 1970 on tty1 Welcome to Linaro 14.04 (GNU/Linux 4.14.0-12222-g6598c88 aarch64) * Documentation: https://wiki.analog.com/ https://ez.analog.com/ New release '16.04.6 LTS' available. Run 'do-release-upgrade' to upgrade to it. root@analog:~#
This specifies any shell prompt running on the target
root@analog:~# iio_info | grep iio:device iio:device0: ams iio:device1: hmc7044-car iio:device2: adm1177 iio:device3: hmc7044 iio:device4: adrv9009-phy iio:device5: adrv9009-phy-b iio:device6: axi-adrv9009-rx-obs-hpc (buffer capable) iio:device7: axi-adrv9009-tx-hpc (buffer capable) iio:device8: axi-adrv9009-rx-hpc (buffer capable)
This specifies any shell prompt running on the target
root@analog:~# iio_attr -q -D hmc7044 status --- PLL1 --- Status: Locked Using: CLKIN1 @ 122880000 Hz PFD: 7680 kHz --- PLL2 --- Status: Locked (Unsynchronized) Frequency: 2949120000 Hz SYSREF Status: Valid & Locked SYNC Status: Unsynchronized Lock Status: PLL1 & PLL2 Locked root@analog:~#
This specifies any shell prompt running on the target
root@analog:~# iio_attr -q -D hmc7044-car status --- PLL1 --- Status: Locked Using: CLKIN3 @ 19200000 Hz PFD: 3840 kHz --- PLL2 --- Status: Locked (Unsynchronized) Frequency: 2949120000 Hz SYSREF Status: Invalid SYNC Status: Unsynchronized Lock Status: PLL1 & PLL2 Locked root@analog:~#
This specifies any shell prompt running on the target
root@analog:~# TERM=vt100 jesd_status -s (DEVICES) Found 3 JESD204 Link Layer peripherals (0): 84a30000.axi-jesd204-tx (1): 84a50000.axi-jesd204-rx (2): 84a70000.axi-jesd204-rx (STATUS) (0) (1) (2) Link is enabled enabled enabled Link Status DATA DATA DATA Measured Link Clock 122.881 245.761 122.881 Reported Link Clock 122.880 245.760 122.880 Lane rate 4915.200 9830.400 4915.200 Lane rate / 40 122.880 245.760 122.880 LMFC rate 7.680 7.680 3.840 SYSREF captured Yes Yes Yes SYSREF alignment error No No No SYNC~ deasserted (LANE STATUS) (1) (2) Lane# 0 1 2 3 0 1 2 3 Errors 0 0 0 0 0 0 0 0 Latency (Multiframes/Octets) 2/80 2/77 2/78 2/80 2/50 2/50 2/49 2/51 CGS State DATA DATA DATA DATA DATA DATA DATA DATA Initial Frame Sync Yes Yes Yes Yes Yes Yes Yes Yes Initial Lane Alignment Sequence Yes Yes Yes Yes Yes Yes Yes Yes
The default configuration for most of the projects is to use the HDMI output, but for this project the DisplayPort is used.
In order for it to work, you should follow the steps described here: DisplayPort No Picture
After following the steps, the board should be rebooted.
Please see also here:Oscilloscope
The IIO Oscilloscope application can be used to connect to another platform that has a connected device in order to configure the device and read data from it.
Build and start osc on a network enabled Linux host.
Once the application is launched goto Settings → Connect and enter the IP address of the target in the popup window.
Even thought this is Linux, this is a persistent file systems. Care should be taken not to corrupt the file system -- please shut down things, don't just turn off the power switch. Depending on your monitor, the standard power off could be hiding. You can do this from the terminal as well with sudo shutdown -h now