Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:adrv9009-zu11eg:quick-start-guide [20 Aug 2021 09:13] – Update Michael Hennerich | resources:eval:user-guides:adrv9009-zu11eg:quick-start-guide [18 Aug 2022 16:28] – [Messages] Michael Hennerich |
---|
<code> | <code> |
Xilinx Zynq MP First Stage Boot Loader | Xilinx Zynq MP First Stage Boot Loader |
Release 2018.3 Jun 14 2019 - 10:06:14 | Release 2021.1 Aug 3 2022 - 11:00:01 |
| |
| |
U-Boot 2018.01-21435-g099c929 (May 28 2019 - 08:42:11 +0000) Analog Devices Inc. ADR9009-ZU11EG | U-Boot 2018.01-21439-gd244ce5 (Mar 28 2021 - 13:30:43 +0100) Analog Devices Inc. ADR9009-ZU11EG, Build: jenkins-development-build_uboot-3 |
| |
I2C: ready | I2C: ready |
I2C EEPROM MAC address read failed | I2C EEPROM MAC address read failed |
| |
Warning: ethernet@ff0b0000 (eth1) using random MAC address - da:3c:6d:34:48:50 | Warning: ethernet@ff0b0000 (eth1) using random MAC address - c6:bd:2a:d9:e2:01 |
eth1: ethernet@ff0b0000ZYNQ GEM: ff0e0000, phyaddr 0, interface rgmii-id | eth1: ethernet@ff0b0000ZYNQ GEM: ff0e0000, phyaddr 0, interface rgmii-id |
I2C EEPROM MAC address read failed | I2C EEPROM MAC address read failed |
| |
Warning: ethernet@ff0e0000 (eth0) using random MAC address - 1e:d5:da:08:37:fe | Warning: ethernet@ff0e0000 (eth0) using random MAC address - aa:cd:e8:38:80:de |
, eth0: ethernet@ff0e0000 | , eth0: ethernet@ff0e0000 |
Hit any key to stop autoboot: 0 | Hit any key to stop autoboot: 0 |
mmc0 is current device | mmc0 is current device |
Device: sdhci@ff170000 | Device: sdhci@ff170000 |
Manufacturer ID: 3 | Manufacturer ID: 41 |
OEM: 5344 | OEM: 3432 |
Name: SU08G | Name: SD16G |
Tran Speed: 50000000 | Tran Speed: 50000000 |
Rd Block Len: 512 | Rd Block Len: 512 |
SD version 3.0 | SD version 3.0 |
High Capacity: Yes | High Capacity: Yes |
Capacity: 7.4 GiB | Capacity: 14.6 GiB |
Bus Width: 4-bit | Bus Width: 4-bit |
Erase Group Size: 512 Bytes | Erase Group Size: 512 Bytes |
reading uEnv.txt | reading uEnv.txt |
376 bytes read in 16 ms (22.5 KiB/s) | 407 bytes read in 21 ms (18.6 KiB/s) |
Loaded environment from uEnv.txt | Loaded environment from uEnv.txt |
Importing environment from SD ... | Importing environment from SD ... |
Copying Linux from SD to RAM... | Copying Linux from SD to RAM... |
** No boot file defined ** | ** No boot file defined ** |
| SF: Detected n25q512a with page size 512 Bytes, erase size 128 KiB, total 128 MiB |
| device 0 offset 0x2000000, size 0x20000 |
| SF: 131072 bytes @ 0x2000000 Read: OK |
reading system.dtb | reading system.dtb |
62255 bytes read in 19 ms (3.1 MiB/s) | 79158 bytes read in 32 ms (2.4 MiB/s) |
reading Image | reading Image |
16228864 bytes read in 1045 ms (14.8 MiB/s) | 32514560 bytes read in 2084 ms (14.9 MiB/s) |
## Flattened Device Tree blob at 04000000 | ## Flattened Device Tree blob at 04000000 |
Booting using the fdt blob at 0x4000000 | Booting using the fdt blob at 0x4000000 |
Loading Device Tree to 000000000ffed000, end 000000000ffff32e ... OK | Loading Device Tree to 000000000ffe9000, end 000000000ffff535 ... OK |
| |
Starting kernel ... | Starting kernel ... |
| |
[ 0.000000] Booting Linux on physical CPU 0x0 | [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] |
[ 0.000000] Linux version 4.14.0-12222-g6598c88 (michael@mhenneri-D06) (gcc version 6.2.1 20161114 (Linaro GCC Snapshot 6.2-2016.11)) #2783 SMP Fri Jun 14 15:35:26 CEST 2019 | [ 0.000000] Linux version 5.10.0-98248-g1bbe32fa5182 (jenkins@romlxbuild1.adlk.analog.com) (aarch64-xilinx-linux-gcc.real (GCC) 10.2.0, 2 |
[ 0.000000] Boot CPU: AArch64 Processor [410fd034] | [ 0.000000] Machine model: Analog Devices ADRV9009-ZU11EG Rev.B |
[ 0.000000] Machine model: Analog Devices ADRV9009-ZU11EG | |
[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8') | [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8') |
[ 0.000000] bootconsole [cdns0] enabled | [ 0.000000] printk: bootconsole [cdns0] enabled |
[ 0.000000] efi: Getting EFI parameters from FDT: | |
[ 0.000000] efi: UEFI not found. | [ 0.000000] efi: UEFI not found. |
[ 0.000000] cma: Reserved 256 MiB at 0x0000000070000000 | [ 0.000000] cma: Reserved 256 MiB at 0x0000000070000000 |
| [ 0.000000] Zone ranges: |
| [ 0.000000] DMA [mem 0x0000000000000000-0x000000003fffffff] |
| [ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000ffffffff] |
| [ 0.000000] Normal [mem 0x0000000100000000-0x000000087fffffff] |
| [ 0.000000] Movable zone start for each node |
| [ 0.000000] Early memory node ranges |
| [ 0.000000] node 0: [mem 0x0000000000000000-0x000000007fffffff] |
| [ 0.000000] node 0: [mem 0x0000000800000000-0x000000087fffffff] |
| [ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000087fffffff] |
[ 0.000000] psci: probing for conduit method from DT. | [ 0.000000] psci: probing for conduit method from DT. |
[ 0.000000] psci: PSCIv1.1 detected in firmware. | [ 0.000000] psci: PSCIv1.1 detected in firmware. |
[ 0.000000] psci: Using standard PSCI v0.2 function IDs | [ 0.000000] psci: Using standard PSCI v0.2 function IDs |
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported. | [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. |
[ 0.000000] random: fast init done | [ 0.000000] psci: SMC Calling Convention v1.2 |
[ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff56000 s45080 r8192 d32744 u86016 | [ 0.000000] percpu: Embedded 22 pages/cpu s49496 r8192 d32424 u90112 |
[ 0.000000] Detected VIPT I-cache on CPU0 | [ 0.000000] Detected VIPT I-cache on CPU0 |
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719 | [ 0.000000] CPU features: detected: ARM erratum 845719 |
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1034240 | [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1034240 |
[ 0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait root=/dev/mmcblk0p2 rw rootwait | [ 0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidl1 |
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes) | [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) |
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes) | [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) |
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes) | [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off |
[ 0.000000] software IO TLB [mem 0x6bfff000-0x6ffff000] (64MB) mapped at [ffffffc06bfff000-ffffffc06fffefff] | [ 0.000000] software IO TLB: mapped [mem 0x000000003bfff000-0x000000003ffff000] (64MB) |
[ 0.000000] Memory: 3783916K/4194304K available (10108K kernel code, 744K rwdata, 4432K rodata, 512K init, 2156K bss, 148244K reserved, 262144K cma-reserved) | [ 0.000000] Memory: 3761492K/4194304K available (15488K kernel code, 1672K rwdata, 11952K rodata, 2496K init, 507K bss, 170668K reserved) |
[ 0.000000] Virtual kernel memory layout: | [ 0.000000] rcu: Hierarchical RCU implementation. |
[ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB) | [ 0.000000] rcu: RCU event tracing is enabled. |
[ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB) | [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. |
[ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008a60000 ( 10112 KB) | [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. |
[ 0.000000] .rodata : 0xffffff8008a60000 - 0xffffff8008ec0000 ( 4480 KB) | [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 |
[ 0.000000] .init : 0xffffff8008ec0000 - 0xffffff8008f40000 ( 512 KB) | |
[ 0.000000] .data : 0xffffff8008f40000 - 0xffffff8008ffa200 ( 745 KB) | |
[ 0.000000] .bss : 0xffffff8008ffa200 - 0xffffff8009215430 ( 2157 KB) | |
[ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB) | |
[ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB) | |
[ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum) | |
[ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual) | |
[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB) | |
[ 0.000000] Hierarchical RCU implementation. | |
[ 0.000000] RCU event tracing is enabled. | |
[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. | |
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 | |
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 | [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 |
[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 | [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 |
[ 0.000000] GIC: Using split EOI/Deactivate mode | [ 0.000000] GIC: Using split EOI/Deactivate mode |
| [ 0.000000] random: get_random_bytes called from start_kernel+0x31c/0x550 with crng_init=0 |
[ 0.000000] arch_timer: cp15 timer(s) running at 33.33MHz (phys). | [ 0.000000] arch_timer: cp15 timer(s) running at 33.33MHz (phys). |
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x7b0074340, max_idle_ns: 440795202884 ns | [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x7b00c47c0, max_idle_ns: 440795202120 ns |
[ 0.000003] sched_clock: 56 bits at 33MHz, resolution 30ns, wraps every 2199023255543ns | [ 0.000003] sched_clock: 56 bits at 33MHz, resolution 30ns, wraps every 2199023255541ns |
[ 0.008323] Console: colour dummy device 80x25 | [ 0.008361] Console: colour dummy device 80x25 |
[ 0.012388] Calibrating delay loop (skipped), value calculated using timer frequency.. 66.66 BogoMIPS (lpj=133332) | [ 0.012394] Calibrating delay loop (skipped), value calculated using timer frequency.. 66.66 BogoMIPS (lpj=133333) |
[ 0.022669] pid_max: default: 32768 minimum: 301 | [ 0.022667] pid_max: default: 32768 minimum: 301 |
[ 0.027357] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes) | [ 0.027374] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) |
[ 0.033923] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes) | [ 0.034613] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) |
[ 0.041603] ASID allocator initialised with 65536 entries | [ 0.043179] rcu: Hierarchical SRCU implementation. |
[ 0.046417] Hierarchical SRCU implementation. | [ 0.047369] EFI services will not be available. |
[ 0.051074] EFI services will not be available. | [ 0.051756] smp: Bringing up secondary CPUs ... |
[ 0.055220] zynqmp_plat_init Platform Management API v1.1 | [ 0.056463] Detected VIPT I-cache on CPU1 |
[ 0.060557] zynqmp_plat_init Trustzone version v1.0 | [ 0.056501] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] |
[ 0.065496] smp: Bringing up secondary CPUs ... | [ 0.056844] Detected VIPT I-cache on CPU2 |
[ 0.070160] Detected VIPT I-cache on CPU1 | [ 0.056866] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] |
[ 0.070191] CPU1: Booted secondary processor [410fd034] | [ 0.057182] Detected VIPT I-cache on CPU3 |
[ 0.070481] Detected VIPT I-cache on CPU2 | [ 0.057203] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] |
[ 0.070501] CPU2: Booted secondary processor [410fd034] | [ 0.057245] smp: Brought up 1 node, 4 CPUs |
[ 0.070781] Detected VIPT I-cache on CPU3 | [ 0.091606] SMP: Total of 4 processors activated. |
[ 0.070801] CPU3: Booted secondary processor [410fd034] | [ 0.096278] CPU features: detected: 32-bit EL0 Support |
[ 0.070847] smp: Brought up 1 node, 4 CPUs | [ 0.101382] CPU features: detected: CRC32 instructions |
[ 0.101470] SMP: Total of 4 processors activated. | [ 0.106518] CPU: All CPU(s) started at EL2 |
[ 0.106143] CPU features: detected feature: 32-bit EL0 Support | [ 0.110562] alternatives: patching kernel code |
[ 0.111941] CPU: All CPU(s) started at EL2 | [ 0.115944] devtmpfs: initialized |
[ 0.116012] alternatives: patching kernel code | [ 0.125323] Registered cp15_barrier emulation handler |
[ 0.121177] devtmpfs: initialized | [ 0.125372] Registered setend emulation handler |
[ 0.130834] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns | [ 0.129346] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns |
[ 0.134930] futex hash table entries: 1024 (order: 5, 131072 bytes) | [ 0.138935] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) |
[ 0.147153] xor: measuring software checksum speed | [ 0.151744] pinctrl core: initialized pinctrl subsystem |
[ 0.185224] 8regs : 2047.000 MB/sec | [ 0.152337] NET: Registered protocol family 16 |
[ 0.225258] 8regs_prefetch: 1825.000 MB/sec | [ 0.156729] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations |
[ 0.265293] 32regs : 2516.000 MB/sec | [ 0.162816] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations |
[ 0.305326] 32regs_prefetch: 2114.000 MB/sec | [ 0.170539] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations |
[ 0.305355] xor: using function: 32regs (2516.000 MB/sec) | [ 0.178353] audit: initializing netlink subsys (disabled) |
[ 0.309731] pinctrl core: initialized pinctrl subsystem | [ 0.183803] audit: type=2000 audit(0.116:1): state=initialized audit_enabled=0 res=1 |
[ 0.315353] NET: Registered protocol family 16 | [ 0.184104] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. |
[ 0.320133] cpuidle: using governor menu | [ 0.198177] ASID allocator initialised with 65536 entries |
[ 0.323806] vdso: 2 pages (1 code @ ffffff8008a66000, 1 data @ ffffff8008f44000) | [ 0.222829] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages |
[ 0.330523] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. | [ 0.223888] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages |
[ 0.337760] DMA: preallocated 256 KiB pool for atomic allocations | [ 0.230544] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages |
[ 0.367510] zynqmp-pinctrl pinctrl: zynqmp pinctrl initialized | [ 0.237205] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages |
[ 0.368562] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed | [ 1.208657] DRBG: Continuing without Jitter RNG |
[ 0.375283] ARM CCI_400_r1 PMU driver probed | [ 1.284514] raid6: neonx8 gen() 2356 MB/s |
[ 0.385206] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages | [ 1.352561] raid6: neonx8 xor() 1757 MB/s |
[ 0.455137] raid6: int64x1 gen() 363 MB/s | [ 1.420621] raid6: neonx4 gen() 2400 MB/s |
[ 0.523090] raid6: int64x1 xor() 396 MB/s | [ 1.488662] raid6: neonx4 xor() 1717 MB/s |
[ 0.591184] raid6: int64x2 gen() 602 MB/s | [ 1.556727] raid6: neonx2 gen() 2274 MB/s |
[ 0.659196] raid6: int64x2 xor() 536 MB/s | [ 1.624764] raid6: neonx2 xor() 1578 MB/s |
[ 0.727208] raid6: int64x4 gen() 877 MB/s | [ 1.692829] raid6: neonx1 gen() 1948 MB/s |
[ 0.795263] raid6: int64x4 xor() 659 MB/s | [ 1.760876] raid6: neonx1 xor() 1339 MB/s |
[ 0.863307] raid6: int64x8 gen() 1021 MB/s | [ 1.828924] raid6: int64x8 gen() 1578 MB/s |
[ 0.931367] raid6: int64x8 xor() 664 MB/s | [ 1.896976] raid6: int64x8 xor() 846 MB/s |
[ 0.999412] raid6: neonx1 gen() 644 MB/s | [ 1.965032] raid6: int64x4 gen() 1754 MB/s |
[ 1.067476] raid6: neonx1 xor() 756 MB/s | [ 2.033084] raid6: int64x4 xor() 897 MB/s |
[ 1.135536] raid6: neonx2 gen() 1039 MB/s | [ 2.101150] raid6: int64x2 gen() 1535 MB/s |
[ 1.203602] raid6: neonx2 xor() 1073 MB/s | [ 2.169190] raid6: int64x2 xor() 823 MB/s |
[ 1.271669] raid6: neonx4 gen() 1341 MB/s | [ 2.237260] raid6: int64x1 gen() 1131 MB/s |
[ 1.339706] raid6: neonx4 xor() 1281 MB/s | [ 2.305308] raid6: int64x1 xor() 567 MB/s |
[ 1.407775] raid6: neonx8 gen() 1410 MB/s | [ 2.305344] raid6: using algorithm neonx4 gen() 2400 MB/s |
[ 1.475796] raid6: neonx8 xor() 1336 MB/s | [ 2.309298] raid6: .... xor() 1717 MB/s, rmw enabled |
[ 1.475823] raid6: using algorithm neonx8 gen() 1410 MB/s | [ 2.314233] raid6: using neon recovery algorithm |
[ 1.479791] raid6: .... xor() 1336 MB/s, rmw enabled | [ 2.319145] iommu: Default domain type: Translated |
[ 1.484722] raid6: using neon recovery algorithm | [ 2.323858] SCSI subsystem initialized |
[ 1.490628] SCSI subsystem initialized | [ 2.327513] usbcore: registered new interface driver usbfs |
[ 1.493184] usbcore: registered new interface driver usbfs | [ 2.332854] usbcore: registered new interface driver hub |
[ 1.498512] usbcore: registered new interface driver hub | [ 2.338129] usbcore: registered new device driver usb |
[ 1.503784] usbcore: registered new device driver usb | [ 2.343240] mc: Linux media interface: v0.10 |
[ 1.508827] media: Linux media interface: v0.10 | [ 2.347380] videodev: Linux video capture interface: v2.00 |
[ 1.513287] Linux video capture interface: v2.00 | [ 2.352865] EDAC MC: Ver: 3.0.0 |
[ 1.517883] pps_core: LinuxPPS API ver. 1 registered | [ 2.356269] zynqmp-ipi-mbox mailbox@ff990400: Registered ZynqMP IPI mbox with TX/RX channels. |
[ 1.522783] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> | [ 2.364886] jesd204: created con: id=0, topo=0, link=0, /fpga-axi@0/axi-jesd204-tx@84a30000 <-> /fpga-axi@0/axi-adrv9009-tx-hpc@84a04000 |
[ 1.531875] PTP clock support registered | [ 2.376610] jesd204: created con: id=1, topo=0, link=0, /fpga-axi@0/axi-adxcvr-tx@84a20000 <-> /fpga-axi@0/axi-jesd204-tx@84a30000 |
[ 1.536000] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver. | [ 2.388288] jesd204: created con: id=2, topo=0, link=0, /axi/spi@ff040000/hmc7044@2 <-> /fpga-axi@0/axi-adxcvr-tx@84a20000 |
[ 1.542718] FPGA manager framework | [ 2.399271] jesd204: created con: id=3, topo=0, link=2, /fpga-axi@0/axi-adxcvr-rx-os@84a60000 <-> /fpga-axi@0/axi-jesd204-rx@84a70000 |
[ 1.546063] fpga-region fpga-full: FPGA Region probed | [ 2.411213] jesd204: created con: id=4, topo=0, link=2, /axi/spi@ff040000/hmc7044@2 <-> /fpga-axi@0/axi-adxcvr-rx-os@84a60000 |
[ 1.551065] Advanced Linux Sound Architecture Driver Initialized. | [ 2.422455] jesd204: created con: id=5, topo=0, link=1, /fpga-axi@0/axi-adxcvr-rx@84a40000 <-> /fpga-axi@0/axi-jesd204-rx@84a50000 |
[ 1.557291] Bluetooth: Core ver 2.22 | [ 2.434132] jesd204: created con: id=6, topo=0, link=1, /axi/spi@ff040000/hmc7044@2 <-> /fpga-axi@0/axi-adxcvr-rx@84a40000 |
[ 1.560596] NET: Registered protocol family 31 | [ 2.445122] jesd204: created con: id=7, topo=0, link=1, /axi/spi@ff040000/hmc7044-car@3 <-> /axi/spi@ff040000/hmc7044@2 |
[ 1.564997] Bluetooth: HCI device and connection manager initialized | [ 2.455843] jesd204: created con: id=8, topo=0, link=2, /axi/spi@ff040000/hmc7044-car@3 <-> /axi/spi@ff040000/hmc7044@2 |
[ 1.571313] Bluetooth: HCI socket layer initialized | [ 2.466570] jesd204: created con: id=9, topo=0, link=0, /axi/spi@ff040000/hmc7044-car@3 <-> /axi/spi@ff040000/hmc7044@2 |
[ 1.576155] Bluetooth: L2CAP socket layer initialized | [ 2.477328] jesd204: created con: id=10, topo=0, link=1, /fpga-axi@0/axi-jesd204-rx@84a50000 <-> /axi/spi@ff040000/adrv9009-phy-b@1 |
[ 1.581186] Bluetooth: SCO socket layer initialized | [ 2.489065] jesd204: created con: id=11, topo=0, link=2, /fpga-axi@0/axi-jesd204-rx@84a70000 <-> /axi/spi@ff040000/adrv9009-phy-b@1 |
[ 1.586633] clocksource: Switched to clocksource arch_sys_counter | [ 2.500830] jesd204: created con: id=12, topo=0, link=0, /fpga-axi@0/axi-adrv9009-tx-hpc@84a04000 <-> /axi/spi@ff040000/adrv9009-phy-b@1 |
[ 1.592151] VFS: Disk quotas dquot_6.6.0 | [ 2.513070] jesd204: created con: id=13, topo=0, link=1, /axi/spi@ff040000/adrv9009-phy-b@1 <-> /axi/spi@ff040000/adrv9009-phy@0 |
[ 1.596010] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) | [ 2.524546] jesd204: created con: id=14, topo=0, link=2, /axi/spi@ff040000/adrv9009-phy-b@1 <-> /axi/spi@ff040000/adrv9009-phy@0 |
[ 1.607024] NET: Registered protocol family 2 | [ 2.536062] jesd204: created con: id=15, topo=0, link=0, /axi/spi@ff040000/adrv9009-phy-b@1 <-> /axi/spi@ff040000/adrv9009-phy@0 |
[ 1.607416] TCP established hash table entries: 32768 (order: 6, 262144 bytes) | [ 2.547543] jesd204: /axi/spi@ff040000/adrv9009-phy@0: JESD204[0:0] transition uninitialized -> initialized |
[ 1.614527] TCP bind hash table entries: 32768 (order: 7, 524288 bytes) | [ 2.557215] jesd204: /axi/spi@ff040000/adrv9009-phy@0: JESD204[0:1] transition uninitialized -> initialized |
[ 1.621359] TCP: Hash tables configured (established 32768 bind 32768) | [ 2.566903] jesd204: /axi/spi@ff040000/adrv9009-phy@0: JESD204[0:2] transition uninitialized -> initialized |
[ 1.627426] UDP hash table entries: 2048 (order: 4, 65536 bytes) | [ 2.576587] jesd204: found 11 devices and 1 topologies |
[ 1.633413] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes) | [ 2.581715] FPGA manager framework |
[ 1.639895] NET: Registered protocol family 1 | [ 2.585176] Advanced Linux Sound Architecture Driver Initialized. |
[ 1.644249] RPC: Registered named UNIX socket transport module. | [ 2.591475] Bluetooth: Core ver 2.22 |
[ 1.649945] RPC: Registered udp transport module. | [ 2.594675] NET: Registered protocol family 31 |
[ 1.654611] RPC: Registered tcp transport module. | [ 2.599078] Bluetooth: HCI device and connection manager initialized |
[ 1.659281] RPC: Registered tcp NFSv4.1 backchannel transport module. | [ 2.605395] Bluetooth: HCI socket layer initialized |
[ 1.666213] hw perfevents: no interrupt-affinity property for /pmu, guessing. | [ 2.610237] Bluetooth: L2CAP socket layer initialized |
[ 1.672962] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available | [ 2.615260] Bluetooth: SCO socket layer initialized |
[ 1.681095] audit: initializing netlink subsys (disabled) | [ 2.620423] clocksource: Switched to clocksource arch_sys_counter |
[ 1.685914] audit: type=2000 audit(1.631:1): state=initialized audit_enabled=0 res=1 | [ 2.626256] VFS: Disk quotas dquot_6.6.0 |
[ 1.686317] workingset: timestamp_bits=62 max_order=20 bucket_order=0 | [ 2.630089] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) |
[ 1.700657] NFS: Registering the id_resolver key type | [ 2.640491] NET: Registered protocol family 2 |
[ 1.704971] Key type id_resolver registered | [ 2.641518] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear) |
[ 1.709106] Key type id_legacy registered | [ 2.649721] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) |
[ 1.713090] nfs4filelayout_init: NFSv4 File Layout Driver Registering... | [ 2.657734] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear) |
[ 1.719758] jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc. | [ 2.665174] TCP: Hash tables configured (established 32768 bind 32768) |
[ 1.753319] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247) | [ 2.671367] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear) |
[ 1.755070] io scheduler noop registered | [ 2.678032] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear) |
[ 1.758968] io scheduler deadline registered | [ 2.685189] NET: Registered protocol family 1 |
[ 1.763211] io scheduler cfq registered (default) | [ 2.689645] RPC: Registered named UNIX socket transport module. |
[ 1.767867] io scheduler mq-deadline registered | [ 2.695275] RPC: Registered udp transport module. |
[ 1.772364] io scheduler kyber registered | [ 2.699940] RPC: Registered tcp transport module. |
[ 1.778180] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed | [ 2.704608] RPC: Registered tcp NFSv4.1 backchannel transport module. |
[ 1.811060] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled | [ 2.711551] PCI: CLS 0 bytes, default 64 |
[ 1.814439] cacheinfo: Unable to detect cache hierarchy for CPU 0 | [ 2.715267] hw perfevents: no interrupt-affinity property for /pmu, guessing. |
[ 1.822332] brd: module loaded | [ 2.722149] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available |
[ 1.825796] loop: module loaded | [ 2.730382] Initialise system trusted keyrings |
[ 1.826457] mtdoops: mtd device (mtddev=name/number) must be supplied | [ 2.734184] workingset: timestamp_bits=62 max_order=20 bucket_order=0 |
[ 1.832536] libphy: Fixed MDIO Bus: probed | [ 2.741039] NFS: Registering the id_resolver key type |
[ 1.835518] tun: Universal TUN/TAP device driver, 1.6 | [ 2.745535] Key type id_resolver registered |
[ 1.839638] CAN device driver interface | [ 2.749675] Key type id_legacy registered |
[ 1.843839] macb ff0b0000.ethernet: Not enabling partial store and forward | [ 2.753666] nfs4filelayout_init: NFSv4 File Layout Driver Registering... |
[ 1.875869] macb ff0e0000.ethernet: Not enabling partial store and forward | [ 2.760329] jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc. |
[ 1.903460] usbcore: registered new interface driver asix | [ 2.767476] fuse: init (API version 7.32) |
[ 1.903535] usbcore: registered new interface driver ax88179_178a | [ 2.804010] NET: Registered protocol family 38 |
[ 1.909297] usbcore: registered new interface driver cdc_ether | [ 2.804051] xor: measuring software checksum speed |
[ 1.915092] usbcore: registered new interface driver net1080 | [ 2.811368] 8regs : 2593 MB/sec |
[ 1.920710] usbcore: registered new interface driver cdc_subset | [ 2.815095] 32regs : 3071 MB/sec |
[ 1.926592] usbcore: registered new interface driver zaurus | [ 2.819983] arm64_neon : 2612 MB/sec |
[ 1.932137] usbcore: registered new interface driver cdc_ncm | [ 2.820543] xor: using function: 32regs (3071 MB/sec) |
[ 1.937967] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM | [ 2.825565] Key type asymmetric registered |
[ 1.945448] usbcore: registered new interface driver uas | [ 2.829626] Asymmetric key parser 'x509' registered |
[ 1.949269] usbcore: registered new interface driver usb-storage | [ 2.834485] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248) |
[ 1.955497] i2c /dev entries driver | [ 2.841823] io scheduler mq-deadline registered |
[ 1.959608] IR NEC protocol handler initialized | [ 2.846320] io scheduler kyber registered |
[ 1.963162] IR RC5(x/sz) protocol handler initialized | [ 2.873248] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled |
[ 1.968176] IR RC6 protocol handler initialized | [ 2.877054] cacheinfo: Unable to detect cache hierarchy for CPU 0 |
[ 1.972676] IR JVC protocol handler initialized | [ 2.883828] brd: module loaded |
[ 1.977171] IR Sony protocol handler initialized | [ 2.887717] loop: module loaded |
[ 1.981756] IR SANYO protocol handler initialized | [ 2.887956] Registered mathworks_ip class |
[ 1.986427] IR Sharp protocol handler initialized | [ 2.891876] libphy: Fixed MDIO Bus: probed |
[ 1.991098] IR MCE Keyboard/mouse protocol handler initialized | [ 2.895120] tun: Universal TUN/TAP device driver, 1.6 |
[ 1.996894] IR XMP protocol handler initialized | [ 2.899287] CAN device driver interface |
[ 2.002058] usbcore: registered new interface driver uvcvideo | [ 2.903665] usbcore: registered new interface driver asix |
[ 2.007103] USB Video Class driver (1.1.1) | [ 2.908433] usbcore: registered new interface driver ax88179_178a |
[ 2.011309] axi_fan_control_driver 80000000.axi-fan-control: Re-mapped from 0x80000000 to ffffff800b6d0000 | [ 2.914465] usbcore: registered new interface driver cdc_ether |
[ 2.020776] axi_fan_control_driver 80000000.axi-fan-control: Major version mismatch. Expected 1.00.a, Reported 0.01. | [ 2.920252] usbcore: registered new interface driver net1080 |
[ 2.031736] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff800921e000 with timeout 60s | [ 2.925874] usbcore: registered new interface driver cdc_subset |
[ 2.040410] Bluetooth: HCI UART driver ver 2.3 | [ 2.931757] usbcore: registered new interface driver zaurus |
[ 2.044647] Bluetooth: HCI UART protocol H4 registered | [ 2.937304] usbcore: registered new interface driver cdc_ncm |
[ 2.049747] Bluetooth: HCI UART protocol BCSP registered | [ 2.943539] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver |
[ 2.055023] Bluetooth: HCI UART protocol ATH3K registered | [ 2.949387] ehci-pci: EHCI PCI platform driver |
[ 2.060385] Bluetooth: HCI UART protocol Three-wire (H5) registered | [ 2.954123] usbcore: registered new interface driver uas |
[ 2.066657] Bluetooth: HCI UART protocol Intel registered | [ 2.959105] usbcore: registered new interface driver usb-storage |
[ 2.071977] Bluetooth: HCI UART protocol QCA registered | [ 2.965091] usbcore: registered new interface driver usbserial_generic |
[ 2.077196] usbcore: registered new interface driver bcm203x | [ 2.971542] usbserial: USB Serial support registered for generic |
[ 2.082816] usbcore: registered new interface driver bpa10x | [ 2.977514] usbcore: registered new interface driver ftdi_sio |
[ 2.088353] usbcore: registered new interface driver bfusb | [ 2.983218] usbserial: USB Serial support registered for FTDI USB Serial Device |
[ 2.093804] usbcore: registered new interface driver btusb | [ 2.990492] usbcore: registered new interface driver upd78f0730 |
[ 2.099226] Bluetooth: Generic Bluetooth SDIO driver ver 0.1 | [ 2.996366] usbserial: USB Serial support registered for upd78f0730 |
[ 2.104890] usbcore: registered new interface driver ath3k | [ 3.003433] i2c /dev entries driver |
[ 2.110751] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1066666 KHz | [ 3.007452] usbcore: registered new interface driver uvcvideo |
[ 2.117695] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz | [ 3.011755] USB Video Class driver (1.1.1) |
[ 2.126504] sdhci: Secure Digital Host Controller Interface driver | [ 3.016188] axi_fan_control_driver 80000000.axi-fan-control: clk_get failed with -517 |
[ 2.132269] sdhci: Copyright(c) Pierre Ossman | [ 3.024182] Bluetooth: HCI UART driver ver 2.3 |
[ 2.136593] sdhci-pltfm: SDHCI platform and OF driver helper | [ 3.028020] Bluetooth: HCI UART protocol H4 registered |
[ 2.143439] ledtrig-cpu: registered to indicate activity on CPUs | [ 3.033118] Bluetooth: HCI UART protocol BCSP registered |
[ 2.148321] usbcore: registered new interface driver usbhid | [ 3.038407] Bluetooth: HCI UART protocol LL registered |
[ 2.153722] usbhid: USB HID core driver | [ 3.043498] Bluetooth: HCI UART protocol ATH3K registered |
[ 2.206546] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered | [ 3.048872] Bluetooth: HCI UART protocol Three-wire (H5) registered |
[ 2.208080] pktgen: Packet Generator for packet performance testing. Version: 2.75 | [ 3.055118] Bluetooth: HCI UART protocol Intel registered |
[ 2.215060] Netfilter messages via NETLINK v0.30. | [ 3.060465] Bluetooth: HCI UART protocol QCA registered |
[ 2.219659] ip_tables: (C) 2000-2006 Netfilter Core Team | [ 3.065665] usbcore: registered new interface driver bcm203x |
[ 2.224955] Initializing XFRM netlink socket | [ 3.071286] usbcore: registered new interface driver bpa10x |
[ 2.229113] NET: Registered protocol family 10 | [ 3.076822] usbcore: registered new interface driver bfusb |
[ 2.233830] Segment Routing with IPv6 | [ 3.082274] usbcore: registered new interface driver btusb |
[ 2.237141] ip6_tables: (C) 2000-2006 Netfilter Core Team | [ 3.087733] usbcore: registered new interface driver ath3k |
[ 2.242594] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver | [ 3.093257] EDAC MC0: 36 UE DDR ECC error type :UE Row 0 Bank 0 BankGroup Number 0 Block Number 0 on mc#0csrow#0channel#0 (csrow:0 chann) |
[ 2.248661] NET: Registered protocol family 17 | [ 3.108288] EDAC MC0: Giving out device to module 1 controller synps_ddr_controller: DEV synps_edac (INTERRUPT) |
[ 2.252766] NET: Registered protocol family 15 | [ 3.118380] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT) |
[ 2.257180] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this. | [ 3.130636] sdhci: Secure Digital Host Controller Interface driver |
[ 2.270056] Ebtables v2.0 registered | [ 3.136490] sdhci: Copyright(c) Pierre Ossman |
[ 2.273682] can: controller area network core (rev 20170425 abi 9) | [ 3.140811] sdhci-pltfm: SDHCI platform and OF driver helper |
[ 2.279769] NET: Registered protocol family 29 | [ 3.146774] ledtrig-cpu: registered to indicate activity on CPUs |
[ 2.284157] can: raw protocol (rev 20170425) | [ 3.152419] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... |
[ 2.288393] can: broadcast manager protocol (rev 20170425 t) | [ 3.158839] zynqmp_firmware_probe Platform Management API v1.1 |
[ 2.294018] can: netlink gateway (rev 20170425) max_hops=1 | [ 3.164601] zynqmp_firmware_probe Trustzone version v1.0 |
[ 2.299519] Bluetooth: RFCOMM TTY layer initialized | [ 3.210464] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized |
[ 2.304315] Bluetooth: RFCOMM socket layer initialized | [ 3.261518] zynqmp-aes firmware:zynqmp-firmware:zynqmp-aes: will run requests pump with realtime priority |
[ 2.309420] Bluetooth: RFCOMM ver 1.11 | [ 3.276577] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384) |
[ 2.313136] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 | [ 3.277249] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa) |
[ 2.318409] Bluetooth: BNEP filters: protocol multicast | [ 3.282776] usbcore: registered new interface driver usbhid |
[ 2.323604] Bluetooth: BNEP socket layer initialized | [ 3.288183] usbhid: USB HID core driver |
[ 2.328530] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 | [ 3.298771] axi_sysid 85000000.axi-sysid-0: AXI System ID core version (1.01.a) found |
[ 2.334413] Bluetooth: HIDP socket layer initialized | [ 3.301131] axi_sysid 85000000.axi-sysid-0: [(null)] on [adrv9009zu11eg] git branch <hdl_2021_r1> git <6a6c5acc8ec422c068c7787cdeb5b0ee4C |
[ 2.339445] 9pnet: Installing 9P2000 support | [ 3.317071] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered |
[ 2.343595] Key type dns_resolver registered | [ 3.323424] usbcore: registered new interface driver snd-usb-audio |
[ 2.348279] registered taskstats version 1 | [ 3.330825] pktgen: Packet Generator for packet performance testing. Version: 2.75 |
[ 2.352220] Btrfs loaded, crc32c=crc32c-generic | [ 3.337115] Initializing XFRM netlink socket |
�ہ 2.370929] console [ttyPS0] enabledat MMIO 0xff010000 (irq = 22, base_baud = 6249999) is a xuartps | [ 3.340999] NET: Registered protocol family 10 |
[ 2.370929] console [ttyPS0] enabled | [ 3.345682] Segment Routing with IPv6 |
[ 2.374506] bootconsole [cdns0] disabled | [ 3.349090] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver |
[ 2.374506] bootconsole [cdns0] disabled | [ 3.355144] NET: Registered protocol family 17 |
[ 2.382895] GPIO line 13 (ulpi-phy-reset) hogged as output/high | [ 3.359259] NET: Registered protocol family 15 |
[ 2.392770] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:8 protocol:4 pll_locked:yes | [ 3.363753] can: controller area network core |
[ 2.400962] PLL: shutdown | [ 3.368008] NET: Registered protocol family 29 |
[ 2.404926] zynqmp_pll_set_rate() set divider failed for dpll_int, ret = -13 | [ 3.372404] can: raw protocol |
[ 2.412016] zynqmp_clk_divider_set_rate() set divider failed for gpu_ref_div1, ret = -13 | [ 3.375339] can: broadcast manager protocol |
[ 2.421593] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Failed to get required clock freq | [ 3.379496] can: netlink gateway - max_hops=1 |
[ 2.431694] xilinx-dp-snd-codec: probe of fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0 failed with error -22 | [ 3.383882] Bluetooth: RFCOMM TTY layer initialized |
[ 2.441756] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed | [ 3.388667] Bluetooth: RFCOMM socket layer initialized |
[ 2.449813] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed | [ 3.393776] Bluetooth: RFCOMM ver 1.11 |
[ 2.457888] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered | [ 3.397485] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 |
[ 2.467957] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000 | [ 3.402758] Bluetooth: BNEP filters: protocol multicast |
[ 2.474991] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). | [ 3.407950] Bluetooth: BNEP socket layer initialized |
[ 2.481600] [drm] No driver support for vblank timestamp query. | [ 3.412878] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 |
[ 2.487557] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008b11f30) | [ 3.418763] Bluetooth: HIDP socket layer initialized |
[ 2.519821] PLL: enable | [ 3.423797] 9pnet: Installing 9P2000 support |
[ 2.649238] Console: switching to colour frame buffer device 240x67 | [ 3.427940] NET: Registered protocol family 36 |
[ 2.674637] zynqmp-display fd4a0000.zynqmp-display: fb0: frame buffer device | [ 3.432354] Key type dns_resolver registered |
[ 2.681970] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0 | [ 3.436762] registered taskstats version 1 |
[ 2.690077] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed | [ 3.440652] Loading compiled-in X.509 certificates |
[ 2.699142] macb ff0b0000.ethernet: Not enabling partial store and forward | [ 3.445743] Btrfs loaded, crc32c=crc32c-generic |
[ 2.706553] libphy: MACB_mii_bus: probed | [ 3.457843] ff010000.serial: ttyPS0 at MMIO 0xff010000 (irq = 31, base_baud = 6249999) is a xuartps |
[ 2.740068] macb ff0e0000.ethernet: Not enabling partial store and forward | [ 3.466866] printk: console [ttyPS0] enabled |
[ 2.747391] libphy: MACB_mii_bus: probed | [ 3.466866] printk: console [ttyPS0] enabled |
[ 2.822746] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 14 (1e:d5:da:08:37:fe) | [ 3.471160] printk: bootconsole [cdns0] disabled |
[ 2.832574] Marvell 88E1510 ff0e0000.ethernet-ffffffff:00: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:00, irq=POLL) | [ 3.471160] printk: bootconsole [cdns0] disabled |
[ 2.848331] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:0 protocol:3 pll_locked:yes | [ 3.480447] of-fpga-region fpga-full: FPGA Region probed |
[ 2.858414] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller | [ 3.490483] gpio-13 (ulpi-phy-reset): hogged as output/high |
[ 2.863909] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 | [ 3.497715] xilinx-zynqmp-dpdma fd4c0000.dma-controller: Xilinx DPDMA engine is probed |
[ 2.871802] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010 | [ 3.506449] zynqmp-display fd4a0000.display: vtc bridge property not present |
[ 2.880522] xhci-hcd xhci-hcd.0.auto: irq 34, io mem 0xfe200000 | [ 3.515394] xilinx-dp-snd-codec fd4a0000.display:zynqmp_dp_snd_codec0: Failed to get required clock freq |
[ 2.886556] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 | [ 3.524898] xilinx-dp-snd-codec: probe of fd4a0000.display:zynqmp_dp_snd_codec0 failed with error -22 |
[ 2.893344] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 | [ 3.535124] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed |
[ 2.900561] usb usb1: Product: xHCI Host Controller | [ 3.543954] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed |
[ 2.905430] usb usb1: Manufacturer: Linux 4.14.0-12222-g6598c88 xhci-hcd | [ 3.552860] OF: graph: no port node found in /axi/display@fd4a0000 |
[ 2.912122] usb usb1: SerialNumber: xhci-hcd.0.auto | [ 3.559244] xlnx-drm xlnx-drm.0: bound fd4a0000.display (ops 0xffffffc010ffd810) |
[ 2.917295] hub 1-0:1.0: USB hub found | [ 4.644438] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes |
[ 2.921056] hub 1-0:1.0: 1 port detected | [ 4.652071] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.display on minor 0 |
[ 2.925157] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller | [ 4.659562] zynqmp-display fd4a0000.display: ZynqMP DisplayPort Subsystem driver probed |
[ 2.930646] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 | [ 4.668777] adrv9009 spi1.0: adrv9009_probe : enter |
[ 2.938339] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. | [ 4.674594] adrv9009 spi1.1: adrv9009_probe : enter |
[ 2.946513] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003 | [ 4.760470] hmc7044 spi1.3: PLL1: Locked, CLKIN3 @ 38400000 Hz, PFD: 7680 kHz - PLL2: Locked @ 2949.120000 MHz |
[ 2.953294] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 | [ 4.770830] jesd204: /axi/spi@ff040000/hmc7044-car@3,jesd204:3,parent=spi1.3: Using as SYSREF provider |
[ 2.960504] usb usb2: Product: xHCI Host Controller | [ 4.780817] hmc7044 spi1.4: Read/Write check failed (0xFF) |
[ 2.965375] usb usb2: Manufacturer: Linux 4.14.0-12222-g6598c88 xhci-hcd | [ 4.833539] hmc7044 spi1.4: Probed, SPI read support failed |
[ 2.972066] usb usb2: SerialNumber: xhci-hcd.0.auto | [ 4.840132] spi-nor spi0.0: SPI-NOR-UniqueID 104000a87704000209002100f73e717c69 |
[ 2.977185] hub 2-0:1.0: USB hub found | [ 4.847824] random: fast init done |
[ 2.980948] hub 2-0:1.0: 1 port detected | [ 4.851386] spi-nor spi0.0: trying to lock already unlocked area |
[ 2.987163] at24 0-002c: 2048 byte 24c16 EEPROM, writable, 1 bytes/write | [ 4.857388] spi-nor spi0.0: n25q512a (131072 Kbytes) |
[ 2.993894] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 16 | [ 4.862362] 4 fixed-partitions partitions found on MTD device spi0.0 |
[ 3.258646] usb 1-1: new full-speed USB device number 2 using xhci-hcd | [ 4.868706] Creating 4 MTD partitions on "spi0.0": |
[ 3.412784] usb 1-1: New USB device found, idVendor=046d, idProduct=c52b | [ 4.873488] 0x000000000000-0x000002000000 : "qspi-fsbl-uboot" |
[ 3.419485] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0 | [ 4.879931] 0x000002000000-0x000002020000 : "qspi-uboot-env" |
[ 3.426618] usb 1-1: Product: USB Receiver | [ 4.886199] 0x000002020000-0x000002100000 : "qspi-nvmfs" |
[ 3.430704] usb 1-1: Manufacturer: Logitech | [ 4.892115] 0x000002100000-0x000007f00000 : "qspi-linux" |
[ 3.444263] input: Logitech USB Receiver as /devices/platform/amba/ff9d0000.usb0/fe200000.dwc3/xhci-hcd.0.auto/usb1/1-1/1-1:1.0/0003:046D:C52B.0001/input/input0 | [ 4.899871] macb ff0e0000.ethernet: Not enabling partial store and forward |
[ 3.515005] hid-generic 0003:046D:C52B.0001: input: USB HID v1.11 Keyboard [Logitech USB Receiver] on usb-xhci-hcd.0.auto-1/input0 | [ 4.907400] libphy: MACB_mii_bus: probed |
[ 3.530419] input: Logitech USB Receiver as /devices/platform/amba/ff9d0000.usb0/fe200000.dwc3/xhci-hcd.0.auto/usb1/1-1/1-1:1.1/0003:046D:C52B.0002/input/input1 | [ 4.913221] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 21 (00:e0:22:fe:0b:d6) |
[ 3.602770] hid-generic 0003:046D:C52B.0002: input: USB HID v1.11 Mouse [Logitech USB Receiver] on usb-xhci-hcd.0.auto-1/input1 | [ 4.923467] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM |
[ 3.616926] hid-generic 0003:046D:C52B.0003: device has no listeners, quitting | [ 4.930029] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM |
[ 4.018649] cdns-i2c ff030000.i2c: timeout waiting on completion | [ 4.936559] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM |
[ 4.024653] pca954x 1-0070: probe failed | [ 4.943067] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM |
[ 4.028626] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 17 | [ 4.951512] OF: graph: no port node found in /axi/phy@fd400000 |
[ 4.078646] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit | [ 5.053782] at24 0-002c: supply vcc not found, using dummy regulator |
[ 4.092758] adrv9009 spi1.0: adrv9009_probe : enter | [ 5.060764] at24 0-002c: 2048 byte 24c16 EEPROM, writable, 1 bytes/write |
[ 4.097840] adrv9009 spi1.1: adrv9009_probe : enter | [ 5.067510] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 23 |
[ 4.157557] axi_adxcvr 84a40000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x84A40000 mapped to 0xffffff8009375000. Number of lanes: 4. | [ 5.075102] i2c i2c-1: Added multiplexed i2c bus 3 |
[ 4.172340] axi_adxcvr 84a60000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x84A60000 mapped to 0xffffff800937d000. Number of lanes: 4. | [ 5.569318] i2c i2c-1: Added multiplexed i2c bus 4 |
[ 4.186326] axi_adxcvr 84a20000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using GTH4 at 0x84A20000 mapped to 0xffffff8009385000. Number of lanes: 8. | [ 5.574255] i2c i2c-1: Added multiplexed i2c bus 5 |
[ 4.201026] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered | [ 5.579276] at24 6-0050: supply vcc not found, using dummy regulator |
[ 4.211374] macb ff0b0000.ethernet: Not enabling partial store and forward | [ 5.615141] i2c i2c-1: Added multiplexed i2c bus 6 |
[ 4.218802] libphy: MACB_mii_bus: probed | [ 5.620155] at24 7-0050: supply vcc not found, using dummy regulator |
[ 4.235694] mmc0: new high speed SDHC card at address aaaa | [ 5.654316] i2c i2c-1: Added multiplexed i2c bus 7 |
[ 4.241355] mmcblk0: mmc0:aaaa SU08G 7.40 GiB | [ 5.659324] at24 8-0050: supply vcc not found, using dummy regulator |
[ 4.246924] mmcblk0: p1 p2 p3 | [ 5.695115] i2c i2c-1: Added multiplexed i2c bus 8 |
[ 4.294737] macb ff0b0000.ethernet eth1: Cadence GEM rev 0x50070106 at 0xff0b0000 irq 13 (da:3c:6d:34:48:50) | [ 5.700043] i2c i2c-1: Added multiplexed i2c bus 9 |
[ 4.304563] Marvell 88E1510 ff0e0000.ethernet-ffffffff:01: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:01, irq=POLL) | [ 5.704968] i2c i2c-1: Added multiplexed i2c bus 10 |
[ 4.318901] adrv9009 spi1.0: adrv9009_probe : enter | [ 5.709847] pca954x 1-0070: registered 8 multiplexed busses for I2C switch pca9548 |
[ 4.326803] adrv9009 spi1.0: ADIHAL_resetHw at index | [ 5.717454] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 24 |
[ 4.799975] random: crng init done | [ 5.724248] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s |
[ 11.866079] adrv9009 spi1.0: TAL_DEFRAMER_A deframerStatus 0x12 | [ 5.731852] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1316666653 (-34) |
[ 11.872090] adrv9009 spi1.0: TAL_FRAMER_A framerStatus 0x21 | [ 5.740593] cpufreq: cpufreq_online: CPU0: Running at unlisted initial frequency: 1316666 KHz, changing to: 1199999 KHz |
[ 11.877752] adrv9009 spi1.0: TAL_FRAMER_B framerStatus 0x29 | [ 5.751385] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1316666653 (-34) |
[ 11.987596] adrv9009 spi1.0: adrv9009_probe: adrv9009-x2 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized | [ 5.761590] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes |
[ 11.999161] adrv9009 spi1.1: adrv9009_probe : enter | [ 5.771554] axi-i2s 82000000.axi-i2s-adi: probed, capture enabled, playback enabled |
[ 12.006907] adrv9009 spi1.1: ADIHAL_resetHw at index | [ 5.779704] adrv9009 spi1.0: adrv9009_probe : enter |
[ 12.690647] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 2 desynced (8 errors), restarting link | [ 5.785338] adrv9009 spi1.1: adrv9009_probe : enter |
[ 12.699342] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 3 desynced (12 errors), restarting link | [ 5.794144] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit |
[ 12.808150] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 2 desynced (9 errors), restarting link | [ 5.838432] hmc7044 spi1.2: PLL1: Locked, CLKIN1 @ 30720000 Hz, PFD: 30720 kHz - PLL2: Locked @ 2949.120000 MHz |
[ 12.816842] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 3 desynced (631 errors), restarting link | [ 5.849324] macb ff0b0000.ethernet: Not enabling partial store and forward |
[ 19.576472] adrv9009 spi1.1: adrv9009_probe: adrv9009 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized | [ 5.859757] mmc0: new high speed SDHC card at address 0001 |
[ 19.599339] cf_axi_dds 84a04000.axi-adrv9009-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A04000 mapped to 0xffffff800cb60000, probed DDS ADRV9009-X2 | [ 5.865588] mmcblk0: mmc0:0001 SD16G 14.6 GiB |
[ 19.614346] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered | [ 5.871588] libphy: MACB_mii_bus: probed |
[ 19.644911] cf_axi_adc 84a00000.axi-adrv9009-rx-hpc: ADI AIM (10.01.b) at 0x84A00000 mapped to 0xffffff800cb70000, probed ADC ADRV9009-X2 as MASTER | [ 5.875571] macb ff0b0000.ethernet eth1: Cadence GEM rev 0x50070106 at 0xff0b0000 irq 20 (c6:bd:2a:d9:e2:01) |
[ 19.658310] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered | [ 5.887653] mmcblk0: p1 p2 p3 |
[ 19.669477] input: gpio_keys as /devices/platform/gpio_keys/input/input2 | [ 5.891736] axi_adxcvr 84a40000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.05.a) using CPLL on GTH4 at 0x84A40000. Number of lanes: 4. |
[ 19.676324] hctosys: unable to open rtc device (rtc0) | [ 5.905263] axi_adxcvr 84a60000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.05.a) using CPLL on GTH4 at 0x84A60000. Number of lanes: 4. |
[ 19.682504] ALSA device list: | [ 5.917738] axi_adxcvr 84a20000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.05.a) using QPLL on GTH4 at 0x84A20000. Number of lanes: 8. |
[ 19.685470] No soundcards found. | [ 5.929482] axi-jesd204-rx 84a50000.axi-jesd204-rx: AXI-JESD204-RX (1.07.a) at 0x84A50000. Encoder 8b10b, width 4/4, lanes 4, jesd204-fs. |
[ 19.689366] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered | [ 5.942407] axi-jesd204-rx 84a70000.axi-jesd204-rx: AXI-JESD204-RX (1.07.a) at 0x84A70000. Encoder 8b10b, width 4/4, lanes 4, jesd204-fs. |
[ 19.723364] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) | [ 5.955219] axi-jesd204-tx 84a30000.axi-jesd204-tx: AXI-JESD204-TX (1.06.a) at 0x84A30000. Encoder 8b10b, width 4/4, lanes 8, jesd204-fs. |
[ 19.731468] VFS: Mounted root (ext4 filesystem) on device 179:2. | [ 5.972920] adrv9009 spi1.0: adrv9009_probe : enter |
[ 19.745864] devtmpfs: mounted | [ 5.983087] adrv9009 spi1.1: adrv9009_probe : enter |
[ 19.748945] Freeing unused kernel memory: 512K | [ 6.014044] cf_axi_adc 84a00000.axi-adrv9009-rx-hpc: ADI AIM (10.01.b) at 0x84A00000 mapped to 0x(____ptrval____), probed ADC ADRV9009-XR |
Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory | [ 6.045146] cf_axi_dds 84a04000.axi-adrv9009-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A04000 mapped to 0x(____ptrval2 |
[ 19.954655] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 2 desynced (50 errors), restarting link | [ 6.059953] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition initialized -> probed |
[ 19.963439] axi-jesd204-rx 84a50000.axi-jesd204-rx: Lane 3 desynced (10 errors), restarting link | [ 6.071171] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition initialized -> probed |
[ 20.080717] init: hwclock main process (1789) terminated with status 1 | [ 6.082381] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition initialized -> probed |
[ 20.082654] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 2 desynced (9 errors), restarting link | [ 6.093608] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition probed -> idle |
[ 20.082660] axi-jesd204-rx 84a70000.axi-jesd204-rx: Lane 3 desynced (9 errors), restarting link | [ 6.104214] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition probed -> idle |
[ OK ]ting up X socket directories... | [ 6.114829] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition probed -> idle |
* STARTDISTCC is set to false in /etc/default/distcc | [ 6.125442] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition idle -> device_init |
* /usr/bin/distccd not starting | [ 6.136484] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition idle -> device_init |
[ OK ]rting IIO Daemon iiod | [ 6.147523] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition idle -> device_init |
| [ 6.158566] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition device_init -> link_init |
| [ 6.170044] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition device_init -> link_init |
| [ 6.181515] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition device_init -> link_init |
| [ 6.193005] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition link_init -> link_supported |
| [ 6.204735] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition link_init -> link_supported |
| [ 6.216469] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition link_init -> link_supported |
| [ 6.228926] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition link_supported -> link_pre_setup |
| [ 6.241098] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition link_supported -> link_pre_setup |
| [ 6.253263] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition link_supported -> link_pre_setup |
| [ 6.309896] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition link_pre_setup -> clk_sync_stage1 |
| [ 6.322153] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition link_pre_setup -> clk_sync_stage1 |
| [ 6.334408] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition link_pre_setup -> clk_sync_stage1 |
| [ 6.356435] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition clk_sync_stage1 -> clk_sync_stage2 |
| [ 6.368780] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition clk_sync_stage1 -> clk_sync_stage2 |
| [ 6.381121] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition clk_sync_stage1 -> clk_sync_stage2 |
| [ 6.393546] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage3 |
| [ 6.405887] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage3 |
| [ 6.418228] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage3 |
| [ 6.430573] jesd204: /fpga-axi@0/axi-jesd204-rx@84a50000,jesd204:5,parent=84a50000.axi-jesd204-rx: Possible instantiation for multiple c2 |
| [ 6.445780] jesd204: /fpga-axi@0/axi-jesd204-rx@84a70000,jesd204:7,parent=84a70000.axi-jesd204-rx: Possible instantiation for multiple c2 |
| [ 6.460988] jesd204: /fpga-axi@0/axi-jesd204-tx@84a30000,jesd204:9,parent=84a30000.axi-jesd204-tx: Possible instantiation for multiple c4 |
| [ 6.478205] adrv9009 spi1.1: ADIHAL_resetHw |
| [ 6.807922] adrv9009 spi1.0: ADIHAL_resetHw |
| [ 7.137699] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition clk_sync_stage3 -> link_setup |
| [ 7.149606] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition clk_sync_stage3 -> link_setup |
| [ 7.161513] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition clk_sync_stage3 -> link_setup |
| [ 7.173585] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition link_setup -> opt_setup_stage1 |
| [ 7.185576] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition link_setup -> opt_setup_stage1 |
| [ 7.197571] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition link_setup -> opt_setup_stage1 |
| [ 7.302940] random: crng init done |
| [ 11.155203] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition opt_setup_stage1 -> opt_setup_sta2 |
| [ 11.167722] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition opt_setup_stage1 -> opt_setup_sta2 |
| [ 11.180234] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition opt_setup_stage1 -> opt_setup_sta2 |
| [ 11.192954] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition opt_setup_stage2 -> opt_setup_sta3 |
| [ 11.205468] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition opt_setup_stage2 -> opt_setup_sta3 |
| [ 11.217981] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition opt_setup_stage2 -> opt_setup_sta3 |
| [ 11.230697] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition opt_setup_stage3 -> opt_setup_sta4 |
| [ 11.243215] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition opt_setup_stage3 -> opt_setup_sta4 |
| [ 11.255731] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition opt_setup_stage3 -> opt_setup_sta4 |
| [ 16.470043] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition opt_setup_stage4 -> opt_setup_sta5 |
| [ 16.482562] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition opt_setup_stage4 -> opt_setup_sta5 |
| [ 16.495075] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition opt_setup_stage4 -> opt_setup_sta5 |
| [ 16.508137] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition opt_setup_stage5 -> clocks_enable |
| [ 16.520399] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition opt_setup_stage5 -> clocks_enable |
| [ 16.532650] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition opt_setup_stage5 -> clocks_enable |
| [ 16.550135] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition clocks_enable -> link_enable |
| [ 16.561954] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition clocks_enable -> link_enable |
| [ 16.573775] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition clocks_enable -> link_enable |
| [ 16.620711] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition link_enable -> link_running |
| [ 16.632446] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition link_enable -> link_running |
| [ 16.644179] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition link_enable -> link_running |
| [ 16.757453] adrv9009 spi1.1: adrv9009_info: adrv9009 Rev 192, Firmware 6.2.1 API version: 3.6.2.1 successfully initialized via jesd204-fm |
| [ 16.871422] adrv9009 spi1.0: adrv9009_info: adrv9009-x2 Rev 192, Firmware 6.2.1 API version: 3.6.2.1 successfully initialized via jesd20m |
| [ 16.884116] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:0] transition link_running -> opt_post_running_e |
| [ 16.896803] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:1] transition link_running -> opt_post_running_e |
| [ 16.909492] jesd204: /axi/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0:2] transition link_running -> opt_post_running_e |
| [ 16.925576] input: gpio_keys as /devices/platform/gpio_keys/input/input0 |
| [ 16.932512] of_cfs_init |
| [ 16.934968] of_cfs_init: OK |
| [ 16.937966] cfg80211: Loading compiled-in X.509 certificates for regulatory database |
| [ 17.061586] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' |
| [ 17.068114] clk: Not disabling unused clocks |
| [ 17.072633] ALSA device list: |
| [ 17.075591] #0: ADRV9009 ZU11EG ADAU1761 |
| [ 17.079945] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 |
| [ 17.088553] cfg80211: failed to load regulatory.db |
| [ 17.944935] EXT4-fs (mmcblk0p2): recovery complete |
| [ 17.953394] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) |
| [ 17.961514] VFS: Mounted root (ext4 filesystem) on device 179:2. |
| [ 17.975849] devtmpfs: mounted |
| [ 17.979570] Freeing unused kernel memory: 2496K |
| [ 17.984188] Run /sbin/init as init process |
| [ 18.494456] systemd[1]: System time before build time, advancing clock. |
| [ 18.533602] systemd[1]: systemd 247.3-7+rpi1 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRY) |
| [ 18.556807] systemd[1]: Detected architecture arm64. |
| |
Last login: Thu Jan 1 00:00:25 UTC 1970 on tty1 | Welcome to Kuiper GNU/Linux 11.2 (bullseye)! |
Welcome to Linaro 14.04 (GNU/Linux 4.14.0-12222-g6598c88 aarch64) | |
| |
* Documentation: https://wiki.analog.com/ https://ez.analog.com/ | [ 18.581954] systemd[1]: Set hostname to <analog>. |
| [ 19.969929] systemd[1]: /lib/systemd/system/plymouth-start.service:16: Unit configured to use KillMode=none. This is unsafe, as it disab. |
| [ 20.190835] systemd[1]: Queued start job for default target Graphical Interface. |
| [ 20.199479] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. |
| [ 20.211857] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) |
| [ 20.220887] systemd[1]: Created slice system-getty.slice. |
| [ OK ] Created slice system-getty.slice. |
| [ 20.240857] systemd[1]: Created slice system-modprobe.slice. |
| [ OK ] Created slice system-modprobe.slice. |
| [ 20.260796] systemd[1]: Created slice system-serial\x2dgetty.slice. |
| [ OK ] Created slice system-serial\x2dgetty.slice. |
| [ 20.284787] systemd[1]: Created slice system-systemd\x2dfsck.slice. |
| [ OK ] Created slice system-systemd\x2dfsck.slice. |
| [ 20.308673] systemd[1]: Created slice User and Session Slice. |
| [ OK ] Created slice User and Session Slice. |
| [ 20.328694] systemd[1]: Started Forward Password Requests to Wall Directory Watch. |
| [ OK ] Started Forward Password R�…uests to Wall Directory Watch. |
| [ 20.352710] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped. |
| [ 20.365061] systemd[1]: Reached target Slices. |
| [ OK ] Reached target Slices. |
| [ 20.380579] systemd[1]: Reached target Swap. |
| [ OK ] Reached target Swap. |
| [ 20.397194] systemd[1]: Listening on Syslog Socket. |
| [ OK ] Listening on Syslog Socket. |
| [ 20.412791] systemd[1]: Listening on fsck to fsckd communication Socket. |
| [ OK ] Listening on fsck to fsckd communication Socket. |
| [ 20.436648] systemd[1]: Listening on initctl Compatibility Named Pipe. |
| [ OK ] Listening on initctl Compatibility Named Pipe. |
| [ 20.461108] systemd[1]: Listening on Journal Audit Socket. |
| [ OK ] Listening on Journal Audit Socket. |
| [ 20.480793] systemd[1]: Listening on Journal Socket (/dev/log). |
| [ OK ] Listening on Journal Socket (/dev/log). |
| [ 20.504852] systemd[1]: Listening on Journal Socket. |
| [ OK ] Listening on Journal Socket. |
| [ 20.522281] systemd[1]: Listening on udev Control Socket. |
| [ OK ] Listening on udev Control Socket. |
| [ 20.544788] systemd[1]: Listening on udev Kernel Socket. |
| [ OK ] Listening on udev Kernel Socket. |
| [ 20.566278] systemd[1]: Mounting Huge Pages File System... |
| Mounting Huge Pages File System... |
| [ 20.582131] systemd[1]: Mounting POSIX Message Queue File System... |
| Mounting POSIX Message Queue File System... |
| [ 20.605935] systemd[1]: Mounting RPC Pipe File System... |
| Mounting RPC Pipe File System... |
| [ 20.622162] systemd[1]: Mounting Kernel Debug File System... |
| Mounting Kernel Debug File System... |
| [ 20.636917] systemd[1]: Condition check resulted in Kernel Trace File System being skipped. |
| [ 20.645539] systemd[1]: Condition check resulted in Kernel Module supporting RPCSEC_GSS being skipped. |
| [ 20.658448] systemd[1]: Starting Restore / save the current clock... |
| Starting Restore / save the current clock... |
| [ 20.687824] systemd[1]: Starting Set the console keyboard layout... |
| Starting Set the console keyboard layout... |
| [ 20.710146] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped. |
| [ 20.723451] systemd[1]: Starting Load Kernel Module configfs... |
| Starting Load Kernel Module configfs... |
| [ 20.742522] systemd[1]: Starting Load Kernel Module drm... |
| Starting Load Kernel Module drm... |
| [ 20.762848] systemd[1]: Starting Load Kernel Module fuse... |
| Starting Load Kernel Module fuse... |
| [ 20.788151] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped. |
| [ 20.797422] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. |
| [ 20.808264] systemd[1]: Starting Journal Service... |
| Starting Journal Service... |
| [ 20.829135] systemd[1]: Starting Load Kernel Modules... |
| Starting Load Kernel Modules... |
| [ 20.846420] systemd[1]: Starting Remount Root and Kernel File Systems... |
| Starting Remount Root and Kernel File Systems... |
| [ 20.870354] systemd[1]: Starting Coldplug All udev Devices... |
| Starting Coldplug All udev Devices... |
| [ 20.893271] systemd[1]: Mounted Huge Pages File System. |
| [ OK ] Mounted Huge Pages File System. |
| [ 20.918303] systemd[1]: Mounted POSIX Message Queue File System. |
| [ OK ] Mounted POSIX Message Queue File System. |
| [ 20.940989] systemd[1]: Mounted RPC Pipe File System. |
| [ OK ] Mounted RPC Pipe File System. |
| [ 20.956993] systemd[1]: Mounted Kernel Debug File System. |
| [ OK ] Mounted Kernel Debug File System. |
| [ 20.977388] systemd[1]: Finished Restore / save the current clock. |
| [ OK ] Finished Restore / save the current clock. |
| [ 21.001586] systemd[1]: Finished Set the console keyboard layout. |
| [ OK ] Finished Set the console keyboard layout. |
| [ 21.027051] systemd[1]: Started Journal Service. |
| [ OK ] Started Journal Service. |
| [ OK ] Finished Load Kernel Module configfs. |
| [ OK ] Finished Load Kernel Module drm. |
| [ OK ] Finished Load Kernel Module fuse. |
| [FAILED] Failed to start Load Kernel Modules. |
| See 'systemctl status systemd-modules-load.service' for details. |
| Mounting FUSE Control File System... |
| Mounting Kernel Configuration File System... |
| Starting Apply Kernel Variables... |
| [ OK ] Mounted FUSE Control File System. |
| [ OK ] Mounted Kernel Configuration File System. |
| [ OK ] Finished Apply Kernel Variables. |
| [ OK ] Finished Coldplug All udev Devices. |
| Starting Helper to synchronize boot up for ifupdown... |
| Starting Wait for udev To �…plete Device Initialization... |
| [ OK ] Finished Helper to synchronize boot up for ifupdown. |
| [ OK ] Finished Remount Root and Kernel File Systems. |
| Starting Flush Journal to Persistent Storage... |
| Starting Load/Save Random Seed... |
| Starting Create System Users... |
| [ OK ] Finished Create System Users. |
| [ OK ] Finished Load/Save Random Seed. |
| Starting Create Static Device Nodes in /dev... |
| [ OK ] Finished Create Static Device Nodes in /dev. |
| [ OK ] Reached target Local File Systems (Pre). |
| Starting Rule-based Manage�…for Device Events and Files... |
| [ OK ] Finished Flush Journal to Persistent Storage. |
| [ OK ] Started Rule-based Manager for Device Events and Files. |
| Starting Show Plymouth Boot Screen... |
| [ OK ] Started Show Plymouth Boot Screen. |
| [ OK ] Started Forward Password R�…s to Plymouth Directory Watch. |
| [ OK ] Reached target Local Encrypted Volumes. |
| [ OK ] Found device /dev/ttyPS0. |
| [ OK ] Found device /dev/disk/by-partuuid/ce8c84ab-01. |
| [ OK ] Found device /dev/ttyS0. |
| [ OK ] Reached target Hardware activated USB gadget. |
| [ OK ] Listening on Load/Save RF �…itch Status /dev/rfkill Watch. |
| Starting File System Check�…isk/by-partuuid/ce8c84ab-01... |
| Starting Load Kernel Modules... |
| [FAILED] Failed to start Load Kernel Modules. |
| See 'systemctl status systemd-modules-load.service' for details. |
| [ OK ] Finished Wait for udev To Complete Device Initialization. |
| [ OK ] Finished File System Check�…/disk/by-partuuid/ce8c84ab-01. |
| Mounting /boot... |
| [ OK ] Started File System Check Daemon to report status. |
| Starting Load Kernel Modules... |
| [ OK ] Mounted /boot. |
| [ OK ] Reached target Local File Systems. |
| Starting Set console font and keymap... |
| Starting Preprocess NFS configuration... |
| Starting Tell Plymouth To Write Out Runtime Data... |
| Starting Create Volatile Files and Directories... |
| [ OK ] Finished Set console font and keymap. |
| [ OK ] Finished Preprocess NFS configuration. |
| [FAILED] Failed to start Load Kernel Modules. |
| See 'systemctl status systemd-modules-load.service' for details. |
| [ OK ] Finished Tell Plymouth To Write Out Runtime Data. |
| Starting Raise network interfaces... |
| [ OK ] Reached target NFS client services. |
| [ OK ] Reached target Remote File Systems (Pre). |
| [ OK ] Reached target Remote File Systems. |
| [ OK ] Finished Create Volatile Files and Directories. |
| Starting Update UTMP about System Boot/Shutdown... |
| [ OK ] Finished Update UTMP about System Boot/Shutdown. |
| [ OK ] Reached target System Initialization. |
| [ OK ] Started CUPS Scheduler. |
| [ OK ] Started Daily apt download activities. |
| [ OK ] Started Daily apt upgrade and clean activities. |
| [ OK ] Started Periodic ext4 Onli�…ata Check for All Filesystems. |
| [ OK ] Started Discard unused blocks once a week. |
| [ OK ] Started Daily rotation of log files. |
| [ OK ] Started Daily man-db regeneration. |
| [ OK ] Started Daily Cleanup of Temporary Directories. |
| [ OK ] Reached target Paths. |
| [ OK ] Reached target Timers. |
| [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. |
| [ OK ] Listening on CUPS Scheduler. |
| [ OK ] Listening on D-Bus System Message Bus Socket. |
| [ OK ] Listening on Erlang Port Mapper Daemon Activation Socket. |
| [ OK ] Listening on GPS (Global P�…ioning System) Daemon Sockets. |
| [ OK ] Listening on triggerhappy.socket. |
| [ OK ] Reached target Sockets. |
| [ OK ] Reached target Basic System. |
| Starting Save/Restore Sound Card State... |
| Starting Avahi mDNS/DNS-SD Stack... |
| [ OK ] Started Regular background program processing daemon. |
| [ OK ] Started D-Bus System Message Bus. |
| Starting dphys-swapfile - �…unt, and delete a swap file... |
| Starting Remove Stale Onli�…t4 Metadata Check Snapshots... |
| Starting Creating IIOD Context Attributes...... |
| Starting Authorization Manager... |
| Starting DHCP Client Daemon... |
| Starting LSB: Switch to on�…nless shift key is pressed)... |
| Starting LSB: rng-tools (Debian variant)... |
| Starting System Logging Service... |
| Starting User Login Management... |
| Starting triggerhappy global hotkey daemon... |
| Starting Disk Manager... |
| Starting WPA supplicant... |
| [ OK ] Finished Save/Restore Sound Card State. |
| [ OK ] Reached target Sound Card. |
| [ OK ] Finished Remove Stale Onli�…ext4 Metadata Check Snapshots. |
| [ OK ] Started triggerhappy global hotkey daemon. |
| [ OK ] Started DHCP Client Daemon. |
| [ OK ] Finished Raise network interfaces. |
| [ OK ] Finished dphys-swapfile - �…mount, and delete a swap file. |
| [ OK ] Started LSB: rng-tools (Debian variant). |
| [ OK ] Started System Logging Service. |
| [ OK ] Started User Login Management. |
| [ OK ] Started Avahi mDNS/DNS-SD Stack. |
| [ OK ] Started WPA supplicant. |
| [ OK ] Reached target Network. |
| [ OK ] Reached target Network is Online. |
| Starting CUPS Scheduler... |
| [ OK ] Started Erlang Port Mapper Daemon. |
| Starting Load USB gadget scheme... |
| Starting HTTP based time synchronization tool... |
| Starting Internet superserver... |
| Starting /etc/rc.local Compatibility... |
| Starting OpenBSD Secure Shell server... |
| Starting Permit User Sessions... |
| [ OK ] Started Unattended Upgrades Shutdown. |
| [ OK ] Started /etc/rc.local Compatibility. |
| [ OK ] Finished Permit User Sessions. |
| Starting Light Display Manager... |
| Starting Hold until boot process finishes up... |
| [ OK ] Started Authorization Manager. |
| Starting Modem Manager... |
| [ OK ] Started HTTP based time synchronization tool. |
| [ OK ] Started Internet superserver. |
| [ OK ] Finished Load USB gadget scheme. |
| Mounting Mount FunctionFS instance... |
| [ OK ] Found device /dev/ttyGS0. |
| [ OK ] Mounted Mount FunctionFS instance. |
| [ OK ] Finished Creating IIOD Context Attributes.... |
| [ OK ] Started IIO Daemon. |
| Starting IIO Daemon with USB FFS support... |
| Stopping IIO Daemon... |
| [ OK ] Stopped IIO Daemon. |
| [ OK ] Started IIO Daemon with USB FFS support. |
| Starting Start USB gadget scheme... |
| [ OK ] Started OpenBSD Secure Shell server. |
| [ OK ] Started LSB: Switch to ond�…(unless shift key is pressed). |
| |
New release '16.04.6 LTS' available. | Raspbian GNU/Linux 11 analog ttyPS0 |
Run 'do-release-upgrade' to upgrade to it. | |
| |
root@analog:~# | analog login: root (automatic login) |
| |
| Linux analog 5.10.0-98248-g1bbe32fa5182 #1143 SMP Wed Aug 3 18:38:55 IST 2022 aarch64 |
| |
| The programs included with the Debian GNU/Linux system are free software; |
| the exact distribution terms for each program are described in the |
| individual files in /usr/share/doc/*/copyright. |
| |
| Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent |
| permitted by applicable law. |
| Last login: Wed Aug 17 12:17:14 BST 2022 on ttyPS0 |
| root@analog:~# |
</code></WRAP> | </code></WRAP> |
| |