This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:adrv9009-zu11eg:quick-start-guide [07 Aug 2020 15:52] – [ADRV9009-ZU11EG Specific Boot Files] Michael Hennerich | resources:eval:user-guides:adrv9009-zu11eg:quick-start-guide [20 Aug 2021 09:13] – Update Michael Hennerich | ||
---|---|---|---|
Line 18: | Line 18: | ||
* A UART terminal (Putty/Tera Term/ | * A UART terminal (Putty/Tera Term/ | ||
+ | Please use the [[: | ||
- | ==== Pre-release SD Card Creation ==== | + | <hidden Older Bootfiles (Click |
- | + | ||
- | The project will be release as part of 2019_r1 release.Before then, the SD image for 2018_r2 can be used. | + | |
- | + | ||
- | ==== Writing the SD Card ==== | + | |
- | + | ||
- | Details on how to write the SD card can be found here: [[resources: | + | |
- | + | ||
- | ==== ADRV9009-ZU11EG Specific Boot Files ==== | + | |
- | + | ||
- | After writing the image, on the boot partition ADRV9009-ZU11EG specific files can be added from | + | |
- | + | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | </ | ||
- | |||
- | Copy: | ||
- | - BOOT.BIN | ||
- | - Image | ||
- | - system.dtb | ||
- | - uEnv.txt | ||
- | |||
- | -> To the root directory of the SD-Card FAT32 BOOT partition. | ||
===== Required Hardware ===== | ===== Required Hardware ===== |