Wiki

This version (14 Jun 2019 21:14) was approved by AdrianC.

Pre-release SD Card Creation

The project will be release as part of 2019_r1 release.Before then, the SD image for 2018_r2 can be used.

Writing the SD Card

Details on how to write the SD card can be found at https://wiki.analog.com/resources/tools-software/linux-software/zynq_images including the 2018_R2 image.

ADRV9009-ZU11EG Specific Boot Files

After writing the image, on the boot partition ADRV9009-ZU11EG specific files can be added from http://swdownloads.analog.com/cse/share/ADRV9009-ZU11EG-14-06-2019.zip .

Video Configuration

The default configuration for most of the projects is to use the HDMI output, but for this project the DisplayPort is used. In order for it to work, you should follow the steps described here: https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/software/linux/zynqmp#displayport_-_no_picture After following the steps, the board should be rebooted.

resources/eval/user-guides/adrv9009-zu11eg/pre-release.txt · Last modified: 14 Jun 2019 21:10 by AdrianC