This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:adrv9009-zu11eg:hardware [17 Sep 2021 16:01] – [Thermal Considerations] Claudia Goga | resources:eval:user-guides:adrv9009-zu11eg:hardware [24 May 2022 19:55] (current) – Brian OLoughlin | ||
---|---|---|---|
Line 2: | Line 2: | ||
- | {{: | + | {{: |
+ | |||
+ | |||
+ | The **ADRV9009-ZU11EG RF-SOM** package includes: | ||
+ | * ADRV9009-ZU11EG board with heat spreader plate mounted on top | ||
{{: | {{: | ||
---- | ---- | ||
Line 8: | Line 13: | ||
{{: | {{: | ||
---- | ---- | ||
+ | |||
==== Connector Interface ==== | ==== Connector Interface ==== | ||
The interface of the ADRV9009-ZU11EG consists of two SAMTEC SEARAY™ 400-pin female connectors P1 and P2. Following signals are present: | The interface of the ADRV9009-ZU11EG consists of two SAMTEC SEARAY™ 400-pin female connectors P1 and P2. Following signals are present: | ||
Line 40: | Line 46: | ||
<WRAP round download > | <WRAP round download > | ||
A detailed description of the connector interface for the complete system ADRV9009-ZU11EG and ADRV2CRR-FMC is located here: | A detailed description of the connector interface for the complete system ADRV9009-ZU11EG and ADRV2CRR-FMC is located here: | ||
- | {{ : | + | {{ : |
</ | </ | ||
---- | ---- | ||
Line 100: | Line 106: | ||
=== Programmable Logic GPIOs === | === Programmable Logic GPIOs === | ||
== High Performance GPIOs == | == High Performance GPIOs == | ||
- | Programmable logic high performance banks 65, 67 and 68 are fully accessible in connector P2. Prior of using these signals the bank supply VCCO must be provided, with a voltage between 0.95V and 1.9V. A reference voltage must be applied as well, if the IO standard requires one. To use the internal VREF voltage a 500 or 1K resistor needs to be connected from VREF pin to ground. | + | Programmable logic high performance banks 65, 67 and 68 are fully accessible in connector P2. Prior of using these signals the bank supply VCCO must be provided, with a voltage between 0.95V and 1.9V. A reference voltage must be applied as well, if the IO standard requires one. To use the internal VREF voltage a 500 or 1KOhm resistor needs to be connected from VREF pin to ground. |
== High Density GPIOs == | == High Density GPIOs == | ||
Programmable logic High density bank 89 is partially available in connector P2. Connect a voltage between 1.14V and 3.4V to the bank supply voltage VCCO_89. | Programmable logic High density bank 89 is partially available in connector P2. Connect a voltage between 1.14V and 3.4V to the bank supply voltage VCCO_89. | ||
Line 130: | Line 136: | ||
---- | ---- | ||
==== ADRV9009-ZU11EG RF-SOM Complete Prototyping System ==== | ==== ADRV9009-ZU11EG RF-SOM Complete Prototyping System ==== | ||
- | {{ : | + | {{ : |
---- | ---- | ||
==== Synchronizing multiple ADRV9009-ZU11EG RF-SOMs ==== | ==== Synchronizing multiple ADRV9009-ZU11EG RF-SOMs ==== | ||
Line 163: | Line 169: | ||
<note important> | <note important> | ||
- | Included in the ADRV9009-ZU11EG RF-SOM | + | The ADRV9009-ZU11EG RF-SOM |
- | The [[adi> | ||
- | For more information about overtemperature protection check the Power Monitoring Section on this page. | + | The heat spreader is designed to accommodate an active cooler with an AMD type SP3/ |
+ | |||
+ | |||
+ | The [[adi> | ||
---- | ---- | ||
+ | ==== Supplementary Testing ==== | ||
+ | |||
+ | <WRAP round download> | ||
+ | EMC testing has been carried out on the SOM. This may be useful as a reference for validation or qualification of custom designs. The report can be found here: | ||
+ | * {{: | ||
+ | |||
+ | </ | ||
+ | |||
+ | ---- | ||
+ | |||
==== Mechanical Reference Material ==== | ==== Mechanical Reference Material ==== | ||
<WRAP round download> | <WRAP round download> | ||
Line 190: | Line 209: | ||
---- | ---- | ||
==== ADRV9009-ZU11EG Schematics, BOM & Errata ==== | ==== ADRV9009-ZU11EG Schematics, BOM & Errata ==== | ||
- | Rev C is the latest | + | Rev C is the latest |
<WRAP round download> | <WRAP round download> | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{ : | ||
</ | </ | ||