This is an old revision of the document!
The ADRV2CRR-FMC is the carrier board to allow users evaluate the functionality of the ADRV9009-ZU11EG RF-SOM. It contains common high speed I/O ports to give flexibility in what connectivity option the user needs. It comes with a power supply that powers up the full system, heatsink that the user fits to the RFSOM heat spreader plate and necessary cables and adapters to get up and running.
Information on getting started and links to access the system software provided is contained on the main RF-SOM Wiki-page.
The ADRV2CRR-FMC has a single 12V supply input, distributed to the internal power supplies and interface connectors. Included in the package is a 12V, 145W power supply, which powers the complete prototyping platform built out of ADRV9009-ZU11EG, ADRV2CRR-FMC and AD-FMCOMMS8-EBZ. There are four LEDs that show the status of the power supplies: PG_ALL, PG_SOM, PWR_FAULT1 and PWR_FAULT2. A detailed description of these signals is available in the ADRV9009-ZU11EG RF-SOM Hardware Overview page.
Slide switches (S13 - S16) select the boot source of the Xilinx ZU11EG Ultrascale+.
The JTAG connector P7 is a 2×14 pin header intended to fit the Xilinx Platform Cable.
The interface to the ADRV9009-ZU11EG consists of two SAMTEC SEARAY™ 400-pin connectors (P12 and P14). For a detailed description of the signal interface visit the ADRV9009-ZU11EG RF-SOM Hardware Overview page.
The ADRV2CRR-FMC includes a standard ANSI/VITA 57.1 FMC high-pin count connector P1, which is partially populated. Following signals are present:
FMC HA and HB differential signals are not populated with user-defined digital IOs as specified in the FMC HPC standard. Instead, RF reference clock signals, synchronization signal, and ADRV9009 IOs are connected to these positions to enhance the capability of the P1 connector by providing the possibility:
IO expansion connector P25 is a 2.54mm pitch 2x10mm female connector that gives access to 12 single-ended (6 differential pairs) general purpose IOs, connected to high-performance ZU11EG PL bank 65. The expansion IOs are referenced to 1.8V. If other levels are needed voltage level translators need to be used.
PMOD connector P10, is a 2×6 pin, low-speed host interface, referenced to 3.3V.
The following table outlines levels of functionality provided in software for the I/O interfaces on the carrier board.
The Footprint is located here:
These are X-GRADE options.