Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:adrv9002:quickstart:zynq [25 Nov 2021 10:43] – [LVDS support] Laszlo Nagy | resources:eval:user-guides:adrv9002:quickstart:zynq [27 Jan 2023 08:34] (current) – Replaced the obsolete Kuiper Linux page link Joyce Velasco |
---|
According to [[https://www.xilinx.com/support/documentation/user_guides/ug471_7Series_SelectIO.pdf|7 Series Select IO guide]] section 'LVDS and LVDS_25' and Table 1-43 the LVDS I/O standard (VADJ 1.8V) is not supported on High Range banks. | According to [[https://www.xilinx.com/support/documentation/user_guides/ug471_7Series_SelectIO.pdf|7 Series Select IO guide]] section 'LVDS and LVDS_25' and Table 1-43 the LVDS I/O standard (VADJ 1.8V) is not supported on High Range banks. |
| |
Since the evaluation board can operate only with VADJ set to 1.8V and the FMC connector on the carrier (ZC706,Zedborad) is mapped to HR banks the **<fc #ff0000>LVDS interface is not supported</fc>**. | Since the evaluation board can operate only with <fc #ff0000>**VADJ set to 1.8V**</fc> and the FMC connector on the carrier (ZC706, Zedborad) is mapped to HR banks the **<fc #ff0000>LVDS interface is not supported</fc>**. |
| |
| |
===== Required Software ===== | ===== Required Software ===== |
| |
* SD Card 16GB imaged using the instructions here: [[resources:tools-software:linux-software:embedded_arm_images|SDCARD for Zynq & Altera SoC Quick Start Guide]]. Use 2020_r1 or newer release. (Pre-released files, built using Vivado 2020.1 can be downloaded from [[ https://swdownloads.analog.com/cse/prebuilt/zynq-zc706-adv7511-adrv9002-master-2021_05_13-08_13_21.zip|here]] ) | * SD Card 16GB imaged using the instructions here: [[:resources:tools-software/linux-software/kuiper-linux |
| |SDCARD for Zynq & Altera SoC Quick Start Guide]]. Use 2020_r1 or newer release. (Pre-released files, built using Vivado 2020.1 can be downloaded from [[ https://swdownloads.analog.com/cse/prebuilt/zynq-zc706-adv7511-adrv9002-master-2021_05_13-08_13_21.zip|here]] ) |
* Copy next boot files from ''zynq-zc706-adv7511-adrv9002'' directory directly on sdcard ''BOOT'' partition : | * Copy next boot files from ''zynq-zc706-adv7511-adrv9002'' directory directly on sdcard ''BOOT'' partition : |
* ''BOOT.bin'' | * ''BOOT.bin'' |