Wiki

This version is outdated by a newer approved version.DiffThis version (22 Feb 2024 02:23) was approved by Joyce Velasco.The Previously approved version (22 Feb 2024 01:43) is available.Diff

This is an old revision of the document!


ADMV96S-WGBE-EK1 Firmware User Guide

Evaluation

The evaluation kit comes with the MAX32650 preprogrammed with a firmware that is ready to use as-is. If you've gone through the hardware setup and you've connected at least the power and the Ethernet cables to the two boards of the setup, the firmware takes care of establishing and maintaining a wireless link automatically on power on.

How to find the firmware version?

Boot message

When a board is powered up or reset with the RESET button, the firmware starts executing and prints some messages over the serial port. You may access the serial port by connecting a MAXDAP to the JTAG SWD header and to the PC. To view the boot messages, open up a serial terminal application of your choice and configure it to listen to the serial port that appears in your system when you connect the MAXDAP to the PC (COMx on Windows, /dev/ttyACMx on Linux). The serial port settings must be 115200 baud, 8 databits, no parity bits, 1 stopbit, no flow control signals.

A typical boot message looks like this:

tags/wethlink-v1.0.0-7c98c2261 for revision B
Transceiver: admv9625
EEPROM: loading non-volatile parameters...
EEPROM: loaded non-volatile parameters.
Running IIOD server...
If successful, you may connect an IIO client application by:
1. Disconnecting the serial terminal you use to view this message.
2. Connecting the IIO client application using the serial backend configured as shown:
	Baudrate: 345600
	Data size: 8 bits
	Parity: none
	Stop bits: 1
	Flow control: none

The firmware version is thus v1.0.0, built using git commit 7c98c2261 for revision B hardware.

Using libiio from command line

The libiio (v0.25 or later) library setup also installs some useful command line tools such as iio_info which can connect to a remote iiod applciation and display information about it. In our case, the firmware is running an iiod application, as can be seen in the boot message, so we can query it over the serial port (replace /dev/ttyACM0 with COMn on Windows):

$ iio_info -u serial:/dev/ttyACM0,345600,8n1n 
iio_info version: 0.25 (git tag:v0.25)
Libiio version: 0.25 (git tag: v0.25) backends: local xml ip usb serial
IIO context created with serial backend.
Backend version: 1.1 (git tag: 0000000)
Backend description string: no-OS/projects/wethlink tags/wethlink-v1.0.0-7c98c2261
...

We can conclude that the on-board firmware is v1.0.0 built using git commit 7c98c2261.

Simply connect to the serial port of the device with the Wethlink GUI app and observe the Context tab content. 300

How to update the firmware ?

Drag and drop a .hex

To update to a newer firmware version (such as the latest release), download the .hex file onto the DAPLINK drive that is created when you plug in the programmer. While the file is being copied, you will see the MAXDAP device blinking. Once the programming is done, the device reconnects again to the PC as a DAPLINK drive. Check this newly attached DAPLINK drive for a FAIL.TXT file. If it doesn't exist, you have correctly programmed the board as in the following video:

If however, there is a FAIL.TXT file, if might be that the programmer isn't connected correctly or that the firmware of the programmer itself is not a firmware that can program a MAX32650 target. Here's how a failed programming looks like:

Is the MAXDAP firmware correct?

Is the MAXDAP firmware correct?

The MAXDAP itself needs to run a specific firmware version to be able to program the MAX32650 with Drag and Drop. The DETAILS.TXT file on the DAPLINK drive specifies the Git SHA of the running firmware:

Git SHA: 649f2a1524190c5f0ea32c97bb8682ad6fd772a0

If what you see on your device is not the one indicated above, please follow the instructions on this page to update the MAXDAP firmware first.

mcufla.sh

no-OS provides a standalone script that can be used to program .elf files to various targets, including the MAX32650. Typical usage and output is shown below:

$ wget https://raw.githubusercontent.com/analogdevicesinc/no-OS/master/tools/scripts/mcufla.sh
$ chmod +x ./mcufla.sh
$ ./mcufla.sh ~/Work/no-OS/projects/wethlink/build/wethlink.elf
Maxim platform detected
Running cmd: /home/dari/.mcuflash/maxim/openocd/src/openocd -s /home/dari/.mcuflash/maxim/openocd/tcl -c 'adapter driver cmsis-dap; transport select swd; ' -f target/max32650.cfg -c 'program /home/dari/Work/no-OS/projects/wethlink/build/wethlink.elf verify reset exit'
Open On-Chip Debugger 0.11.0+dev-g56a818e4c (2023-10-24-15:55)
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
swd
Info : CMSIS-DAP: SWD  supported
Info : CMSIS-DAP: Atomic commands supported
Info : CMSIS-DAP: Test domain timer supported
Info : CMSIS-DAP: FW Version = 2.1.0
Info : CMSIS-DAP: Serial# = 042517028fbd037a00000000000000000000000097969906
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 2000 kHz
Info : SWD DPIDR 0x2ba01477
Info : max32xxx.cpu: Cortex-M4 r0p1 processor detected
Info : max32xxx.cpu: target has 6 breakpoints, 4 watchpoints
Info : max32xxx.cpu: external reset detected
Info : starting gdb server for max32xxx.cpu on 3333
Info : Listening on port 3333 for gdb connections
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x00000184 msp: 0x2000b300
** Programming Started **
** Programming Finished **
** Verify Started **
** Verified OK **
** Resetting Target **
shutdown command invoked

make run

This method involves installing the toolchain for building the projects/wethlink project and uploading the generated binary to the target with make run.

Hardware revision must be specified when building the wethlink project, otherwise the build errors out. make HW_VERSION=0 builds for rev A hardware, and make HW_VERSION=1 builds for rev B hardware.

No-OS Build Guide

NOTE: This build guide is valid for the projects found in the no-OS/projects folder. If your project resides elsewhere under the no-OS repository tree, it is a legacy project. A build guide for legacy projects can be found Build no-OS with GNU make.

Clone NO-OS with the --recursive flag:

git clone --recursive https://github.com/analogdevicesinc/no-OS

If however you've already cloned NO-OS without the --recursive flag, you may initialize all the submodules in an existing NO-OS clone with:

git submodule update --recursive --init
Build Prerequisites

Prior to building a no-OS project, it is required to set up some environment variables so that the build process may find the necessary tools (compiler, linker, SDK etc.).

Use the following commands to prepare your environment for building no-OS projects:

Linux (Click to expand)

Linux (Click to expand)

Make sure the GNU Make version you are using is >= 4.2.

Intel (Click to expand)

Intel (Click to expand)

Assuming the SDK is installed at this path:

/path/to/intel
└── intelFPGA
    └── 18.1

Run:

$ source no-OS/tools/scripts/platform/intel/environment.sh /path/to/intel/intelFPGA 18.1

Xilinx (Click to expand)

Xilinx (Click to expand)

Assuming the Vitis 2022.2 is installed at this path:

/path/to/xilinx
├── DocNav
├── Downloads
└── Vitis
    └── 2022.2

Run:

$ source /path/to/xilinx/Vitis/2022.2/settings64.sh

STM32 (Click to expand)

STM32 (Click to expand)

  • Install stm32cubeide to default location /opt/stm32cubeide. If you'd rather install it at a different location, run export STM32CUBEIDE=/path/to/your/stm32cubeide in the terminal used for building.
  • Install stm32cubemx to default location /opt/stm32cubemx. If you'd rather install it at a different location, run export STM32CUBEMX=/path/to/your/stm32cubemx in the terminal used for building.
  • Currently we are testing projects with CubeMx Version 6.5.0, but other versions should work as well.
  • Install java (openjdk-17), sed and head (if not already present, they normally are).
  • Install python (if not already present) and make sure python command executes Python3 (not Python2). This can be easily achieved by running the following command sudo apt install python-is-python3.

Maxim (Click to expand)

Maxim (Click to expand)

  • Install the Maxim Micros SDK.
  • Set the MAXIM_LIBRARIES environment variable to the MaximSDK/Libraries path (the default should be ~/MaximSDK/Libraries).
  • For visual debugging and building, install Visual Studio Code, and the Cortex-Debug extension.

Mbed (Click to expand)

Mbed (Click to expand)

  • Install Mbed CLI 1 as per guide here: https://os.mbed.com/docs/mbed-os/v6.15/build-tools/install-and-set-up.html .Usually the following steps should be sufficient: sudo apt install python3 python3-pip git mercurial gcc-arm-none-eabi and sudo python3 -m pip install mbed-cli pyelftools==0.29.
  • Configure the compiler location with Mbed CLI. This can be carried out by running the “mbed config -G GCC_ARM_PATH “path-to-your-gcc-compiler”” in Command Prompt.

Pico (Click to expand)

Pico (Click to expand)

  • Set the PICO_SDK_PATH environment variable to the pico-sdk cloned repository path.
  • Install the J-Link software
  • Set the JLINK_SERVER_PATH environment variable to the JLinkGDBServerCLExe path (the default path should be /opt/SEGGER/JLink/JLinkGDBServerCLExe).
  • For visual debugging and building, install Visual Studio Code, and the Cortex-Debug extension.

ADuCM3029 (Click to expand)

ADuCM3029 (Click to expand)

Please install all the necessary packs locally and then manually import them in CrossCore

Common Issues with environment setup:

  • Makefiles searches for the CCES_HOME in its default installation directory. It may happen that multiple version are installed and may not work. To select a CCES_HOME run export CCES_HOME=/opt/analog/cces/2.10.0

Windows (Click to expand)

Windows (Click to expand)

Open up a Git Bash as Administrator once and run the tools/scripts/git-bash.sh script. Close the window. You only need to do this once per Git Bash installation.
Use Git Bash (unelevated) for the rest of your development.

Xilinx (Click to expand)

Xilinx (Click to expand)

Assuming the Vitis 2022.2 is installed at this path:

C:\Xilinx
├── DocNav
├── Downloads
└── Vitis
    └── 2022.2

Run:

$ export PATH=/c/Xilinx/Vitis/2022.2/bin:/c/Xilinx/Vitis/2022.2/gnu/aarch64/nt/aarch64-none/bin/:$PATH

Maxim (Click to expand)

Maxim (Click to expand)

  • Install the Maxim Micros SDK to a path without whitespaces like C:\MaximSDK.
  • Set the MAXIM_LIBRARIES environment variable by running: export MAXIM_LIBRARIES=/c/MaximSDK/Libraries.
  • (Optional) For visual debugging and building, install Visual Studio Code, and the Cortex-Debug extension.

ADuCM3029 (Click to expand)

ADuCM3029 (Click to expand)

Building a project

Go in the project directory that should be built.

Linux (Click to expand)

Linux (Click to expand)

$ cd no-OS/projects/project_name/
$ tree
.
├── builds.json
├── Makefile
├── src
└── src.mk

Intel (Click to expand)

Intel (Click to expand)

Copy the .sof and .sopcinfo to the project folder.

$ ls
Makefile  profiles  src  src.mk  system_bd.sopcinfo  adrv9009_a10gx.sof	
$ make

# Alternatively you may select a .sopcinfo file explicitly by:
$ make HARDWARE=path/to/system_bd.sopcinfo

Xilinx (Click to expand)

Xilinx (Click to expand)

Copy the .xsa in the project folder.

$ ls
Makefile  profiles  src  src.mk system_top.xsa
$ make

# Alternatively you may select an .xsa file explicitly by:
$ make HARDWARE=path/to/file.xsa

Maxim (Click to expand)

Maxim (Click to expand)

To build a project, type:

make PLATFORM=maxim TARGET=...

The TARGET specifies the chip for which the project is built. If it is missing, max32660 will be used. At the moment, the available targets are: max32650, max32655, max32660, max32665, max32670, max32690 and max78000.

Mbed (Click to expand)

Mbed (Click to expand)

To build a project, type:

make PLATFORM=mbed

Pico (Click to expand)

Pico (Click to expand)

To build a project, type:

make PLATFORM=pico

STM32 (Click to expand)

STM32 (Click to expand)

Make sure you have the .ioc file in the project directory, then type:

$ make PLATFORM=stm32

If during the project generation you get a dialog saying that you are using an .ioc file generated with an old CubeMX version, click Continue. Migrate is also a valid option but only if you know what you are doing.

If you're trying to use an .ioc file generated with a newer CubeMX than the one installed on your machine, you will get a prompt that asks you to upgrade your installation to the new version, there is no other choice than to click OK and then manually upgrade.

ADuCM3029 (Click to expand)

ADuCM3029 (Click to expand)

The ADuCM3029 projects also contain a pinmux_config.c file which contains pin configuration instructions.

# build an ADuCM3029-only project
$ make

# if the platform autodetection picks the wrong platform, explicitly specify the PLATFORM
$ make PLATFORM=aducm3029

Windows (Click to expand)

Windows (Click to expand)

Use Git Bash to run these commands.
$ cd no-OS/projects/project_name

It should contain make-related files and source files:

./no-OS/projects/project_name
├── builds.json
├── Makefile
├── src
└── src.mk

Xilinx (Click to expand)

Xilinx (Click to expand)

Copy the .xsa to the project folder and run:

./no-OS/projects/adrv9009
├── Makefile
├── profiles
├── src
├── src.mk
└── system_top.xsa

$ make

Maxim (Click to expand)

Maxim (Click to expand)

To build a project, type:

$ make PLATFORM=maxim TARGET=...

The TARGET specifies the chip for which the project is built. If it is missing, max32660 will be used. At the moment, the available targets are: max32650, max32655, max32660, max32665, max32670, max32690 and max78000.

ADuCM3029 (Click to expand)

ADuCM3029 (Click to expand)

$ export PLATFORM=aducm3029
$ make

The build process creates a build directory in the project folder:

build
├── app
├── bsp
├── obj
├── project_name.elf
└── tmp
Running/Debugging

Once the .elf, .hex or .bin file has been generated, make sure the board is powered on, JTAG cable connected and use the following commands to upload the program to the board or debug.

Uploading the binary to target is generically achieved with:

$ make run

Xilinx (Click to expand)

Xilinx (Click to expand)

For Xilinx project you can flash the board connected to a remote host. On the remote host make sure to start `hw_server`. On your development environment run

$ export XSCT_REMOTE_HOST=<remote host ip>
$ export XSCT_REMOTE_PORT=<remote host hw_server port>
$ make run

By default the `hw_server` port should be 3121.

Use the following command to launch the SDK associated to the used platform in order to be able to debug graphically by clicking the debug button:

$ make sdkopen

Fore more details about the available make rules, check out this page.

Running/Debugging in WSL

17 Mar 2021 10:27 · Darius B

Theory of Operation

The firmware uses many no-OS modules for accessing the various peripherals it needs for this project. The diagram below shows how these modules interact with the hardware and with each other. Of particular interest is the feedback loop from the embedded ADC that is periodically used to sample TX_DET and RX_DET at 1 Hz (provided by the embedded RTC) to the no_os_pid P.I.D. controller which computes a new set of gain values that are written back into the transceiver. This feedback loop is the core functionality of this system and it ensures that the wireless link operates with optimum gains at any distance that the ADMV9615 and ADMV9625 are set apart.

A detailed view of this feedback loop is represented below, showing exactly what gains the feedback loop controls:

The firmware can also interact with a PC application over the serial line (UART). Upon boot, it prints boot messages at 115200 baudrate, then launches an iiod application that can be accessed from a PC using libiio over a serial backend at 345600 baudrate. The following existing PC applications may be used to interact with the firmware:

  1. iio_info, iio_attr (command-line tools from ''libiio'')

The fact that the firmware exposes the on-board devices as iio devices in a standardized way means that it is easy to devise new applications that can interact with the firmware by simply using the libiio library.

IIO devices

You can see all the iio devices and their channels and attributes below, as obtained with iio_info:

$ iio_info -u serial:/dev/ttyACM0,345600,8n1n 
iio_info version: 0.25 (git tag:v0.25)
Libiio version: 0.25 (git tag: v0.25) backends: local xml ip usb serial
IIO context created with serial backend.
Backend version: 1.1 (git tag: 0000000)
Backend description string: no-OS/projects/wethlink tags/wethlink-v1.0.0-rc1-7c98c2261
IIO context has 9 attributes:
	hw_model: admv9625
	hw_version: b
	hw_serial: serial
	carrier_model: model
	carrier_version: b
	carrier_serial: serial
	uri: serial:/dev/ttyACM0,345600,8n1n
	serial,port: /dev/ttyACM0
	serial,description: DAPLink CMSIS-DAP - 042517028fbd037a00000000000000000000000097969906
IIO context has 6 devices:
	iio:device0: hmc6300
		1 channels found:
			temp:  (input)
			1 channel-specific attributes found:
				attr  0: raw value: 15
		8 device-specific attributes found:
				attr  0: enabled value: 1
				attr  1: vco value: 59850000
				attr  2: vco_available value: 55125000 55387500 55650000 55912500 56175000 56437500 56700000 56962500 57225000 57487500 57750000 58012500 58275000 58537500 58800000 59062500 59325000 59587500 59850000 60112500 60375000 60637500 60900000 61162500 61425000 61687500 61950000 62212500 62475000 62737500 63000000 63262500 63525000 63787500 64050000 64312500 64575000 64837500 65100000 65362500 65625000 65887500 66150000 
				attr  3: vco_band value: 8
				attr  4: vco_lock value: 1
				attr  5: if_attn value: 15
				attr  6: temp_en value: 1
				attr  7: rf_attn value: 9
		1 debug attributes found:
				debug attr  0: direct_reg_access value: 0
		No trigger on this device
	iio:device1: hmc6301
		1 channels found:
			temp:  (input)
			1 channel-specific attributes found:
				attr  0: raw value: 15
		14 device-specific attributes found:
				attr  0: enabled value: 1
				attr  1: vco value: 63262500
				attr  2: vco_available value: 55125000 55387500 55650000 55912500 56175000 56437500 56700000 56962500 57225000 57487500 57750000 58012500 58275000 58537500 58800000 59062500 59325000 59587500 59850000 60112500 60375000 60637500 60900000 61162500 61425000 61687500 61950000 62212500 62475000 62737500 63000000 63262500 63525000 63787500 64050000 64312500 64575000 64837500 65100000 65362500 65625000 65887500 66150000 
				attr  3: vco_band value: 15
				attr  4: vco_lock value: 1
				attr  5: if_attn value: 6
				attr  6: temp_en value: 1
				attr  7: rf_lna_gain value: 1
				attr  8: bb_attn1 value: 0
				attr  9: bb_attn2 value: 0
				attr 10: bb_attni_fine value: 0
				attr 11: bb_attnq_fine value: 0
				attr 12: bb_lpc value: 0
				attr 13: bb_hpc value: 0
		1 debug attributes found:
				debug attr  0: direct_reg_access value: 0
		No trigger on this device
	iio:device2: mwc
		2 channels found:
			voltage0: tx_det (input)
			2 channel-specific attributes found:
				attr  0: raw value: 257
				attr  1: scale value: 1.191406250
			voltage1: rx_det (input)
			2 channel-specific attributes found:
				attr  0: raw value: 596
				attr  1: scale value: 2.978515625
		10 device-specific attributes found:
				attr  0: tx_autotuning value: 1
				attr  1: tx_target value: 350
				attr  2: tx_tolerance value: 50
				attr  3: rx_autotuning value: 1
				attr  4: rx_target value: 1950
				attr  5: rx_tolerance value: 50
				attr  6: tx_auto_ifvga value: 1
				attr  7: rx_auto_ifvga_rflna value: 1
				attr  8: reset value: 0
				attr  9: save value: 0
		1 debug attributes found:
				debug attr  0: direct_reg_access value: 1
		No trigger on this device
	iio:device3: adin1300
		0 channels found:
		3 device-specific attributes found:
				attr  0: link value: 0
				attr  1: speed value: 6
				attr  2: autonegotiate value: 1
		1 debug attributes found:
				debug attr  0: direct_reg_access value: 4416
		No trigger on this device
	iio:device4: max24287
		0 channels found:
		3 device-specific attributes found:
				attr  0: par_speed value: 5
				attr  1: ser_link value: 1
				attr  2: ser_speed value: 5
		1 debug attributes found:
				debug attr  0: direct_reg_access value: 0
		No trigger on this device
	iio:device5: adm1177 (buffer capable)
		2 channels found:
			voltage0:  (input, index: 0, format: le:u12/32>>0)
			2 channel-specific attributes found:
				attr  0: raw value: 1901
				attr  1: scale value: 6.433105468
			current0:  (input, index: 1, format: le:u12/32>>0)
			2 channel-specific attributes found:
				attr  0: raw value: 358
				attr  1: scale value: 1.033593750
		No trigger on this device

The context contains information that is provisioned at manufacturing such as serial number, hardware revision etc. or information produced during the build process such as the firmware version. The ADMV9615 or ADMV9625 DIP switch state is also exposed as a context attribute and the firmware makes certain decisions based on it.

There are 6 exposed devices:

  1. hmc6300 - the transmitter or the ADMV96x5 module
  2. hmc6301- the receiver of the ADMV96x5 module
  3. mwc - this device exposes attributes and channels that are specific to this project, such as the tx_det and rx_det ADC channels, attributes to enable/disable automatic gain control, attributes to write settings to non-volatile memory etc. (read “mwc” as “microwave connector”)
  4. adin1300 - the Ethernet PHY
  5. max24287 - the RGMII to SGMII Serializer/Deserializer
  6. adm1177 - the input power monitor

LED

Each ADMV96S-WGBE-EK reference design board has a few LED's to convey information from the firmware to the user.

The blue LED is a power good LED and it only lights up if the input power is a clean 12V.

The 4 LED series at the top of the board convey the following information:

RX TX
DET_OUT RX_LOCK DET_OUT TX_LOCK
Lit (green or red) when RX autotuning is on, otherwise not lit. Green when RX_DET is within tolerance of the target. Red when RX_DET is not within tolerance of the target. Lit when RX VCO has locked. Lit (green or red) when TX autotuning is on, otherwise not lit. Green when TX_DET is within tolerance of the target. Red when TX_DET is not within tolerance of the target. Lit when TX VCO has locked.

The following examples shows a board that has TX and RX VCO's locked, TX and RX autotuning on, TX_DET within tolerance of target but the firmware can't keep RX_DET within tolerance of target. To force this error, one of the boards facing each other was unplugged so the photographed board was trying to maximize the RX gains to receive something meaningful. But if there is no incoming signal, gain changes cannot possibly affect RX_DET so the firmware lights up the LED in red.

The RJ-45 connector also has embedded LED's. The top left one lights up green when the ADIN1300 has connected to another PHY over the Ethernet cable. This LED is briefly turned off when there is activity on the Ethernet cable essentially blinking it. So a blinking top left LED means both the Ethernet link is up and there is ongoing activity. The top right LED conveys link speed information and is turned off when link speed is 10 Mbps, lit green for 100 Mbps and lit amber when speed is 1000 Mbps.

EEPROM

The 24LC32A EEPROM has 32Kb memory capacity (4 KB) and is connected to an I2C bus. The firmware uses the EEPROM to store non-volatile parameters to be loaded at boot.

In order not to waste space, and to make sure future iterations of the firmware may use areas of the EEPROM that are currently unused, a design decision had to be made from the start, as to what size a non-volatile parameter set should have. A reasonable size of 256 bytes was chosen, which makes it possible to fit 16 such parameter sets into the memory.

Address Name Size
0x0 NVMP1 256
0x100 Reserved 3584
0xF00 Factory defaults 256

Two such areas are currently used by the firmware, one is the NVMP1 area which is the active configuration loaded at boot and the other one is the factory defaults configuration which can be copied into the active configuration with a certain procedure.

The 0x100 to 0x3FF memory area is not used.

Each NVMP area has 255 bytes of actual parameters and 1 last byte consisting of a CRC8 computed over the leading 255 bytes.

The CRC8 checksums are checked at boot and if they have been incorrectly written or tampered with, the parameters are not used. If no suitable parameters are found in NVMP1 or in the factory defaults area, a set of in-firmware hardcoded parameters are used for the boot.

Resetting to factory defaults

To explicitly reset to factory defaults, click the S3 button, keep it pressed and click the S2 button briefly. The four LED's will blink 10 times for about 3 seconds to confirm the reset to factory defaults has completed.

Production firmware and provisioning

There are two versions of the firmware that are for normal and production use.

The normal firmware is the one that runs on the hardware, provided the hardware had gone through the production process fully. The production process has 3 main steps: actual hardware production, provisioning and testing.

The production firmware is a variant that has the following extra features:

  • It disregards whatever is in the EEPROM and loads up with hardcoded parameters.
  • It allows writing of the factory defaults area of the EEPROM by exposing the mwc.save_defaults attribute.
  • It allows provisioning by allowing the change of the serial number (mwc.hw_serial, mwc.carrier_serial), revision (mwc.hw_version, mwc.carrier_version) and model name (mwc.carrier_model) which all default to - when the device is not provisioned.

With a normal firmware, the device will not behave correctly if it was not provisioned. The firmware needs valid parameters to operate correctly so having - being displayed as carrier serial number is an indicator that the device hasn't somehow gone through the full production cycle that performs provisioning.

Autonegotiation

The EVAL-ADMV96S-WGBE-EK1 is a system composed of two independent boards that connect to the outside world through Ethernet. The network infrastructure at the other end of the Ethernet cable is not known yet the system can detect its capabilities in terms of data bandwidth and dulplex mode due to autonegotiation signaling at physical layer (OSI model).

The system may be connected at any time to devices on a network that have different capabilities. The device at one end could be able to talk 100 Mbps half-duplex, the one at the other end could be capable of 1 Gbps full-duplex. In this scenario, the system needs to adapt for the weakest link and configure the 100 Mbps half-duplex speed at all levels, it's the common denominator that allows the two devices to talk to each other.

Having two independent devices in a system, each running its own firmware, this could only be possible if there is some mechanism through which the devices could advertise speeds to one another. The wireless link carries SGMII interface and the SGMII itself has an autonegotiation mechanism through which a frame containing speed and duplex information can be passed on from one device to the other. The firmware uses this feature to propagate an Ethernet link speed change throughout the whole system.

Steps 1-4 are executed in an interrupt service routine from the PHY when link status changes.

Steps 5-6 are executed in an interrupt service routine from the SERDES when new autonegotiation page was received.

To resume this section:

  • there is speed and duplex mode autonegotiation at Ethernet level
  • there is speed and duplex mode autonegotiation at SGMII level
  • the lowest advertised speed of a device in the system is propagated and the system subsequently works at that speed

Temperature compensated gains

Due to reasons related to the transceiver hardware, the optimum gains at which it operates are temperature dependent. Affected gains are TX IF VGA, RX IF VGA and RX RF LNA. The optimum gains found through lab characterization are provided by Analog Devices.

The transceivers have a very coarse temperature sensor that is used by the firmware to look up gains in a lookup table. The default behavior of the firmware is to auto compensate gains for temperature using the factory default lookup tables.

You can disable auto compensation by unticking the checkbox, or you can keep it and adjust the tables to your liking.

TX temperature compensation table:

RX temperature compensation table:

Raw Temp Range
1 -40°C … -25°C
3 -25°C … 10°C
7 10°C … 40°C
15 40°C … 75°C
31 > 75°C

P.I.D. controlled gains

TX_DET and RX_DET analog signals of the transceivers are sampled regularly by the embedded ADC of the microcontroller. They correspond to the TX and RX signal power and need to be kept in a certain sweetspot for proper operation of the wireless link.

The remaining gains, that aren't temperature controlled, are the TX RF VGA and the RX BB (COARSE1, COARSE2 and FINE). By controlling these gains up and down, one can see a change in the RX and RX power detectors.

So we have a feedback loop and we can apply control theory on it in the form of a P.I.D. algorithm to keep the TX_DET and RX_DET in the sweetspot by having the algorithm tweak the gains. The implementation actually only uses the proportional and integral coefficients, essentially making this a P.I. control.

Every second the algorithm is run for several iterations until it settles on a resulting gain. There are two challenges:

  1. Make it settle fast! We don't care too much about overshoot, we care about settling fast because the algorithm is run on the main loop along with other things and we don't want to block for too long.
  2. Make it settle with as little gain changes as possible! Any gain change will momentarily mess with the signals being sent in that instant across the wireless link, so by minimizing the gain changes, we minimize the bit error rate throughout the whole system.

To illustrate how the algorithm works, here's the result of a simulation with artificial perturbations at samples 100, 200, 300 and 400 in order to observe the characteristics of the control. The top part shows the output of the P.I. as an attenuation in steps between 0 and 31. The bottom part is a simulated RX_DET (mV) based on what attenuation the algorithm previously set.

With the factory default settings, the algorithm finds the target within 10 iterations or less and does it with few gain changes addressing both of the above points. As with any P.I.D. algorithm, it's possible that better behavior is achievable by experimentally fine tuning the coefficients but with the factory default coefficients and initial release implementation, the system achieves a bit error rate of less than 10E-10 for constant distance and across the whole -40°C to 80°C.

resources/eval/user-guides/admv96s-wgbe-ek1/firmware/setup.1708565026.txt.gz · Last modified: 22 Feb 2024 02:23 by Joyce Velasco