This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:adin1300-and-adin1200:ksz8081_to_adin1200_phy_exchange_guide [17 Oct 2021 21:21] – cr Catherine Redmond | resources:eval:user-guides:adin1300-and-adin1200:ksz8081_to_adin1200_phy_exchange_guide [17 Oct 2021 21:28] – cr Catherine Redmond | ||
---|---|---|---|
Line 131: | Line 131: | ||
---- | ---- | ||
+ | |||
<WRAP group> | <WRAP group> | ||
<WRAP half column> | <WRAP half column> | ||
+ | |||
+ | |||
===== Hardware Configuration ===== | ===== Hardware Configuration ===== | ||
Line 178: | Line 181: | ||
</ | </ | ||
+ | <WRAP center round important 60%> | ||
+ | Strapping configurations are very specific to the device, consult the respective datasheets to determine the exact configuration for required use case. | ||
+ | </ | ||
---- | ---- | ||
Line 196: | Line 201: | ||
==== RGMII ==== | ==== RGMII ==== | ||
- | The ADIN1200 also supports RGMII MAC interface mode. | + | The ADIN1200 also supports RGMII MAC interface mode. |
</ | </ | ||
Line 209: | Line 214: | ||
The ADIN1200 has a Linux Driver available in the Linux mainline kernel. The ADIN1200 linux driver detail is captured here: | The ADIN1200 has a Linux Driver available in the Linux mainline kernel. The ADIN1200 linux driver detail is captured here: | ||
https:// | https:// | ||
+ | |||
</ | </ | ||
</ | </ | ||
+ | <note tip>The ADIN1200 has a Linux Driver available in the Linux mainline kernel.</ | ||
+ | |||
---- | ---- | ||
Line 232: | Line 240: | ||
The following example captures how to configure the ADIN1200 for an unmanaged configuration with RMII Interface, operating in Auto-negotiation mode advertising all speeds. The PHY will power up in this state, ready to establish a link with a link partner. | The following example captures how to configure the ADIN1200 for an unmanaged configuration with RMII Interface, operating in Auto-negotiation mode advertising all speeds. The PHY will power up in this state, ready to establish a link with a link partner. | ||
The MAC interface configuration pins (MACIF_SEL0/ | The MAC interface configuration pins (MACIF_SEL0/ | ||
+ | |||
The following list summarizes an RMII auto negotiate, 10 Mbps or 100 Mbps full duplex or half duplex: | The following list summarizes an RMII auto negotiate, 10 Mbps or 100 Mbps full duplex or half duplex: | ||
* MAC Interface = RMII | * MAC Interface = RMII |