This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:adin1300-and-adin1200:dp83867_to_adin1300_phy_exchange_guide [07 Jan 2022 15:23] Mark Bolger Formatting changed for even pages |
resources:eval:user-guides:adin1300-and-adin1200:dp83867_to_adin1300_phy_exchange_guide [05 Apr 2022 11:02] Mark Bolger Table 4 Updated |
||
---|---|---|---|
Line 104: | Line 104: | ||
The ADIN1300 supports RGMII, MII and RMII MAC interface modes. The following sections describe the RGMII, MII and RMII interfaces for both devices. | The ADIN1300 supports RGMII, MII and RMII MAC interface modes. The following sections describe the RGMII, MII and RMII interfaces for both devices. | ||
+ | |||
=== RGMII Interface === | === RGMII Interface === | ||
Line 109: | Line 110: | ||
Both devices support the internal delay on the clocks. By default, the ADIN1300 is configured in RGMII mode with a 2 ns delay on RXC and TXC. | Both devices support the internal delay on the clocks. By default, the ADIN1300 is configured in RGMII mode with a 2 ns delay on RXC and TXC. | ||
- | {{:resources:eval:user-guides:adin1300-and-adin1200:table4_rgmii_mc_interface_pin_mode_comparison_dp83867.png|}} | + | {{:resources:eval:user-guides:adin1300-and-adin1200:table4_rgmii_mac_interface_pin_mode_comparison_dp83867.png|}} |
=== MII Interface === | === MII Interface === |