Wiki

This version is outdated by a newer approved version.DiffThis version (18 Dec 2019 16:27) was approved by Micheál Lambe.

This is an old revision of the document!


ADE120x Supplemental User Guide

The ADE120x is an isolated binary input monitor. It performs an isolated measurement of a binary input voltage and communicates the status of this input to low voltage processors or logic circuits. The ADE120x application circuit can accept a wide range of binary input voltages from 10 V to 300 V scaled using a resistor divider before applying the voltage to the pins. This content applies to both ADE1201 and ADE1202.

resources/eval/user-guides/ade120x.1576098248.txt.gz · Last modified: 11 Dec 2019 22:04 by Meghan Kaiserman