The ADE120x is an isolated binary input monitor. It performs an isolated measurement of a binary input voltage and communicates the status of this input to low voltage processors or logic circuits. The ADE120x application circuit can accept a wide range of binary input voltages from 10 V to 300 V scaled using a resistor divider before applying the voltage to the pins. This content applies to both ADE1201 and ADE1202.