This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:adbt1000 [10 Nov 2021 10:18] Frances de la Rama [Bill of Materials] |
resources:eval:user-guides:adbt1000 [17 Nov 2021 01:38] Frances de la Rama Figure 5 Edit |
||
---|---|---|---|
Line 52: | Line 52: | ||
- Connect the Device Under Test (electronic load or battery) to connector P5 on the switching power module. {{ :resources:eval:user-guides:adbt1000_two_wire_load_connection.jpg?300 |2-wire Battery Connection}} <WRAP centeralign> //Figure 3. 2-wire Battery Connection//</WRAP> | - Connect the Device Under Test (electronic load or battery) to connector P5 on the switching power module. {{ :resources:eval:user-guides:adbt1000_two_wire_load_connection.jpg?300 |2-wire Battery Connection}} <WRAP centeralign> //Figure 3. 2-wire Battery Connection//</WRAP> | ||
- Connect the SDP-S controller to the System Control Board. {{ :resources:eval:user-guides:adbt1000_sdp_s_connection.jpg?300 | SDP-S Connection}} <WRAP centeralign> //Figure 4. SDP-S Connection//</WRAP> | - Connect the SDP-S controller to the System Control Board. {{ :resources:eval:user-guides:adbt1000_sdp_s_connection.jpg?300 | SDP-S Connection}} <WRAP centeralign> //Figure 4. SDP-S Connection//</WRAP> | ||
- | - Connect power supplies of +/-15V to P5 of the system control board for the Auxiliary Power Input. {{ :resources:eval:user-guides:adbt1000_sdp_s_connection.jpg?300 |}} <WRAP centeralign> //Figure 5. Auxiliary Power Supply Connection//</WRAP> | + | - Connect power supplies of +/-15V to P5 of the system control board for the Auxiliary Power Input. {{ :resources:eval:user-guides:adbt1000_auxiliary_power_supply_connection.jpg?300 |}} <WRAP centeralign> //Figure 5. Auxiliary Power Supply Connection//</WRAP> |
- Connect power supplies for the DC bus voltage to P2 of the system control board. Connect an electronic load in parallel. Set the electronic load to CV mode at a level about 200mV above the DC bus voltage. {{ :resources:eval:user-guides:dc_bus_connection.jpg?300 | DC Bus Connection}} <WRAP centeralign> //Figure 6. DC Bus Connection//</WRAP> | - Connect power supplies for the DC bus voltage to P2 of the system control board. Connect an electronic load in parallel. Set the electronic load to CV mode at a level about 200mV above the DC bus voltage. {{ :resources:eval:user-guides:dc_bus_connection.jpg?300 | DC Bus Connection}} <WRAP centeralign> //Figure 6. DC Bus Connection//</WRAP> | ||
- Turn on Auxiliary power, then DC bus voltage, then electronic load at DC bus. | - Turn on Auxiliary power, then DC bus voltage, then electronic load at DC bus. |