Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:adar2001-evalz [15 Jul 2020 17:29] – [Mutliplier Block Setup] Weston Sapiaresources:eval:user-guides:adar2001-evalz [16 Jul 2020 17:35] (current) – [RELATED PARTS] Weston Sapia
Line 7: Line 7:
 The [[adi>adar2001|ADAR2001]] has two integrated state machines, one for the Multiplier section and another for the Transmitter section. The sequencers are configured through the SPI, and can be used to quickly cycle through pre-programmed states. These sequencers can be exercised in one of two ways: The [[adi>adar2001|ADAR2001]] has two integrated state machines, one for the Multiplier section and another for the Transmitter section. The sequencers are configured through the SPI, and can be used to quickly cycle through pre-programmed states. These sequencers can be exercised in one of two ways:
   - External Advance and Reset Pins:   - External Advance and Reset Pins:
-      * TxADV - Transmitter Advance (Pin 8) +    * TxADV - Transmitter Advance (Pin 8) 
-      * TxRST - Transmitter Reset (Pin 9) +    * TxRST - Transmitter Reset (Pin 9) 
-      * MADV - Multiplier Advance (Pin 10) +    * MADV - Multiplier Advance (Pin 10) 
-      * MRST - Multiplier Reset (Pin 11)+    * MRST - Multiplier Reset (Pin 11)
   - SPI writes to the SEQUENCER_CTRL_SPI register (0x44)   - SPI writes to the SEQUENCER_CTRL_SPI register (0x44)
 \\  \\ 
 {{ :resources:eval:user-guides:adar2001:1_adar2001_board.png?direct&500 | ADAR2001-EVALZ Board}} {{ :resources:eval:user-guides:adar2001:1_adar2001_board.png?direct&500 | ADAR2001-EVALZ Board}}
 <WRAP centeralign>**//Figure 1: ADAR2001-EVALZ Board//**</WRAP> <WRAP centeralign>**//Figure 1: ADAR2001-EVALZ Board//**</WRAP>
-\\ \\ +\\  
 +---- 
 +====== RELATED PARTS ====== 
 +=== ADAR2004: 10GHz to 40GHz 4-Channel Rx Mixer With 4x LO === 
 +  * [[adi>adar2004|ADAR2004 Product page]] 
 +  * [[/resources/eval/user-guides/adar2004-evalz|ADAR2004-EVALZ Wiki]] 
 +=== AD9083: 16-Channel, 100MHz Bandwidth, JESD204B Analog-to-Digital Converter === 
 +  * [[adi>ad9083|AD9083 Product page]] 
 +=== ADF5610: Microwave Wideband Synthesizer with Integrated VCO === 
 +  * [[adi>adf5610|ADF5610 Product page]] 
 ---- ----
 ====== REQUIREMENTS ====== ====== REQUIREMENTS ======
resources/eval/user-guides/adar2001-evalz.txt · Last modified: 16 Jul 2020 17:35 by Weston Sapia