Wiki

This version is outdated by a newer approved version.DiffThis version (10 Feb 2023 10:36) was approved by Dragos Bogdan.The Previously approved version (23 Nov 2021 00:35) is available.Diff

This is an old revision of the document!


**UNDER CONSTRUCTION** AD-AD9213-DUAL-EBZ User Guide

All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.

Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.

resources/eval/user-guides/ad9213_dual_ebz/start.1676021756.txt.gz · Last modified: 10 Feb 2023 10:35 by Dragos Bogdan