Wiki

This version is outdated by a newer approved version.DiffThis version (28 Oct 2021 18:58) was approved by Travis Collins.The Previously approved version (26 Apr 2021 16:49) is available.Diff

This is an old revision of the document!


AD9208-DUAL-EBZ Virtex UltraScale+ VCU118 Quick Start Guide

This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the AD9208-DUAL-EBZ on the VCU118 platform.

The ADCs are set to run at full bandwidth mode 3 GSPS, which translates to a lane rate of 15.5 Gbps. Each converter has its own SYSREF that is driven from a common clock chip HMC7044. Ideally these SYREF lines should be length matched, if not the HMC has capability to adjust delays on its outputs. Sampling clocks are generated by the same HMC clock chip and should be ideally length matched as well.

Design and Integration Files

Prerequisites

Required Hardware

  • Xilinx VCU118 Rev 1.0 or later board
  • AD9208-DUAL-EBZ FMC board.
  • 2 x Micro-USB cable
  • Ethernet cable
  • Signal generator
  • 4 way splitter (optional)

Required Software

  • A Linux OS on a PC
  • Xilinx Vivado 2019.1 or later
  • UART terminal (e.g TeraTerm)
  • IIO Scope Download

Board setup

There are two options for powering the board, both require a rework :
  • In order to supply the board from the FMC connector populate F1 with a 2A fuse. Use this method if you can ensure the FMC carrier can drive 2A on its 12V power line.
  • Use an external 12V power supply and connect it to the TP1 (PWR_IN) and TP2 (AGND) points.

Steps

1. Build the HDL project

Before building the hdl project setup your computer based on the following guide: Building HDL projects

git clone https://github.com/analogdevicesinc/hdl.git
git checkout hdl_2019_r2;  // or latest release
cd hdl/projects/ad9208_dual_ebz/vcu118
make
Prebuild files for boards with 125MHz VCXO can be downloaded from here

2. Build the Linux files

Instructions on how to build the MicroBlaze Linux kernel and devicetrees from source can be found here:

make simpleImage.vcu118_dual_ad9208
Prebuild files for boards with 125MHz VCXO can be downloaded from here

3. Program the board

First we need to prepare a working directory where we will gather all the required binary files.
From the HDL build directory locate the system_top.bit and copy it to the working directory. From the Linux build directory locate the simpleImage and copy it to the working directory.

mkdir <working_dir>
cp <hdl_repo_dir>/projects/ad9208_dual_ebz_vcu118.runs/impl_1/system_top.bit  <working_dir>
cp <linux_repo_dir>/arch/microblaze/boot/simpleImage.vcu118_dual_ad9208  <working_dir>

Next step is to program the board with xsct or similar tool. See generic instructions for programming the MicroBlaze bases systems here Boot Kernel on FPGA Microblaze

xsct% connect
xsct% fpga -f system_top.bit
xsct% after 1000
xsct% target 3
xsct% dow simpleImage.vcu118_dual_ad9208.strip
xsct% after 1000
xsct% con
xsct% disconnect

Linux BOOT messages

Complete kernel boot log (Click to expand)

Complete kernel boot log (Click to expand)

This specifies any shell prompt running on the target

Ramdisk addr 0x00000000,
Compiled-in FDT at 8041955c
Linux version 4.14.0-g6f4b7f7 (<HOSTNAME>) (gcc version 8.2.0 (crosstool-NG 1.20.0)) #4 Tue Aug 18 10:15:22 IST 2020
setup_cpuinfo: initialising
setup_cpuinfo: Using full CPU PVR support
wt_msr_noirq
setup_memory: max_mapnr: 0x30000
setup_memory: min_low_pfn: 0x80000
setup_memory: max_low_pfn: 0xb0000
setup_memory: max_pfn: 0xb0000
Zone ranges:
  DMA      [mem 0x0000000080000000-0x00000000afffffff]
  Normal   empty
Movable zone start for each node
Early memory node ranges
  node   0: [mem 0x0000000080000000-0x00000000ffffefff]
Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffefff]
On node 0 totalpages: 196608
free_area_init_node: node 0, pgdat 805c5a4c, node_mem_map 808e8000
  DMA zone: 1536 pages used for memmap
  DMA zone: 0 pages reserved
  DMA zone: 196608 pages, LIFO batch:31
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists, mobility grouping on.  Total pages: 195072
Kernel command line: console=ttyUL0,115200
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 769556K/786432K available (4197K kernel code, 145K rwdata, 1496K rodata, 3074K init, 96K bss, 16876K reserved, 0K cma-reserved)
Kernel virtual memory layout:
  * 0xffffe000..0xfffff000  : fixmap
  * 0xffffe000..0xffffe000  : early ioremap
  * 0xb0000000..0xffffe000  : vmalloc & ioremap
NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
irq-xilinx: /amba_pl/interrupt-controller@41200000: num_irq=16, edge=0x35f8
/amba_pl/timer@41c00000: irq=1
clocksource: xilinx_clocksource: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns
xilinx_timer_shutdown
xilinx_timer_set_periodic
sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns
Calibrating delay loop... 49.35 BogoMIPS (lpj=246784)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
devtmpfs: initialized
random: get_random_u32 called from bucket_table_alloc+0x248/0x29c with crng_init=0
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 256 (order: -1, 3072 bytes)
NET: Registered protocol family 16
clocksource: Switched to clocksource xilinx_clocksource
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
random: fast init done
Skipping unavailable RESET gpio -2 (reset)
workingset: timestamp_bits=30 max_order=18 bucket_order=0
jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
40600000.serial: ttyUL0 at MMIO 0x40600000 (irq = 5, base_baud = 0) is a uartlite
console [ttyUL0] enabled
brd: module loaded
Xilinx SystemACE device driver, major=254
libphy: Fixed MDIO Bus: probed
xilinx_axienet 40c00000.ethernet: TX_CSUM 2
xilinx_axienet 40c00000.ethernet: RX_CSUM 2
libphy: Xilinx Axi Ethernet MDIO: probed
i2c /dev entries driver
i2c i2c-0: Added multiplexed i2c bus 1
at24 2-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write
i2c i2c-0: Added multiplexed i2c bus 2
i2c i2c-0: Added multiplexed i2c bus 3
i2c i2c-0: Added multiplexed i2c bus 4
i2c i2c-0: Added multiplexed i2c bus 5
i2c i2c-0: Added multiplexed i2c bus 6
i2c i2c-0: Added multiplexed i2c bus 7
i2c i2c-0: Added multiplexed i2c bus 8
pca954x 0-0075: registered 8 multiplexed busses for I2C switch pca9548
axi_adxcvr 44a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using GTY4 at 0x44A60000 mapped to 0xb0110000. Number of lanes: 8.
axi_adxcvr 44b60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using GTY4 at 0x44B60000 mapped to 0xb0330000. Number of lanes: 8.
NET: Registered protocol family 17
ad9208 spi0.1: AD9208 PLL LOCKED
ad9208 spi0.1: Failed to request FastDetect IRQs (-6)
ad9208 spi0.1: AD9208 DUAL (MASTER with DMA) Rev. 3 Grade 0 (API 1.0.1) probed
ad9208 spi0.2: AD9208 PLL LOCKED
ad9208 spi0.2: Failed to request FastDetect IRQs (-6)
ad9208 spi0.2: AD9208 Rev. 3 Grade 0 (API 1.0.1) probed
iio_dmaengine_buffer_alloc:227 width 0 (DMA width >= 256-bits ?)
cf_axi_adc 44a10000.axi-ad9208-0-hpc: ADI AIM (10.01.b) at 0x44A10000 mapped to 0xb0101000, probed ADC AD9208 DUAL (MASTER with DMA) as MASTER
cf_axi_adc 44b10000.axi-ad9208-1-hpc: ADI AIM (10.01.b) at 0x44B10000 mapped to 0xb010b000, probed ADC AD9208 as MASTER
Freeing unused kernel memory: 3072K
This architecture does not have kernel memory protection.
Starting syslogd: OK
Starting klogd: OK
Initializing random number generator... done.
Starting network: udhcpc: started, v1.29.3
net eth0: Promiscuous mode disabled.
net eth0: Promiscuous mode disabled.
udhcpc: sending discover
xilinx_axienet 40c00000.ethernet eth0: Link is Down
udhcpc: sending discover
xilinx_axienet 40c00000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
udhcpc: sending discover
udhcpc: sending discover
udhcpc: sending select for 10.48.65.139
udhcpc: lease of <IP> obtained, lease time 21600
deleting routers
adding dns <IP>
adding dns <IP>
Starting dropbear sshd: OK
Starting IIO Server Daemon

Welcome to Buildroot
buildroot login: root
Password:
#
#grep "" /sys/bus/platform/devices/*.axi-jesd*/status*
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:Link is enabled
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:Measured Link Clock: 350.821 MHz
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:Reported Link Clock: 375.000 MHz
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:Lane rate: 15000.000 MHz
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:Lane rate / 40: 375.000 MHz
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:LMFC rate: 46.875 MHz
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:Link status: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:SYSREF captured: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/status:SYSREF alignment error: No
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:Link is enabled
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:Measured Link Clock: 350.821 MHz
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:Reported Link Clock: 375.000 MHz
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:Lane rate: 15000.000 MHz
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:Lane rate / 40: 375.000 MHz
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:LMFC rate: 46.875 MHz
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:Link status: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:SYSREF captured: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/status:SYSREF alignment error: No
#
# grep "" /sys/bus/platform/devices/*.axi-jesd*/lane*
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:Errors: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:CGS state: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:Lane Latency: 3 Multi-frames and 27 Octets
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:DID: 0, BID: 0, LID: 0, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:FCHK: 0x86, CF: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane0_info:FC: 15000000
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:Errors: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:CGS state: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:Lane Latency: 3 Multi-frames and 27 Octets
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:DID: 0, BID: 0, LID: 1, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:FCHK: 0x87, CF: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane1_info:FC: 15000000
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:Errors: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:CGS state: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:Lane Latency: 3 Multi-frames and 26 Octets
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:DID: 0, BID: 0, LID: 2, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:FCHK: 0x88, CF: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane2_info:FC: 15000000
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:Errors: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:CGS state: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:Lane Latency: 3 Multi-frames and 28 Octets
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:DID: 0, BID: 0, LID: 3, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:FCHK: 0x89, CF: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane3_info:FC: 15000000
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:Errors: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:CGS state: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:Lane Latency: 3 Multi-frames and 28 Octets
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:DID: 0, BID: 0, LID: 4, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:FCHK: 0x8A, CF: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane4_info:FC: 15000000
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:Errors: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:CGS state: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:Lane Latency: 3 Multi-frames and 24 Octets
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:DID: 0, BID: 0, LID: 5, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:FCHK: 0x8B, CF: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane5_info:FC: 15000000
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:Errors: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:CGS state: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:Lane Latency: 3 Multi-frames and 25 Octets
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:DID: 0, BID: 0, LID: 6, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:FCHK: 0x8C, CF: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane6_info:FC: 15000000
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:Errors: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:CGS state: DATA
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:Lane Latency: 3 Multi-frames and 25 Octets
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:DID: 0, BID: 0, LID: 7, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:FCHK: 0x8D, CF: 0
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44a90000.axi-jesd204-rx/lane7_info:FC: 15000000
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:Errors: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:CGS state: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:Lane Latency: 3 Multi-frames and 26 Octets
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:DID: 0, BID: 0, LID: 0, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:FCHK: 0x86, CF: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane0_info:FC: 15000000
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:Errors: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:CGS state: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:Lane Latency: 3 Multi-frames and 28 Octets
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:DID: 0, BID: 0, LID: 1, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:FCHK: 0x87, CF: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane1_info:FC: 15000000
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:Errors: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:CGS state: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:Lane Latency: 3 Multi-frames and 26 Octets
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:DID: 0, BID: 0, LID: 2, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:FCHK: 0x88, CF: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane2_info:FC: 15000000
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:Errors: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:CGS state: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:Lane Latency: 3 Multi-frames and 27 Octets
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:DID: 0, BID: 0, LID: 3, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:FCHK: 0x89, CF: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane3_info:FC: 15000000
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:Errors: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:CGS state: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:Lane Latency: 3 Multi-frames and 26 Octets
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:DID: 0, BID: 0, LID: 4, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:FCHK: 0x8A, CF: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane4_info:FC: 15000000
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:Errors: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:CGS state: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:Lane Latency: 3 Multi-frames and 28 Octets
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:DID: 0, BID: 0, LID: 5, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:FCHK: 0x8B, CF: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane5_info:FC: 15000000
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:Errors: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:CGS state: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:Lane Latency: 3 Multi-frames and 25 Octets
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:DID: 0, BID: 0, LID: 6, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:FCHK: 0x8C, CF: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane6_info:FC: 15000000
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:Errors: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:CGS state: DATA
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:Initial Frame Synchronization: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:Lane Latency: 3 Multi-frames and 27 Octets
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:Initial Lane Alignment Sequence: Yes
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:DID: 0, BID: 0, LID: 7, L: 8, SCR: 1, F: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:K: 32, M: 2, N: 16, CS: 0, N': 16, S: 2, HD: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:FCHK: 0x8D, CF: 0
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
/sys/bus/platform/devices/44b90000.axi-jesd204-rx/lane7_info:FC: 15000000

The following devices should be present:

This specifies any shell prompt running on the target

# iio_info | grep iio:device
        iio:device0: hmc7044
        iio:device1: axi-ad9208-0-hpc (buffer capable)
        iio:device2: axi-ad9208-1-hpc

4. Connect to board with IIO Scope

From the UART console find out the board IP address that was allocated by the DHCP server. If you do not use a DHCP server manually assign an IP to the board Ethernet port.

5. Capture data with IIO Scope

JESD SubClass 0 example

When the device is configured from device tree into subclass 0 we can observe the two links are not synchronized and the channels present phase differences.  Subclass 0

JESD SubClass 1 example

When the devices are configured into subclass 1 (default), we can observe the JESD links are synchronized and there is no phase difference between the input channels.  Subclass 1

More Information

Support

Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Video, Audio, etc) via the EngineerZone.

resources/eval/user-guides/ad9208_dual_ebz/quickstart/vcu118.1619507614.txt.gz · Last modified: 27 Apr 2021 09:13 by Laszlo Nagy