This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ad9208_dual_ebz:quickstart:vcu118 [27 Apr 2021 09:13] Laszlo Nagy [AD9208-DUAL-EBZ Virtex UltraScale+ VCU118 Quick Start Guide] |
resources:eval:user-guides:ad9208_dual_ebz:quickstart:vcu118 [28 Oct 2021 19:01] Travis Collins add login info |
||
---|---|---|---|
Line 416: | Line 416: | ||
==== 4. Connect to board with IIO Scope ==== | ==== 4. Connect to board with IIO Scope ==== | ||
- | From the UART console find out the board IP address that was allocated by the DHCP server. If you do not use a DHCP server manually assign an IP to the board Ethernet port. | + | From the UART console find out the board IP address that was allocated by the DHCP server. If you do not use a DHCP server manually assign an IP to the board Ethernet port. The default username:password for Linux is **root:analog**. |
{{ :resources:eval:user-guides:ad9208_dual_ebz:quickstart:iio_connect_noip.png?nolink%400 |}} | {{ :resources:eval:user-guides:ad9208_dual_ebz:quickstart:iio_connect_noip.png?nolink%400 |}} |