Both sides previous revisionPrevious revision | |
resources:eval:user-guides:ad9081_fmca_ebz [19 Mar 2021 16:44] – [Table of Contents] Michael Hennerich | resources:eval:user-guides:ad9081_fmca_ebz [03 Dec 2021 09:37] (current) – add new variants Michael Hennerich |
---|
====== AD9081 & AD9082 Prototyping Platform User Guide ====== | ====== AD9081 & AD9082 & AD9988 & AD9986 Prototyping Platform User Guide ====== |
| |
{{ :resources:eval:user-guides:ad9081-fmca-ebz_ad9082-fmca-ebz.png?600 |}} | {{ :resources:eval:user-guides:ad9081-fmca-ebz_ad9082-fmca-ebz.png?600 |}} |
| |
The [[adi>AD9081-FMCA-EBZ]] or [[adi>AD9082-FMCA-EBZ]] is a FMC cards for the [[adi>AD9081]] or[[adi>AD9082]], information on the card and how to use it with standard Xilinx and Intel Carriers, the design package that surrounds it, and the software which can make it work can be found here. | The [[adi>AD9081-FMCA-EBZ]], [[adi>AD9988-FMCB-EBZ]] or [[adi>AD9082-FMCA-EBZ]], [[adi>AD9986-FMCB-EBZ]] is a FMC cards for the [[adi>AD9081]], [[adi>AD9988]] or [[adi>AD9082]], [[adi>AD9986]], information on the card and how to use it with standard Xilinx and Intel Carriers, the design package that surrounds it, and the software which can make it work can be found here. |
| |
===== Table of Contents ===== | ===== Table of Contents ===== |
People who follow the flow that is outlined, have a much better experience with things. However, like many things, documentation is never as complete as it should be. If you have any questions, feel free to [[.:ad-fmcomms2-ebz:help_and_support|ask]]. | People who follow the flow that is outlined, have a much better experience with things. However, like many things, documentation is never as complete as it should be. If you have any questions, feel free to [[.:ad-fmcomms2-ebz:help_and_support|ask]]. |
| |
- Use the board to better understand the [[adi>AD9081]] | - Use the board to better understand the [[adi>AD9081]], [[adi>AD9988]], [[adi>AD9082]], [[adi>AD9986]] |
- [[./ad9081_fmca_ebz/prerequisites|Prerequisites to using the board]] | - [[./ad9081_fmca_ebz/prerequisites|Prerequisites to using the board]] |
- [[:resources:eval:ad9082#installation_of_the_heat_sink_with_integrated_fan | Installation of the Heat Sink with Integrated Fan]] | - [[:resources:eval:ad9082#installation_of_the_heat_sink_with_integrated_fan | Installation of the Heat Sink with Integrated Fan]] |