This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad9081_fmca_ebz:radar [27 Sep 2021 12:56] – [Using the OFDM Radar] David Winter | resources:eval:user-guides:ad9081_fmca_ebz:radar [30 Jan 2023 01:51] (current) – Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== gr-ofdmradar - OFDM Radar on MxFE Platforms using IIO ===== | + | ====== gr-ofdmradar - OFDM Radar on MxFE Platforms using IIO ====== |
This page is dedicated to the details of building an OFDM radar on a ZCU102 + AD9081 with GNURadio and IIO. | This page is dedicated to the details of building an OFDM radar on a ZCU102 + AD9081 with GNURadio and IIO. | ||
+ | |||
+ | This was based on a paper pressented at: | ||
+ | * {{youtube> | ||
+ | * [[https:// | ||
If you just want to get the software and hardware running, the following section covers the setup instructions: | If you just want to get the software and hardware running, the following section covers the setup instructions: | ||
Line 22: | Line 26: | ||
==== Preparing the ZCU102 boot files ==== | ==== Preparing the ZCU102 boot files ==== | ||
- | It is usually a good idea to start out by installing a recent image of [[resources: | + | It is usually a good idea to start out by installing a recent image of [[:resources: |
=== Linux Kernel === | === Linux Kernel === | ||
Line 126: | Line 130: | ||
< | < | ||
# Checkout code | # Checkout code | ||
- | git clone https:// | + | git clone https:// |
cd gr-ofdmradar | cd gr-ofdmradar | ||
Line 179: | Line 183: | ||
For more details in general about the theoretical underpinnings of OFDM radar, please check out Martin Brauns dissertation: | For more details in general about the theoretical underpinnings of OFDM radar, please check out Martin Brauns dissertation: | ||
- | For more information about gr-ofdmradar system parameters check out the [[https:// | + | For more information about gr-ofdmradar system parameters check out the [[https:// |
- | * [[https:// | + | * [[https:// |
* [[https:// | * [[https:// | ||
Line 190: | Line 194: | ||
This section will describe how you can use the OFDM radar to get some actual returns, how you can tune the system and choose your parameters. | This section will describe how you can use the OFDM radar to get some actual returns, how you can tune the system and choose your parameters. | ||
- | Before going on, please make yourself familiar with the basic operating principles of an OFDM radar, and the meaning of the system parameters: https:// | + | Before going on, please make yourself familiar with the basic operating principles of an OFDM radar, and the meaning of the system parameters: https:// |
To reinforce your understanding, | To reinforce your understanding, | ||
Line 240: | Line 244: | ||
</ | </ | ||
- | This value is then fed though the turbo color map and shown on screen. For more information see the fragment shader in which all of this is happening: https:// | + | This value is then fed though the turbo color map and shown on screen. For more information see the fragment shader in which all of this is happening: https:// |
To really get an understanding of the max and min sliders you may need to play around with them in a simulation, but at least now you should have an idea of what they' | To really get an understanding of the max and min sliders you may need to play around with them in a simulation, but at least now you should have an idea of what they' | ||
Line 487: | Line 491: | ||
{{: | {{: | ||
- | **For more information on the parameters and OFDM radar algorithm, take a look at the [[https:// | + | **For more information on the parameters and OFDM radar algorithm, take a look at the [[https:// |
== DoA Blocks == | == DoA Blocks == |