This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad9081_fmca_ebz:radar [21 Sep 2021 12:41] – [GNU Radio Integration] David Winter | resources:eval:user-guides:ad9081_fmca_ebz:radar [30 Jan 2023 01:51] (current) – Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== gr-ofdmradar - OFDM Radar on MxFE Platforms using IIO ===== | + | ====== gr-ofdmradar - OFDM Radar on MxFE Platforms using IIO ====== |
This page is dedicated to the details of building an OFDM radar on a ZCU102 + AD9081 with GNURadio and IIO. | This page is dedicated to the details of building an OFDM radar on a ZCU102 + AD9081 with GNURadio and IIO. | ||
+ | |||
+ | This was based on a paper pressented at: | ||
+ | * {{youtube> | ||
+ | * [[https:// | ||
If you just want to get the software and hardware running, the following section covers the setup instructions: | If you just want to get the software and hardware running, the following section covers the setup instructions: | ||
Line 17: | Line 21: | ||
* A development device running x86_64 Linux | * A development device running x86_64 Linux | ||
- | * Vivado 2020.2 (Or whatever the current hdl master branch requires) | + | * Vivado 2020.2 (Or whatever the current hdl master branch requires), the Vitis SDK and a License for MPSoC parts (Included with evaluation kit) |
* A recent software build toolchain. (Usually provided by your Linux distribution. build-essential on debian stable+, base-devel on ArchLinux, etc.) | * A recent software build toolchain. (Usually provided by your Linux distribution. build-essential on debian stable+, base-devel on ArchLinux, etc.) | ||
==== Preparing the ZCU102 boot files ==== | ==== Preparing the ZCU102 boot files ==== | ||
- | It is usually a good idea to start out by installing a recent image of [[resources: | + | It is usually a good idea to start out by installing a recent image of [[:resources: |
=== Linux Kernel === | === Linux Kernel === | ||
Line 126: | Line 130: | ||
< | < | ||
# Checkout code | # Checkout code | ||
- | git clone https:// | + | git clone https:// |
cd gr-ofdmradar | cd gr-ofdmradar | ||
Line 172: | Line 176: | ||
{{: | {{: | ||
- | The following video shows a test where we covered a distance of 30-40m: | + | The following video shows a test where we covered a distance of ~35m: |
{{youtube> | {{youtube> | ||
Line 179: | Line 183: | ||
For more details in general about the theoretical underpinnings of OFDM radar, please check out Martin Brauns dissertation: | For more details in general about the theoretical underpinnings of OFDM radar, please check out Martin Brauns dissertation: | ||
- | For more information about gr-ofdmradar system parameters check out the [[https:// | + | For more information about gr-ofdmradar system parameters check out the [[https:// |
- | * [[https:// | + | * [[https:// |
* [[https:// | * [[https:// | ||
+ | |||
+ | ---- | ||
+ | ===== Using the OFDM Radar ===== | ||
+ | |||
+ | This section will describe how you can use the OFDM radar to get some actual returns, how you can tune the system and choose your parameters. | ||
+ | |||
+ | Before going on, please make yourself familiar with the basic operating principles of an OFDM radar, and the meaning of the system parameters: https:// | ||
+ | |||
+ | To reinforce your understanding, | ||
+ | |||
+ | {{: | ||
+ | |||
+ | * The complex system sample rate is '' | ||
+ | * the FFT Size '' | ||
+ | * a frame has '' | ||
+ | * and the cyclic prefix length '' | ||
+ | * and '' | ||
+ | |||
+ | thus | ||
+ | |||
+ | * the total TX frame length is '' | ||
+ | * the frame duration is '' | ||
+ | * the (non-oversampled), | ||
+ | * the (non-oversampled) doppler resolution is '' | ||
+ | * the true system bandwidth is '' | ||
+ | * the final processing gain '' | ||
+ | * and finally the covered distance spread: '' | ||
+ | |||
+ | This leaves us with a couple flowgraph parameters that should be discussed: | ||
+ | |||
+ | {{: | ||
+ | |||
+ | * The '' | ||
+ | * The '' | ||
+ | * '' | ||
+ | * The '' | ||
+ | |||
+ | Now lets take a look at the OFDM radar screen as you may see it when opening the simulation example in gr-ofdmradar: | ||
+ | |||
+ | {{: | ||
+ | |||
+ | There are still four parameters left to be explained, that control visualization parameters (But don't change anything about the signals themselves): | ||
+ | |||
+ | * The range slider controls range which is shown, and can be thought of as an inverted zoom slider: If you want to zoom in the range dimension, move the slider to the left. | ||
+ | * The doppler range slider works similarly, but reduces the doppler ranges which are shown. This isn't usually too much of an issue. | ||
+ | |||
+ | To explain the min and max value sliders, we need to take a look at how the visualization code works: | ||
+ | |||
+ | * The input values to the gui widget have already been fully processed and can be thought of as a complex 2D matrix over range and doppler. To visualize this matrix we first take the energy of each value, then use a mapping function like the following to map those energy values to something between 0 and 1, where '' | ||
+ | |||
+ | < | ||
+ | def mapv(x): | ||
+ | x = (x-minV)/ | ||
+ | return max(min(x, 1.0), 0.0) | ||
+ | </ | ||
+ | |||
+ | This value is then fed though the turbo color map and shown on screen. For more information see the fragment shader in which all of this is happening: https:// | ||
+ | |||
+ | To really get an understanding of the max and min sliders you may need to play around with them in a simulation, but at least now you should have an idea of what they' | ||
---- | ---- | ||
Line 193: | Line 256: | ||
* The Transceiver / RF ADC/DAC (AD9081) | * The Transceiver / RF ADC/DAC (AD9081) | ||
- | * Hardware, | + | * Hardware, HDL |
* Linux drivers | * Linux drivers | ||
* gr-ofdmradar and its blocks | * gr-ofdmradar and its blocks | ||
Line 408: | Line 471: | ||
gr-ofdmradar is where all the interesting signal processing is happening. gr-ofdmradar ships with two categories of blocks: Those implementing OFDM Radar, and those implementing direction of arrival (DoA) for a linear array. | gr-ofdmradar is where all the interesting signal processing is happening. gr-ofdmradar ships with two categories of blocks: Those implementing OFDM Radar, and those implementing direction of arrival (DoA) for a linear array. | ||
- | == OFDM Radar == | + | == OFDM Radar Blocks |
- | Many of the system parameters are shared between the TX, RX and Gui blocks, thus these are stored in a separate "OFDM Radar System Parameters" | + | Many of the system parameters are shared between the TX, RX and GUI blocks, thus these are stored in a separate "OFDM Radar System Parameters" |
{{: | {{: | ||
+ | The '' | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The '' | ||
+ | |||
+ | {{: | ||
+ | |||
+ | <note tip>The `Buffer Size` parameter determines how many samples will be expected / ofdm frame. While the amount of samples which is actually processed is determined by the ofdm system parameters, the block can consume (and discard) additional samples to align frame boundaries to the iio buffers for example. The amount of discarded samples after each received ofdm frame can be determined as '' | ||
+ | |||
+ | Finally the '' | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **For more information on the parameters and OFDM radar algorithm, take a look at the [[https:// | ||
+ | |||
+ | == DoA Blocks == | ||
+ | |||
+ | The Doa blocks are less integrated, but also don't come with many parameters. The implicit assumption is that we're working with a linear array and '' | ||
+ | |||
+ | ** DoA Autocorrelator ** | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ** DoA Calibration Block ** | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ** DoA MUSIC Estimator ** | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ** DoA ESPRIT Estimator ** | ||
+ | |||
+ | {{: | ||