Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:ad9081_fmca_ebz:radar [27 Sep 2021 12:56]
David Winter [Using the OFDM Radar]
resources:eval:user-guides:ad9081_fmca_ebz:radar [28 Sep 2021 10:31] (current)
David Winter Update links to gr-ofdmradar
Line 1: Line 1:
-===== gr-ofdmradar - OFDM Radar on MxFE Platforms using IIO =====+====== gr-ofdmradar - OFDM Radar on MxFE Platforms using IIO ======
  
 This page is dedicated to the details of building an OFDM radar on a ZCU102 + AD9081 with GNURadio and IIO. This page is dedicated to the details of building an OFDM radar on a ZCU102 + AD9081 with GNURadio and IIO.
Line 126: Line 126:
 <​code>​ <​code>​
 # Checkout code # Checkout code
-git clone https://​github.com/​Yamakaja/​gr-ofdmradar.git+git clone https://​github.com/​analogdevicesinc/​gr-ofdmradar.git
 cd gr-ofdmradar cd gr-ofdmradar
  
Line 179: Line 179:
 For more details in general about the theoretical underpinnings of OFDM radar, please check out Martin Brauns dissertation:​ [[https://​publikationen.bibliothek.kit.edu/​1000038892]] For more details in general about the theoretical underpinnings of OFDM radar, please check out Martin Brauns dissertation:​ [[https://​publikationen.bibliothek.kit.edu/​1000038892]]
  
-For more information about gr-ofdmradar system parameters check out the [[https://​github.com/​Yamakaja/​gr-ofdmradar/​blob/​master/​README.md|gr-ofdmradar/​README.md]]+For more information about gr-ofdmradar system parameters check out the [[https://​github.com/​analogdevicesinc/​gr-ofdmradar/​blob/​master/​README.md|gr-ofdmradar/​README.md]]
  
  
-  * [[https://​github.com/​Yamakaja/​gr-ofdmradar|gr-ofdmradar]]+  * [[https://​github.com/​analogdevicesinc/​gr-ofdmradar|gr-ofdmradar]]
   * [[https://​github.com/​Yamakaja/​gnuradio/​tree/​feature/​gr-iio-tdd|GNU Radio branch with AD9081 blocks]]   * [[https://​github.com/​Yamakaja/​gnuradio/​tree/​feature/​gr-iio-tdd|GNU Radio branch with AD9081 blocks]]
  
Line 190: Line 190:
 This section will describe how you can use the OFDM radar to get some actual returns, how you can tune the system and choose your parameters. This section will describe how you can use the OFDM radar to get some actual returns, how you can tune the system and choose your parameters.
  
-Before going on, please make yourself familiar with the basic operating principles of an OFDM radar, and the meaning of the system parameters: https://​github.com/​Yamakaja/​gr-ofdmradar#​operating-principle+Before going on, please make yourself familiar with the basic operating principles of an OFDM radar, and the meaning of the system parameters: https://​github.com/​analogdevicesinc/​gr-ofdmradar#​operating-principle
  
 To reinforce your understanding,​ lets take a look at this example set of parameters. To reinforce your understanding,​ lets take a look at this example set of parameters.
Line 240: Line 240:
 </​code>​ </​code>​
  
-This value is then fed though the turbo color map and shown on screen. For more information see the fragment shader in which all of this is happening: https://​github.com/​Yamakaja/​gr-ofdmradar/​blob/​master/​lib/​resources/​screen.frag+This value is then fed though the turbo color map and shown on screen. For more information see the fragment shader in which all of this is happening: https://​github.com/​analogdevicesinc/​gr-ofdmradar/​blob/​master/​lib/​resources/​screen.frag
  
 To really get an understanding of the max and min sliders you may need to play around with them in a simulation, but at least now you should have an idea of what they'​re doing. To really get an understanding of the max and min sliders you may need to play around with them in a simulation, but at least now you should have an idea of what they'​re doing.
Line 487: Line 487:
 {{:​resources:​eval:​user-guides:​ad9081_fmca_ebz:​radar:​gr_ofdmradar_gui.png|}} {{:​resources:​eval:​user-guides:​ad9081_fmca_ebz:​radar:​gr_ofdmradar_gui.png|}}
  
-**For more information on the parameters and OFDM radar algorithm, take a look at the [[https://​github.com/​Yamakaja/​gr-ofdmradar#​operating-principle|gr-ofdmradar/​README.md]].**+**For more information on the parameters and OFDM radar algorithm, take a look at the [[https://​github.com/​analogdevicesinc/​gr-ofdmradar#​operating-principle|gr-ofdmradar/​README.md]].**
  
 == DoA Blocks == == DoA Blocks ==
resources/eval/user-guides/ad9081_fmca_ebz/radar.txt · Last modified: 28 Sep 2021 10:31 by David Winter