This is an old revision of the document!
The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the AD9081-FMCA-EBZ and AD9082-FMCA-EBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.
The AD9081-FMCA-EBZ and AD9082-FMCA-EBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:
In most carriers, the AD9081-FMCA-EBZ board connects to the HPC0 connector (unless otherwise noted). The carrier setup requires power, UART (115200), ethernet (Linux), DisplayPort or HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.
Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.