This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:eval:user-guides:ad9081_fmca_ebz:quickstart:zynqmp [08 Oct 2021 13:50] – vcxo122.88 fix name Dragos Bogdan | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== AD9081/ | ||
+ | {{ : | ||
+ | This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the [[adi> | ||
+ | |||
+ | Instructions on how to build the ZynqMP / MPSoC Linux kernel and devicetrees from source can be found here: | ||
+ | |||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | |||
+ | ===== Required Software ===== | ||
+ | |||
+ | * SD Card 16GB imaged using the instructions here: [[resources: | ||
+ | * Alternatively if you already have a SD-Card with the [[resources: | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * A UART terminal (Putty/Tera Term/ | ||
+ | |||
+ | ===== Required Hardware ===== | ||
+ | * Xilinx [[xilinx> | ||
+ | * AD9081-FMCA-EBZ/ | ||
+ | * Micro-USB cable | ||
+ | * Ethernet cable | ||
+ | * Optionally USB keyboard mouse and a Display Port compatible monitor | ||
+ | |||
+ | ===== Example Device Trees ===== | ||
+ | |||
+ | ==== AD9081-FMCA-EBZ / AD9082-FMCA-EBZ on ZCU102 (Zynq UltraScale+ MPSoC) ==== | ||
+ | |||
+ | ^ Function ^ File ^ | ||
+ | | dtsi | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | |||
+ | ====== Testing ====== | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | * Connect the [[adi> | ||
+ | * Connect USB UART J83 (Micro USB) to your host PC. | ||
+ | * Insert SD card into socket. | ||
+ | * Configure ZCU102 for SD BOOT (mode SW6[4:1] switch in the position **OFF, | ||
+ | * Turn on the power switch on the FPGA board. | ||
+ | * Observe kernel and serial console messages on your terminal. (use the first ttyUSB or COM port registered) | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | {{page> | ||
+ | |||
+ | |||
+ | ===== SDcard boot files ===== | ||
+ | |||
+ | The files that need to be present on the sdcard '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | |||
+ | Copy the '' | ||
+ | For evaluation boards populated with VXCO 100 MHz copy the device tree from '' | ||
+ | For evaluation boards populated with VXCO 122.88 MHz copy the device tree from '' | ||
+ | Copy the '' | ||
+ | <note important> | ||
+ | |||
+ | ===== Setting up UART ===== | ||
+ | When setting up the UART make sure you connect to the Interface 0 | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ===== Boot messages ===== | ||
+ | |||
+ | The **2019_R2** Image based boot messages looks like the followings : | ||
+ | |||
+ | <hidden Complete kernel boot log (Click to expand)> | ||
+ | <WRAP box bggreen>< | ||
+ | < | ||
+ | |||
+ | Xilinx Zynq MP First Stage Boot Loader | ||
+ | Release 2019.1 | ||
+ | NOTICE: | ||
+ | NOTICE: | ||
+ | NOTICE: | ||
+ | NOTICE: | ||
+ | NOTICE: | ||
+ | PMUFW: | ||
+ | |||
+ | |||
+ | U-Boot 2018.01-21436-gbba91bc203 (Jan 13 2020 - 10:50:58 +0200) Xilinx ZynqMP ZCU102 rev1.0, Build: jenkins-development-build_uboot-1 | ||
+ | |||
+ | I2C: ready | ||
+ | DRAM: 4 GiB | ||
+ | EL Level: | ||
+ | Chip ID: zu9eg | ||
+ | MMC: | ||
+ | *** Warning - bad CRC, using default environment | ||
+ | |||
+ | In: serial@ff000000 | ||
+ | Out: | ||
+ | Err: | ||
+ | Bootmode: LVL_SHFT_SD_MODE1 | ||
+ | Net: ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id | ||
+ | |||
+ | Warning: ethernet@ff0e0000 using MAC address from ROM | ||
+ | eth0: ethernet@ff0e0000 | ||
+ | Hit any key to stop autoboot: | ||
+ | switch to partitions #0, OK | ||
+ | mmc0 is current device | ||
+ | Device: sdhci@ff170000 | ||
+ | Manufacturer ID: 3 | ||
+ | OEM: 5344 | ||
+ | Name: SC32G | ||
+ | Tran Speed: 50000000 | ||
+ | Rd Block Len: 512 | ||
+ | SD version 3.0 | ||
+ | High Capacity: Yes | ||
+ | Capacity: 29.7 GiB | ||
+ | Bus Width: 4-bit | ||
+ | Erase Group Size: 512 Bytes | ||
+ | reading uEnv.txt | ||
+ | 407 bytes read in 16 ms (24.4 KiB/s) | ||
+ | Loaded environment from uEnv.txt | ||
+ | Importing environment from SD ... | ||
+ | Running uenvcmd ... | ||
+ | Copying Linux from SD to RAM... | ||
+ | ** No boot file defined ** | ||
+ | reading system.dtb | ||
+ | 44731 bytes read in 24 ms (1.8 MiB/s) | ||
+ | reading Image | ||
+ | 29737472 bytes read in 2000 ms (14.2 MiB/s) | ||
+ | ## Flattened Device Tree blob at 04000000 | ||
+ | | ||
+ | | ||
+ | |||
+ | Starting kernel ... | ||
+ | |||
+ | [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] | ||
+ | [ 0.000000] Linux version 4.19.0-ga6ef26d (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (GCC)) #1105 SMP Fri Feb 19 16:51:27 GMT 2021 | ||
+ | [ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0 | ||
+ | [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options ' | ||
+ | [ 0.000000] bootconsole [cdns0] enabled | ||
+ | [ 0.000000] efi: Getting EFI parameters from FDT: | ||
+ | [ 0.000000] efi: UEFI not found. | ||
+ | [ 0.000000] cma: Reserved 256 MiB at 0x0000000070000000 | ||
+ | [ 0.000000] psci: probing for conduit method from DT. | ||
+ | [ 0.000000] psci: PSCIv1.1 detected in firmware. | ||
+ | [ 0.000000] psci: Using standard PSCI v0.2 function IDs | ||
+ | [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. | ||
+ | [ 0.000000] psci: SMC Calling Convention v1.1 | ||
+ | [ 0.000000] random: get_random_bytes called from start_kernel+0x94/ | ||
+ | [ 0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s52504 r8192 d29416 u90112 | ||
+ | [ 0.000000] Detected VIPT I-cache on CPU0 | ||
+ | [ 0.000000] CPU features: enabling workaround for ARM erratum 845719 | ||
+ | [ 0.000000] Speculative Store Bypass Disable mitigation not required | ||
+ | [ 0.000000] CPU features: detected: Kernel page table isolation (KPTI) | ||
+ | [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1034240 | ||
+ | [ 0.000000] Kernel command line: console=ttyPS0, | ||
+ | rootwait | ||
+ | [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes) | ||
+ | [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes) | ||
+ | [ 0.000000] software IO TLB: mapped [mem 0x6bfff000-0x6ffff000] (64MB) | ||
+ | [ 0.000000] Memory: 3772348K/ | ||
+ | [ 0.000000] rcu: Hierarchical RCU implementation. | ||
+ | [ 0.000000] rcu: RCU event tracing is enabled. | ||
+ | [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. | ||
+ | [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, | ||
+ | [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 | ||
+ | [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 | ||
+ | [ 0.000000] GIC: Using split EOI/ | ||
+ | [ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys). | ||
+ | [ 0.000000] clocksource: | ||
+ | [ 0.000003] sched_clock: | ||
+ | [ 0.008255] Console: colour dummy device 80x25 | ||
+ | [ 0.012391] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960) | ||
+ | [ 0.022756] pid_max: default: 32768 minimum: 301 | ||
+ | [ 0.027449] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes) | ||
+ | [ 0.034012] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes) | ||
+ | [ 0.041794] ASID allocator initialised with 32768 entries | ||
+ | [ 0.046508] rcu: Hierarchical SRCU implementation. | ||
+ | [ 0.051548] EFI services will not be available. | ||
+ | [ 0.055828] smp: Bringing up secondary CPUs ... | ||
+ | [ 0.060485] Detected VIPT I-cache on CPU1 | ||
+ | [ 0.060515] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] | ||
+ | [ 0.060814] Detected VIPT I-cache on CPU2 | ||
+ | [ 0.060834] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] | ||
+ | [ 0.061114] Detected VIPT I-cache on CPU3 | ||
+ | [ 0.061133] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] | ||
+ | [ 0.061176] smp: Brought up 1 node, 4 CPUs | ||
+ | [ 0.095681] SMP: Total of 4 processors activated. | ||
+ | [ 0.100354] CPU features: detected: 32-bit EL0 Support | ||
+ | [ 0.106862] CPU: All CPU(s) started at EL2 | ||
+ | [ 0.109534] alternatives: | ||
+ | [ 0.114847] devtmpfs: initialized | ||
+ | [ 0.122736] Registered cp15_barrier emulation handler | ||
+ | [ 0.122785] Registered setend emulation handler | ||
+ | [ 0.126847] clocksource: | ||
+ | [ 0.136437] futex hash table entries: 1024 (order: 4, 65536 bytes) | ||
+ | [ 0.148125] xor: measuring software checksum speed | ||
+ | [ 0.186641] | ||
+ | [ 0.226666] | ||
+ | [ 0.266697] | ||
+ | [ 0.306725] | ||
+ | [ 0.306766] xor: using function: 32regs (2724.000 MB/sec) | ||
+ | [ 0.311069] pinctrl core: initialized pinctrl subsystem | ||
+ | [ 0.316855] NET: Registered protocol family 16 | ||
+ | [ 0.321065] audit: initializing netlink subsys (disabled) | ||
+ | [ 0.326090] audit: type=2000 audit(0.272: | ||
+ | [ 0.333728] vdso: 2 pages (1 code @ (____ptrval____), | ||
+ | [ 0.333733] hw-breakpoint: | ||
+ | [ 0.348492] DMA: preallocated 256 KiB pool for atomic allocations | ||
+ | [ 0.367721] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages | ||
+ | [ 0.436460] raid6: int64x1 | ||
+ | [ 0.504424] raid6: int64x1 | ||
+ | [ 0.572515] raid6: int64x2 | ||
+ | [ 0.640548] raid6: int64x2 | ||
+ | [ 0.708557] raid6: int64x4 | ||
+ | [ 0.776599] raid6: int64x4 | ||
+ | [ 0.844679] raid6: int64x8 | ||
+ | [ 0.912701] raid6: int64x8 | ||
+ | [ 0.980756] raid6: neonx1 | ||
+ | [ 1.048776] raid6: neonx1 | ||
+ | [ 1.116859] raid6: neonx2 | ||
+ | [ 1.184865] raid6: neonx2 | ||
+ | [ 1.252949] raid6: neonx4 | ||
+ | [ 1.320970] raid6: neonx4 | ||
+ | [ 1.389006] raid6: neonx8 | ||
+ | [ 1.457058] raid6: neonx8 | ||
+ | [ 1.457096] raid6: using algorithm neonx8 gen() 1550 MB/s | ||
+ | [ 1.461056] raid6: .... xor() 1459 MB/s, rmw enabled | ||
+ | [ 1.465986] raid6: using neon recovery algorithm | ||
+ | [ 1.471291] SCSI subsystem initialized | ||
+ | [ 1.474463] usbcore: registered new interface driver usbfs | ||
+ | [ 1.479776] usbcore: registered new interface driver hub | ||
+ | [ 1.485050] usbcore: registered new device driver usb | ||
+ | [ 1.490203] media: Linux media interface: v0.10 | ||
+ | [ 1.494556] videodev: Linux video capture interface: v2.00 | ||
+ | [ 1.500037] pps_core: LinuxPPS API ver. 1 registered | ||
+ | [ 1.504917] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti < | ||
+ | [ 1.514010] PTP clock support registered | ||
+ | [ 1.517908] EDAC MC: Ver: 3.0.0 | ||
+ | [ 1.521385] zynqmp-ipi-mbox mailbox@ff990400: | ||
+ | [ 1.528760] jesd204: created con: id=0, topo=0, link=0, / | ||
+ | [ 1.539355] jesd204: created con: id=1, topo=0, link=2, / | ||
+ | [ 1.550427] jesd204: created con: id=2, topo=0, link=0, / | ||
+ | [ 1.562104] jesd204: created con: id=3, topo=0, link=2, / | ||
+ | [ 1.573782] jesd204: created con: id=4, topo=0, link=0, / | ||
+ | [ 1.585807] jesd204: created con: id=5, topo=0, link=2, / | ||
+ | [ 1.597833] jesd204: created con: id=6, topo=0, link=2, / | ||
+ | [ 1.609167] jesd204: created con: id=7, topo=0, link=0, / | ||
+ | [ 1.620504] jesd204: / | ||
+ | [ 1.629577] jesd204: / | ||
+ | [ 1.638658] jesd204: found 8 devices and 1 topologies | ||
+ | [ 1.643706] FPGA manager framework | ||
+ | [ 1.647220] Advanced Linux Sound Architecture Driver Initialized. | ||
+ | [ 1.653380] Bluetooth: Core ver 2.22 | ||
+ | [ 1.656666] NET: Registered protocol family 31 | ||
+ | [ 1.661065] Bluetooth: HCI device and connection manager initialized | ||
+ | [ 1.667382] Bluetooth: HCI socket layer initialized | ||
+ | [ 1.672225] Bluetooth: L2CAP socket layer initialized | ||
+ | [ 1.677258] Bluetooth: SCO socket layer initialized | ||
+ | [ 1.682620] clocksource: | ||
+ | [ 1.688238] VFS: Disk quotas dquot_6.6.0 | ||
+ | [ 1.692077] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) | ||
+ | [ 1.703496] NET: Registered protocol family 2 | ||
+ | [ 1.703884] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes) | ||
+ | [ 1.711025] TCP established hash table entries: 32768 (order: 6, 262144 bytes) | ||
+ | [ 1.718360] TCP bind hash table entries: 32768 (order: 7, 524288 bytes) | ||
+ | [ 1.725133] TCP: Hash tables configured (established 32768 bind 32768) | ||
+ | [ 1.731285] UDP hash table entries: 2048 (order: 4, 65536 bytes) | ||
+ | [ 1.737263] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes) | ||
+ | [ 1.743750] NET: Registered protocol family 1 | ||
+ | [ 1.748136] RPC: Registered named UNIX socket transport module. | ||
+ | [ 1.753814] RPC: Registered udp transport module. | ||
+ | [ 1.758473] RPC: Registered tcp transport module. | ||
+ | [ 1.763146] RPC: Registered tcp NFSv4.1 backchannel transport module. | ||
+ | [ 1.770312] hw perfevents: no interrupt-affinity property for /pmu, guessing. | ||
+ | [ 1.776794] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available | ||
+ | [ 1.785179] Initialise system trusted keyrings | ||
+ | [ 1.788825] workingset: timestamp_bits=62 max_order=20 bucket_order=0 | ||
+ | [ 1.795858] NFS: Registering the id_resolver key type | ||
+ | [ 1.800184] Key type id_resolver registered | ||
+ | [ 1.804323] Key type id_legacy registered | ||
+ | [ 1.808307] nfs4filelayout_init: | ||
+ | [ 1.814975] jffs2: version 2.2. (NAND) (SUMMARY) | ||
+ | [ 2.903619] NET: Registered protocol family 38 | ||
+ | [ 2.964582] Key type asymmetric registered | ||
+ | [ 2.964620] Asymmetric key parser ' | ||
+ | [ 2.967916] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246) | ||
+ | [ 2.975239] io scheduler noop registered | ||
+ | [ 2.979129] io scheduler deadline registered | ||
+ | [ 2.983387] io scheduler cfq registered (default) | ||
+ | [ 2.988040] io scheduler mq-deadline registered | ||
+ | [ 2.992537] io scheduler kyber registered | ||
+ | [ 3.024197] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled | ||
+ | [ 3.028267] cacheinfo: Unable to detect cache hierarchy for CPU 0 | ||
+ | [ 3.035571] brd: module loaded | ||
+ | [ 3.039411] loop: module loaded | ||
+ | [ 3.039622] Registered mathworks_ip class | ||
+ | [ 3.041890] mtdoops: mtd device (mtddev=name/ | ||
+ | [ 3.048941] libphy: Fixed MDIO Bus: probed | ||
+ | [ 3.052744] tun: Universal TUN/TAP device driver, 1.6 | ||
+ | [ 3.056689] CAN device driver interface | ||
+ | [ 3.061300] usbcore: registered new interface driver asix | ||
+ | [ 3.065785] usbcore: registered new interface driver ax88179_178a | ||
+ | [ 3.071820] usbcore: registered new interface driver cdc_ether | ||
+ | [ 3.077615] usbcore: registered new interface driver net1080 | ||
+ | [ 3.083240] usbcore: registered new interface driver cdc_subset | ||
+ | [ 3.089120] usbcore: registered new interface driver zaurus | ||
+ | [ 3.094666] usbcore: registered new interface driver cdc_ncm | ||
+ | [ 3.100944] ehci_hcd: USB 2.0 ' | ||
+ | [ 3.106748] ehci-pci: EHCI PCI platform driver | ||
+ | [ 3.111413] usbcore: registered new interface driver uas | ||
+ | [ 3.116466] usbcore: registered new interface driver usb-storage | ||
+ | [ 3.122459] usbcore: registered new interface driver usbserial_generic | ||
+ | [ 3.128910] usbserial: USB Serial support registered for generic | ||
+ | [ 3.134882] usbcore: registered new interface driver ftdi_sio | ||
+ | [ 3.140589] usbserial: USB Serial support registered for FTDI USB Serial Device | ||
+ | [ 3.147857] usbcore: registered new interface driver upd78f0730 | ||
+ | [ 3.153736] usbserial: USB Serial support registered for upd78f0730 | ||
+ | [ 3.161301] rtc_zynqmp ffa60000.rtc: | ||
+ | [ 3.167191] i2c /dev entries driver | ||
+ | [ 3.172562] usbcore: registered new interface driver uvcvideo | ||
+ | [ 3.176302] USB Video Class driver (1.1.1) | ||
+ | [ 3.181738] Bluetooth: HCI UART driver ver 2.3 | ||
+ | [ 3.184784] Bluetooth: HCI UART protocol H4 registered | ||
+ | [ 3.189881] Bluetooth: HCI UART protocol BCSP registered | ||
+ | [ 3.195179] Bluetooth: HCI UART protocol LL registered | ||
+ | [ 3.200262] Bluetooth: HCI UART protocol ATH3K registered | ||
+ | [ 3.205642] Bluetooth: HCI UART protocol Three-wire (H5) registered | ||
+ | [ 3.211894] Bluetooth: HCI UART protocol Intel registered | ||
+ | [ 3.217236] Bluetooth: HCI UART protocol QCA registered | ||
+ | [ 3.222446] usbcore: registered new interface driver bcm203x | ||
+ | [ 3.228057] usbcore: registered new interface driver bpa10x | ||
+ | [ 3.233593] usbcore: registered new interface driver bfusb | ||
+ | [ 3.239046] usbcore: registered new interface driver btusb | ||
+ | [ 3.244468] Bluetooth: Generic Bluetooth SDIO driver ver 0.1 | ||
+ | [ 3.250134] usbcore: registered new interface driver ath3k | ||
+ | [ 3.255665] EDAC MC: ECC not enabled | ||
+ | [ 3.259365] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT) | ||
+ | [ 3.271530] CPUidle arm: Failed to register cpuidle driver | ||
+ | [ 3.276816] sdhci: Secure Digital Host Controller Interface driver | ||
+ | [ 3.282791] sdhci: Copyright(c) Pierre Ossman | ||
+ | [ 3.287115] sdhci-pltfm: | ||
+ | [ 3.293118] ledtrig-cpu: | ||
+ | [ 3.298752] zynqmp_firmware_probe Platform Management API v1.1 | ||
+ | [ 3.304507] zynqmp_firmware_probe Trustzone version v1.0 | ||
+ | [ 3.312598] zynqmp-pinctrl firmware: | ||
+ | [ 3.339995] zynqmp_clk_mux_get_parent() getparent failed for clock: lpd_wdt, ret = -22 | ||
+ | [ 3.342694] alg: No test for xilinx-zynqmp-aes (zynqmp-aes) | ||
+ | [ 3.347809] zynqmp_aes zynqmp_aes: AES Successfully Registered | ||
+ | [ 3.347809] | ||
+ | [ 3.355326] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384) | ||
+ | [ 3.361554] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa) | ||
+ | [ 3.367047] usbcore: registered new interface driver usbhid | ||
+ | [ 3.372366] usbhid: USB HID core driver | ||
+ | [ 3.383901] axi_sysid 85000000.axi-sysid-0: | ||
+ | [ 3.392227] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered | ||
+ | [ 3.398822] usbcore: registered new interface driver snd-usb-audio | ||
+ | [ 3.406188] pktgen: Packet Generator for packet performance testing. Version: 2.75 | ||
+ | [ 3.412338] Initializing XFRM netlink socket | ||
+ | [ 3.416261] NET: Registered protocol family 10 | ||
+ | [ 3.420966] Segment Routing with IPv6 | ||
+ | [ 3.424320] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver | ||
+ | [ 3.430457] NET: Registered protocol family 17 | ||
+ | [ 3.434536] NET: Registered protocol family 15 | ||
+ | [ 3.438952] bridge: filtering via arp/ | ||
+ | [ 3.452044] can: controller area network core (rev 20170425 abi 9) | ||
+ | [ 3.457998] NET: Registered protocol family 29 | ||
+ | [ 3.462384] can: raw protocol (rev 20170425) | ||
+ | [ 3.466621] can: broadcast manager protocol (rev 20170425 t) | ||
+ | [ 3.472247] can: netlink gateway (rev 20170425) max_hops=1 | ||
+ | [ 3.477965] Bluetooth: RFCOMM TTY layer initialized | ||
+ | [ 3.482546] Bluetooth: RFCOMM socket layer initialized | ||
+ | [ 3.487654] Bluetooth: RFCOMM ver 1.11 | ||
+ | [ 3.491367] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 | ||
+ | [ 3.496639] Bluetooth: BNEP filters: protocol multicast | ||
+ | [ 3.501831] Bluetooth: BNEP socket layer initialized | ||
+ | [ 3.506761] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 | ||
+ | [ 3.512645] Bluetooth: HIDP socket layer initialized | ||
+ | [ 3.517685] 9pnet: Installing 9P2000 support | ||
+ | [ 3.521822] NET: Registered protocol family 36 | ||
+ | [ 3.526238] Key type dns_resolver registered | ||
+ | [ 3.530999] registered taskstats version 1 | ||
+ | [ 3.534525] Loading compiled-in X.509 certificates | ||
+ | [ 3.539629] Btrfs loaded, crc32c=crc32c-generic | ||
+ | [ 3.550250] ff000000.serial: | ||
+ | [ 3.559638] console [ttyPS0] enabled | ||
+ | [ 3.559638] console [ttyPS0] enabled | ||
+ | [ 3.563238] bootconsole [cdns0] disabled | ||
+ | [ 3.563238] bootconsole [cdns0] disabled | ||
+ | [ 3.571303] ff010000.serial: | ||
+ | [ 3.584662] of-fpga-region fpga-full: FPGA Region probed | ||
+ | [ 3.590786] nwl-pcie fd0e0000.pcie: | ||
+ | [ 3.595430] nwl-pcie fd0e0000.pcie: | ||
+ | [ 3.602400] nwl-pcie fd0e0000.pcie: | ||
+ | [ 3.609622] nwl-pcie fd0e0000.pcie: | ||
+ | [ 3.617203] nwl-pcie fd0e0000.pcie: | ||
+ | [ 3.623380] pci_bus 0000:00: root bus resource [bus 00-ff] | ||
+ | [ 3.628863] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff] | ||
+ | [ 3.635732] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref] | ||
+ | [ 3.647664] pci 0000: | ||
+ | [ 3.653802] xilinx-dpdma fd4c0000.dma: | ||
+ | [ 3.660381] xilinx-zynqmp-dma fd500000.dma: | ||
+ | [ 3.667483] xilinx-zynqmp-dma fd510000.dma: | ||
+ | [ 3.674585] xilinx-zynqmp-dma fd520000.dma: | ||
+ | [ 3.681683] xilinx-zynqmp-dma fd530000.dma: | ||
+ | [ 3.688789] xilinx-zynqmp-dma fd540000.dma: | ||
+ | [ 3.695893] xilinx-zynqmp-dma fd550000.dma: | ||
+ | [ 3.702994] xilinx-zynqmp-dma fd560000.dma: | ||
+ | [ 3.710096] xilinx-zynqmp-dma fd570000.dma: | ||
+ | [ 3.717341] xilinx-psgtr fd400000.zynqmp_phy: | ||
+ | [ 3.728810] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, | ||
+ | [ 3.737497] xilinx-dp-snd-codec fd4a0000.zynqmp-display: | ||
+ | [ 3.748264] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: | ||
+ | [ 3.756343] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: | ||
+ | [ 3.764844] xilinx-dp-snd-card fd4a0000.zynqmp-display: | ||
+ | [ 3.777288] xilinx-dp-snd-card fd4a0000.zynqmp-display: | ||
+ | [ 3.789963] xilinx-dp-snd-card fd4a0000.zynqmp-display: | ||
+ | [ 3.800141] OF: graph: no port node found in / | ||
+ | [ 3.807107] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). | ||
+ | [ 3.813716] [drm] No driver support for vblank timestamp query. | ||
+ | [ 3.819699] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008dc2e70) | ||
+ | [ 4.906629] [drm] Cannot find any crtc or sizes | ||
+ | [ 4.911375] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0 | ||
+ | [ 4.919475] zynqmp-display fd4a0000.zynqmp-display: | ||
+ | [ 4.928469] xilinx-psgtr fd400000.zynqmp_phy: | ||
+ | [ 4.946413] ahci-ceva fd0c0000.ahci: | ||
+ | [ 4.955374] ahci-ceva fd0c0000.ahci: | ||
+ | [ 4.965786] scsi host0: ahci-ceva | ||
+ | [ 4.969342] scsi host1: ahci-ceva | ||
+ | [ 4.972799] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37 | ||
+ | [ 4.980710] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37 | ||
+ | [ 5.039829] jesd204: / | ||
+ | [ 5.049613] m25p80 spi0.0: SPI-NOR-UniqueID 1044000ad9040001f6ff0f009e90a67dfd | ||
+ | [ 5.056835] m25p80 spi0.0: found n25q512a, expected m25p80 | ||
+ | [ 5.062534] m25p80 spi0.0: n25q512a (131072 Kbytes) | ||
+ | [ 5.067427] 4 fixed-partitions partitions found on MTD device spi0.0 | ||
+ | [ 5.073774] Creating 4 MTD partitions on " | ||
+ | [ 5.078559] 0x000000000000-0x000000100000 : " | ||
+ | [ 5.084753] 0x000000100000-0x000000600000 : " | ||
+ | [ 5.090451] 0x000000600000-0x000000620000 : " | ||
+ | [ 5.096678] 0x000000620000-0x000000c00000 : " | ||
+ | [ 5.104544] macb ff0e0000.ethernet: | ||
+ | [ 5.111908] libphy: MACB_mii_bus: | ||
+ | [ 5.115903] mdio_bus ff0e0000.ethernet-ffffffff: | ||
+ | [ 5.126076] TI DP83867 ff0e0000.ethernet-ffffffff: | ||
+ | [ 5.139117] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 22 (00: | ||
+ | [ 5.149227] xilinx-axipmon ffa00000.perf-monitor: | ||
+ | [ 5.155754] xilinx-axipmon fd0b0000.perf-monitor: | ||
+ | [ 5.162237] xilinx-axipmon fd490000.perf-monitor: | ||
+ | [ 5.168720] xilinx-axipmon ffa10000.perf-monitor: | ||
+ | [ 5.176674] dwc3 fe200000.dwc3: | ||
+ | [ 5.182527] xilinx-psgtr fd400000.zynqmp_phy: | ||
+ | [ 5.190909] xhci-hcd xhci-hcd.0.auto: | ||
+ | [ 5.196407] xhci-hcd xhci-hcd.0.auto: | ||
+ | [ 5.204406] xhci-hcd xhci-hcd.0.auto: | ||
+ | [ 5.213817] xhci-hcd xhci-hcd.0.auto: | ||
+ | [ 5.219940] usb usb1: New USB device found, idVendor=1d6b, | ||
+ | [ 5.228203] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 | ||
+ | [ 5.235422] usb usb1: Product: xHCI Host Controller | ||
+ | [ 5.240290] usb usb1: Manufacturer: | ||
+ | [ 5.246462] usb usb1: SerialNumber: | ||
+ | [ 5.251612] hub 1-0:1.0: USB hub found | ||
+ | [ 5.255375] hub 1-0:1.0: 1 port detected | ||
+ | [ 5.259480] xhci-hcd xhci-hcd.0.auto: | ||
+ | [ 5.264973] xhci-hcd xhci-hcd.0.auto: | ||
+ | [ 5.272626] xhci-hcd xhci-hcd.0.auto: | ||
+ | [ 5.279352] usb usb2: New USB device found, idVendor=1d6b, | ||
+ | [ 5.287614] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 | ||
+ | [ 5.294833] usb usb2: Product: xHCI Host Controller | ||
+ | [ 5.299702] usb usb2: Manufacturer: | ||
+ | [ 5.300811] ata1: SATA link down (SStatus 0 SControl 330) | ||
+ | [ 5.305874] usb usb2: SerialNumber: | ||
+ | [ 5.306113] hub 2-0:1.0: USB hub found | ||
+ | [ 5.311293] ata2: SATA link down (SStatus 0 SControl 330) | ||
+ | [ 5.316171] hub 2-0:1.0: 1 port detected | ||
+ | [ 5.330409] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator | ||
+ | [ 5.337665] pca953x 0-0020: Linked as a consumer to regulator.0 | ||
+ | [ 5.344455] GPIO line 496 (sel0) hogged as output/low | ||
+ | [ 5.349834] GPIO line 497 (sel1) hogged as output/high | ||
+ | [ 5.355300] GPIO line 498 (sel2) hogged as output/high | ||
+ | [ 5.360765] GPIO line 499 (sel3) hogged as output/high | ||
+ | [ 5.366112] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator | ||
+ | [ 5.373354] pca953x 0-0021: Linked as a consumer to regulator.0 | ||
+ | [ 5.380763] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.387580] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.394384] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.401192] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.408001] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.414808] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.421623] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.428431] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.435240] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.442056] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.448469] i2c i2c-0: Added multiplexed i2c bus 3 | ||
+ | [ 5.453935] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm) | ||
+ | [ 5.460744] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.467547] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.474367] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.481181] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.487994] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.494816] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.501622] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm) | ||
+ | [ 5.508017] i2c i2c-0: Added multiplexed i2c bus 4 | ||
+ | [ 5.516615] random: fast init done | ||
+ | [ 5.550092] i2c i2c-0: Added multiplexed i2c bus 5 | ||
+ | [ 5.555052] i2c i2c-0: Added multiplexed i2c bus 6 | ||
+ | [ 5.559839] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544 | ||
+ | [ 5.567190] cdns-i2c ff020000.i2c: | ||
+ | [ 5.574995] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write | ||
+ | [ 5.581742] i2c i2c-1: Added multiplexed i2c bus 7 | ||
+ | [ 5.586868] i2c i2c-1: Added multiplexed i2c bus 8 | ||
+ | [ 5.593772] si570 9-005d: registered, current frequency 300000000 Hz | ||
+ | [ 5.600174] i2c i2c-1: Added multiplexed i2c bus 9 | ||
+ | [ 5.619008] si570 10-005d: registered, current frequency 148500000 Hz | ||
+ | [ 5.625495] i2c i2c-1: Added multiplexed i2c bus 10 | ||
+ | [ 5.630593] si5324 11-0069: si5328 probed | ||
+ | [ 5.694709] si5324 11-0069: si5328 probe successful | ||
+ | [ 5.699631] i2c i2c-1: Added multiplexed i2c bus 11 | ||
+ | [ 5.704679] i2c i2c-1: Added multiplexed i2c bus 12 | ||
+ | [ 5.709716] i2c i2c-1: Added multiplexed i2c bus 13 | ||
+ | [ 5.714769] i2c i2c-1: Added multiplexed i2c bus 14 | ||
+ | [ 5.719646] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548 | ||
+ | [ 5.727932] at24 15-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write | ||
+ | [ 5.734677] i2c i2c-1: Added multiplexed i2c bus 15 | ||
+ | [ 5.739725] i2c i2c-1: Added multiplexed i2c bus 16 | ||
+ | [ 5.744770] i2c i2c-1: Added multiplexed i2c bus 17 | ||
+ | [ 5.749819] i2c i2c-1: Added multiplexed i2c bus 18 | ||
+ | [ 5.754868] i2c i2c-1: Added multiplexed i2c bus 19 | ||
+ | [ 5.759911] i2c i2c-1: Added multiplexed i2c bus 20 | ||
+ | [ 5.764953] i2c i2c-1: Added multiplexed i2c bus 21 | ||
+ | [ 5.770001] i2c i2c-1: Added multiplexed i2c bus 22 | ||
+ | [ 5.774882] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548 | ||
+ | [ 5.782491] cdns-i2c ff030000.i2c: | ||
+ | [ 5.788864] cdns-wdt fd4d0000.watchdog: | ||
+ | [ 5.828893] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit | ||
+ | [ 5.845173] axi_adxcvr 84a60000.axi-adxcvr-rx: | ||
+ | [ 5.857108] axi_adxcvr 84b60000.axi-adxcvr-tx: | ||
+ | [ 5.951002] mmc0: new ultra high speed SDR104 SDHC card at address aaaa | ||
+ | [ 5.958116] mmcblk0: mmc0:aaaa SC32G 29.7 GiB | ||
+ | [ 5.966523] | ||
+ | [ 6.038634] [drm] Cannot find any crtc or sizes | ||
+ | [ 6.682135] ad9081 spi1.0: AD9081 Rev. 3 Grade 10 (API 1.0.6) probed | ||
+ | [ 6.710789] cf_axi_adc 84a10000.axi-ad9081-rx-hpc: | ||
+ | [ 6.743436] cf_axi_dds 84b10000.axi-ad9081-tx-hpc: | ||
+ | [ 6.757628] jesd204: / | ||
+ | [ 6.768231] jesd204: / | ||
+ | [ 6.778837] jesd204: / | ||
+ | [ 6.788830] jesd204: / | ||
+ | [ 6.798825] jesd204: / | ||
+ | [ 6.809255] jesd204: / | ||
+ | [ 6.819686] jesd204: / | ||
+ | [ 6.830549] jesd204: / | ||
+ | [ 6.841421] jesd204: / | ||
+ | [ 6.852547] jesd204: / | ||
+ | [ 6.863766] hmc7044 spi2.0: hmc7044_jesd204_link_pre_setup: | ||
+ | [ 6.872686] hmc7044 spi2.0: hmc7044_jesd204_link_pre_setup: | ||
+ | [ 6.881514] jesd204: / | ||
+ | [ 6.893071] jesd204: / | ||
+ | [ 6.904644] jesd204: / | ||
+ | [ 6.916290] jesd204: / | ||
+ | [ 6.927935] jesd204: / | ||
+ | [ 6.939669] jesd204: / | ||
+ | [ 6.951401] jesd204: / | ||
+ | [ 6.963132] jesd204: / | ||
+ | [ 6.975886] jesd204: / | ||
+ | [ 6.987180] jesd204: / | ||
+ | [ 7.003833] jesd204: / | ||
+ | [ 7.015222] jesd204: / | ||
+ | [ 7.031631] jesd204: / | ||
+ | [ 7.043540] jesd204: / | ||
+ | [ 7.055540] jesd204: / | ||
+ | [ 7.067445] jesd204: / | ||
+ | [ 7.079358] jesd204: / | ||
+ | [ 7.091263] jesd204: / | ||
+ | [ 7.103170] jesd204: / | ||
+ | [ 7.115075] jesd204: / | ||
+ | [ 7.128071] jesd204: / | ||
+ | [ 7.139722] jesd204: / | ||
+ | [ 7.151421] jesd204: / | ||
+ | [ 7.162632] jesd204: / | ||
+ | [ 7.174069] ad9081 spi1.0: JESD RX (JTX) Link2 in DATA, SYNC deasserted, PLL locked, PHASE established, | ||
+ | [ 7.184652] ad9081 spi1.0: JESD TX (JRX) Link0 0xF lanes in DATA | ||
+ | [ 7.190662] jesd204: / | ||
+ | [ 7.201788] jesd204: / | ||
+ | [ 7.212914] jesd204: / | ||
+ | [ 7.224992] jesd204: / | ||
+ | [ 7.239566] input: gpio-keys as / | ||
+ | [ 7.246550] rtc_zynqmp ffa60000.rtc: | ||
+ | [ 7.255424] of_cfs_init | ||
+ | [ 7.257871] of_cfs_init: | ||
+ | [ 7.260796] cfg80211: Loading compiled-in X.509 certificates for regulatory database | ||
+ | [ 7.399733] cfg80211: Loaded X.509 cert ' | ||
+ | [ 7.406260] clk: Not disabling unused clocks | ||
+ | [ 7.410526] ALSA device list: | ||
+ | [ 7.413484] | ||
+ | [ 7.417510] platform regulatory.0: | ||
+ | [ 7.426120] cfg80211: failed to load regulatory.db | ||
+ | [ 7.440104] EXT4-fs (mmcblk0p2): | ||
+ | [ 7.448203] VFS: Mounted root (ext4 filesystem) on device 179:2. | ||
+ | [ 7.459066] devtmpfs: mounted | ||
+ | [ 7.462199] Freeing unused kernel memory: 832K | ||
+ | [ 7.482646] Run /sbin/init as init process | ||
+ | [ 7.712777] systemd[1]: System time before build time, advancing clock. | ||
+ | [ 7.734730] systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +S | ||
+ | ECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid) | ||
+ | [ 7.756467] systemd[1]: Detected architecture arm64. | ||
+ | |||
+ | Welcome to Kuiper GNU/Linux 10 (buster)! | ||
+ | |||
+ | [ 7.781175] systemd[1]: Set hostname to < | ||
+ | [ 7.925008] systemd[1]: File / | ||
+ | group based firewalling. | ||
+ | [ 7.942166] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.) | ||
+ | [ 8.063665] systemd[1]: / | ||
+ | [ 8.073365] systemd[1]: / | ||
+ | [ 8.225124] random: systemd: uninitialized urandom read (16 bytes read) | ||
+ | [ 8.237991] random: systemd: uninitialized urandom read (16 bytes read) | ||
+ | [ 8.245182] systemd[1]: Created slice system-systemd\x2dfsck.slice. | ||
+ | [ OK ] Created slice system-systemd\x2dfsck.slice. | ||
+ | [ 8.266718] random: systemd: uninitialized urandom read (16 bytes read) | ||
+ | [ 8.273358] systemd[1]: Reached target Swap. | ||
+ | [ OK ] Reached target Swap. | ||
+ | [ 8.286958] systemd[1]: Listening on udev Kernel Socket. | ||
+ | [ OK ] Listening on udev Kernel Socket. | ||
+ | [ OK ] Listening on udev Control Socket. | ||
+ | [ OK ] Created slice system-serial\x2dgetty.slice. | ||
+ | [ OK ] Started Forward Password R�…uests to Wall Directory Watch. | ||
+ | [ OK ] Created slice system-getty.slice. | ||
+ | [ OK ] Listening on initctl Compatibility Named Pipe. | ||
+ | [ OK ] Listening on Syslog Socket. | ||
+ | [ OK ] Listening on fsck to fsckd communication Socket. | ||
+ | [ OK ] Listening on Journal Audit Socket. | ||
+ | [ OK ] Created slice User and Session Slice. | ||
+ | [ OK ] Reached target Slices. | ||
+ | [ OK ] Listening on Journal Socket (/dev/log). | ||
+ | [ OK ] Listening on Journal Socket. | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | [ OK ] Mounted Kernel Debug File System. | ||
+ | [ OK ] Started Restore / save the current clock. | ||
+ | [ OK ] Mounted POSIX Message Queue File System. | ||
+ | [ OK ] Mounted RPC Pipe File System. | ||
+ | [ OK ] Mounted Huge Pages File System. | ||
+ | [FAILED] Failed to start Load Kernel Modules. | ||
+ | See ' | ||
+ | | ||
+ | | ||
+ | | ||
+ | [ OK ] Started Journal Service. | ||
+ | [ OK ] Started Apply Kernel Variables. | ||
+ | [ OK ] Mounted Kernel Configuration File System. | ||
+ | [ OK ] Started Set the console keyboard layout. | ||
+ | [ OK ] Started Remount Root and Kernel File Systems. | ||
+ | | ||
+ | | ||
+ | | ||
+ | [ OK ] Started Create System Users. | ||
+ | [ OK ] Started Flush Journal to Persistent Storage. | ||
+ | [ OK ] Started udev Coldplug all Devices. | ||
+ | [ OK ] Started Load/Save Random Seed. | ||
+ | | ||
+ | | ||
+ | [ OK ] Started Helper to synchronize boot up for ifupdown. | ||
+ | [ OK ] Started Create Static Device Nodes in /dev. | ||
+ | [ OK ] Reached target Local File Systems (Pre). | ||
+ | | ||
+ | [ OK ] Started udev Kernel Device Manager. | ||
+ | | ||
+ | [ OK ] Started Show Plymouth Boot Screen. | ||
+ | [ OK ] Reached target Local Encrypted Volumes. | ||
+ | [ OK ] Started Forward Password R�…s to Plymouth Directory Watch. | ||
+ | [ OK ] Found device / | ||
+ | | ||
+ | [FAILED] Failed to start Load Kernel Modules. | ||
+ | See ' | ||
+ | [ OK ] Found device / | ||
+ | | ||
+ | [ OK ] Started File System Check Daemon to report status. | ||
+ | [ OK ] Found device /dev/ttyS0. | ||
+ | [ OK ] Listening on Load/Save RF �…itch Status /dev/rfkill Watch. | ||
+ | [ OK ] Started File System Check �…/ | ||
+ | | ||
+ | [ OK ] Mounted /boot. | ||
+ | [ OK ] Reached target Local File Systems. | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | [ OK ] Started Set console font and keymap. | ||
+ | [ OK ] Started Preprocess NFS configuration. | ||
+ | [ OK ] Started Tell Plymouth To Write Out Runtime Data. | ||
+ | [ OK ] Reached target NFS client services. | ||
+ | [ OK ] Reached target Remote File Systems (Pre). | ||
+ | [ OK ] Reached target Remote File Systems. | ||
+ | [ OK ] Started Create Volatile Files and Directories. | ||
+ | | ||
+ | | ||
+ | [ OK ] Started Update UTMP about System Boot/ | ||
+ | | ||
+ | | ||
+ | [ OK ] Started Tell Plymouth To Write Out Runtime Data. | ||
+ | [FAILED] Failed to start Load Kernel Modules. | ||
+ | See ' | ||
+ | [ OK ] Started Raise network interfaces. | ||
+ | [ OK ] Started Network Time Synchronization. | ||
+ | [ OK ] Reached target System Initialization. | ||
+ | [ OK ] Listening on triggerhappy.socket. | ||
+ | [ OK ] Started Daily Cleanup of Temporary Directories. | ||
+ | [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. | ||
+ | [ OK ] Listening on GPS (Global P�…ioning System) Daemon Sockets. | ||
+ | [ OK ] Listening on D-Bus System Message Bus Socket. | ||
+ | [ OK ] Started CUPS Scheduler. | ||
+ | [ OK ] Reached target Paths. | ||
+ | [ OK ] Listening on CUPS Scheduler. | ||
+ | [ OK ] Reached target Sockets. | ||
+ | [ OK ] Reached target Basic System. | ||
+ | [ OK ] Started D-Bus System Message Bus. | ||
+ | | ||
+ | [ OK ] Started Manage Sound Card State (restore and store). | ||
+ | | ||
+ | | ||
+ | | ||
+ | [ OK ] Started CUPS Scheduler. | ||
+ | | ||
+ | | ||
+ | [ OK ] Started Regular background program processing daemon. | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | [ OK ] Started tof-server.service. | ||
+ | | ||
+ | [ OK ] Reached target System Time Synchronized. | ||
+ | [ OK ] Started Daily apt download activities. | ||
+ | [ OK ] Started Daily apt upgrade and clean activities. | ||
+ | [ OK ] Started Daily rotation of log files. | ||
+ | [ OK ] Started Daily man-db regeneration. | ||
+ | [ OK ] Reached target Timers. | ||
+ | [ OK ] Started triggerhappy global hotkey daemon. | ||
+ | [FAILED] Failed to start rng-tools.service. | ||
+ | See ' | ||
+ | [ OK ] Started Save/ | ||
+ | [ OK ] Reached target Sound Card. | ||
+ | [ OK ] Started Login Service. | ||
+ | [ OK ] Started System Logging Service. | ||
+ | [ OK ] Started dhcpcd on all interfaces. | ||
+ | [FAILED] Failed to start Check for Raspberry Pi EEPROM updates. | ||
+ | See ' | ||
+ | [ OK ] Started Avahi mDNS/DNS-SD Stack. | ||
+ | [ OK ] Started WPA supplicant. | ||
+ | [ OK ] Started dphys-swapfile - s�…mount, | ||
+ | | ||
+ | [ OK ] Started Make remote CUPS printers available locally. | ||
+ | [ OK ] Reached target Network. | ||
+ | | ||
+ | [ OK ] Started IIO Daemon. | ||
+ | | ||
+ | | ||
+ | | ||
+ | [ OK ] Started / | ||
+ | [ OK ] Started Permit User Sessions. | ||
+ | | ||
+ | | ||
+ | [ OK ] Started HTTP based time synchronization tool. | ||
+ | [ OK ] Started OpenBSD Secure Shell server. | ||
+ | [ OK ] Started Authorization Manager. | ||
+ | |||
+ | Raspbian GNU/Linux 10 analog ttyPS0 | ||
+ | |||
+ | analog login: root (automatic login) | ||
+ | |||
+ | Last login: Wed Feb 24 01:09:27 GMT 2021 on ttyPS0 | ||
+ | Linux analog 4.19.0-ga6ef26d #1105 SMP Fri Feb 19 16:51:27 GMT 2021 aarch64 | ||
+ | |||
+ | The programs included with the Debian GNU/Linux system are free software; | ||
+ | the exact distribution terms for each program are described in the | ||
+ | individual files in / | ||
+ | |||
+ | Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent | ||
+ | permitted by applicable law. | ||
+ | root@analog: | ||
+ | |||
+ | </ | ||
+ | </ | ||
+ | |||
+ | Login Information | ||
+ | * user: analog | ||
+ | * password: analog | ||
+ | |||
+ | |||
+ | The following devices should be present: | ||
+ | <WRAP box bggreen>< | ||
+ | < | ||
+ | root@analog: | ||
+ | iio: | ||
+ | iio: | ||
+ | iio: | ||
+ | iio: | ||
+ | |||
+ | </ | ||
+ | |||
+ | ===== IIO Oscilloscope Remote | ||
+ | |||
+ | ===== IIO Oscilloscope Remote | ||
+ | |||
+ | Please see also here: | ||
+ | |||
+ | The IIO Oscilloscope application can be used locally on FPGA platforms featuring a graphical desktop environment such as ZCU102 or ZC706 or remote using a network connection. | ||
+ | |||
+ | When using the remote option, once you logged in to the Linux terminal you need to check the IP address of the using the ifconfig command to see if there was any address assigned by a DHCP server. | ||
+ | If not, you need to manually set an address with ifconfig in the same address space your PC is using. | ||
+ | |||
+ | Once the IIO Osc application is launched goto Settings -> Connect and enter the IP address of the target in the popup window. | ||
+ | {{ : | ||
+ | |||
+ | {{page>: | ||
+ | {{page>: | ||
+ | |||
+ | ===== Shut down ===== | ||
+ | <WRAP important round> | ||
+ | {{: | ||
+ | </ | ||
+ | |||
+ | ====== ====== | ||
+ | |||
+ | {{page>: | ||
+ | {{page>: |