This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad9081_fmca_ebz:quickstart:zynq [19 Mar 2021 16:38] – [IIO Oscilloscope Remote] Michael Hennerich | resources:eval:user-guides:ad9081_fmca_ebz:quickstart:zynq [06 Nov 2023 11:33] (current) – Add the hardware change needed iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD9081 Zynq-7000 SoC ZC706 Quick Start Guide ====== | ====== AD9081 Zynq-7000 SoC ZC706 Quick Start Guide ====== | ||
- | {{ : | + | |
+ | {{ : | ||
This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the [[adi> | This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the [[adi> | ||
Line 13: | Line 14: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * SD Card 16GB imaged using the instructions here: [[resources: | + | * SD Card 16GB imaged using the instructions here: [[:resources: |
- | * Copy next boot files from '' | + | * Starting with our 2020_R1 |
+ | * Alternatively if you already have a SD-Card - download the files below. | ||
+ | * [[http:// | ||
+ | * Copy next boot files from '' | ||
* '' | * '' | ||
* '' | * '' | ||
Line 30: | Line 34: | ||
* Optionally USB keyboard, mouse and a HDMI compatible monitor | * Optionally USB keyboard, mouse and a HDMI compatible monitor | ||
+ | {{page>: | ||
+ | |||
+ | ===== Example Device Trees ===== | ||
+ | |||
+ | ^ Function ^ File ^ | ||
+ | | dtsi | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
+ | | dts | [[linux.github> | ||
====== Testing ====== | ====== Testing ====== | ||
Line 39: | Line 53: | ||
* Connect USB UART (Mini USB) to your host PC. | * Connect USB UART (Mini USB) to your host PC. | ||
* Insert SD card into socket. | * Insert SD card into socket. | ||
- | * Configure ZC706 for SD BOOT (Set the jumpers: The main one is: SW11 - Big Blue Switch in the middle, which controls the Boot Mode, it needs to be set: 1: Down, 2: Down, 3: Up, 4: Up, 5: Down. Other Jumpers can be checked via looking at the picture. (click the picture to make it bigger)). | + | * Configure ZC706 for SD BOOT (Set the jumpers: The main one is: SW11 - Big Blue Switch in the middle, which controls the Boot Mode, it needs to be set: 1: Down, 2: Down, 3: Up, 4: Up, 5: Down. |
* Turn on the power switch on the FPGA board. | * Turn on the power switch on the FPGA board. | ||
* Observe kernel and serial console messages on your terminal. | * Observe kernel and serial console messages on your terminal. | ||
Line 554: | Line 568: | ||
</ | </ | ||
</ | </ | ||
+ | |||
+ | Login Information | ||
+ | * user: analog | ||
+ | * password: analog | ||
These devices should be present: | These devices should be present: | ||
Line 566: | Line 584: | ||
iio: | iio: | ||
</ | </ | ||
+ | |||
+ | All links should be in '' | ||
<WRAP box bggreen>< | <WRAP box bggreen>< | ||
< | < | ||
- | root@analog: | + | root@analog: |
(DEVICES) Found 2 JESD204 Link Layer peripherals | (DEVICES) Found 2 JESD204 Link Layer peripherals | ||
Line 599: | Line 619: | ||
</ | </ | ||
- | For more on device modes, check [[resources: | + | More info on [[:resources: |
- | + | ||
===== Pyadi-iio Example ===== | ===== Pyadi-iio Example ===== | ||
- | Pyadi-iio is a python abstraction module for ADI hardware with IIO drivers to make them easier to use. For more check [[https:// | + | Pyadi-iio is a python abstraction module for ADI hardware with IIO drivers to make them easier to use. For more check [[https:// |
===== IIO Oscilloscope Remote | ===== IIO Oscilloscope Remote | ||
Line 620: | Line 638: | ||
{{page>: | {{page>: | ||
{{page>: | {{page>: | ||
+ | |||
+ | ===== Shut down ===== | ||
<WRAP important round> | <WRAP important round> |