Wiki

This version (07 Jul 2022 08:45) was approved by Michael Hennerich.The Previously approved version (22 Nov 2021 14:47) is available.Diff

AD9081/AD9082 Virtex UltraScale+ VCU118 Quick Start Guide

This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the AD9081-FMCA-EBZ or AD9082-FMCA-EBZ on the VCU118 platform.

Prerequisites

Required Hardware

Required Software

  • A Linux OS on a PC
  • Xilinx Vivado 2019.1 or later
  • UART terminal (e.g TeraTerm)
  • IIO-Oscilloscope Download

Downloads (Pre-build Images for VCU118)

Example Device Trees

Board setup

The following rework is required:
  • In order to avoid using an external clock source and fully rely on the HMC7044 clock chip, rotate the C6D/C4D caps in C5D/C3D position (Please note: In the latest version of the board, this is now the default configuration, so this configuration step might not be needed anymore)
  • If LEDS V1P0_LED and VINT_LED are not on please depopulate R22M and populate R2M

Steps

1. Build the HDL project

Before building the hdl project setup your computer based on the following guide: Building HDL projects

git clone https://github.com/analogdevicesinc/hdl.git
git checkout hdl_2019_r2;  // or latest release
cd hdl/projects/ad9081_fmca_ebz/vcu118
make

2. Build the Linux files

Instructions on how to build the MicroBlaze Linux kernel and devicetrees from source can be found here:

make simpleImage.vcu118_ad9081_m8_l4
Latest released files can be downloaded from here

3. Program the board

First we need to prepare a working directory where we will gather all the required binary files.
From the HDL build directory locate the system_top.bit and copy it to the working directory. From the Linux build directory locate the simpleImage and copy it to the working directory.

mkdir <working_dir>
cp <hdl_repo_dir>/projects/ad9081_fmca_ebz_vcu118.runs/impl_1/system_top.bit  <working_dir>
cp <linux_repo_dir>/arch/microblaze/boot/simpleImage.vcu118_ad9081_m8_l4.strip  <working_dir>

Next step is to program the board with xsct or similar tool. See generic instructions for programming the MicroBlaze bases systems here Boot Kernel on FPGA Microblaze

xsct% connect
xsct% fpga -f system_top.bit
xsct% after 1000
xsct% target 3
xsct% dow simpleImage.vcu118_ad9081_m8_l4.strip
xsct% after 1000
xsct% con
xsct% disconnect
When using the downloaded archives, simply open xsdb and source run.tcl

Complete Xilinx xsdb command log (Click to expand)

Complete Xilinx xsdb command log (Click to expand)

This specifies any shell prompt running on the target

michael@mhenneri-D06:~/vcu118_ad9081_m8_l4$ xsdb
                                                                                                                                                                                                           
****** Xilinx System Debugger (XSDB) v2019.1
  **** Build date : May 24 2019-15:06:52
    ** Copyright 1986-2018 Xilinx, Inc. All Rights Reserved.

xsdb% source run.tcl                                                                                                                                                                                       
attempting to launch hw_server                                                                                                                                                                             
                                                                                                                                                                                                           
****** Xilinx hw_server v2019.1
  **** Build date : May 24 2019 at 15:06:40
    ** Copyright 1986-2019 Xilinx, Inc. All Rights Reserved.

INFO: hw_server application started
INFO: Use Ctrl-C to exit hw_server application

INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121

100%   30MB   1.7MB/s  00:17                                                                                                                                                                               
Downloading Program -- /home/michael/devel/pshare/AD9081/AD9081_FMCA_EBZ/vcu118_ad9081_m8_l4/simpleImage.vcu118_ad9081_m8_l4.strip                                                                         
	section, .text: 0x80000000 - 0x80510477
	section, __fdt_blob: 0x80510478 - 0x80520477
	section, .rodata: 0x80521000 - 0x809f63a7
	section, .pci_fixup: 0x809f63a8 - 0x809f8067
	section, .builtin_fw: 0x809f8068 - 0x809f808b
	section, __ksymtab: 0x809f808c - 0x80a02117
	section, __ksymtab_gpl: 0x80a02118 - 0x80a0a88f
	section, __ksymtab_strings: 0x80a0a890 - 0x80a27cfc
	section, __param: 0x80a27d00 - 0x80a282db
	section, __modver: 0x80a282dc - 0x80a28fff
	section, __ex_table: 0x80a29000 - 0x80a2a4ef
	section, .notes: 0x80a2a4f0 - 0x80a2a52b
	section, .sdata2: 0x80a2a52c - 0x80a2afff
	section, .data: 0x80a2b000 - 0x80ab879f
	section, .data..percpu: 0x80ab9000 - 0x80ab8fff
	section, .init.text: 0x80ab9000 - 0x80adf0f3
	section, .init.data: 0x80adf0f4 - 0x80ae1d93
	section, .init.ivt: 0x80ae1d94 - 0x80ae1dbb
	section, .init.setup: 0x80ae1dbc - 0x80ae219f
	section, .initcall.init: 0x80ae21a0 - 0x80ae263b
	section, .con_initcall.init: 0x80ae263c - 0x80ae263f
	section, .bss: 0x80ae3000 - 0x80b0992f
	section, .init.ramfs: 0x81000000 - 0x814bd74b
100%   15MB   0.2MB/s  01:22                                                                                                                                                                               
Setting PC to Program Start Address 0x80000000
Successfully downloaded /home/michael/devel/pshare/AD9081/AD9081_FMCA_EBZ/vcu118_ad9081_m8_l4/simpleImage.vcu118_ad9081_m8_l4.strip
Info: MicroBlaze #0 (target 3) Running                                                                                                                                                                     
xsdb% Info: tcfchan#0 closed
xsdb%

Linux BOOT messages

Complete kernel boot log (Click to expand)

Complete kernel boot log (Click to expand)

This specifies any shell prompt running on the target

Ramdisk addr 0x00000000, 
Compiled-in FDT at 0x80510478
earlycon: uartlite_a0 at MMIO 0x40600000 (options '115200n8')
printk: bootconsole [uartlite_a0] enabled
cma: Reserved 512 MiB at 0x8e000000
Linux version 5.4.0-168125-g1d1209cdb0ce (michael@mhenneri-D06) (gcc version 7.3.1 20180425 (crosstool-NG 1.20.0)) #2837 Fri Mar 12 17:41:16 CET 2021
setup_memory: max_mapnr: 0x7ffff
setup_memory: min_low_pfn: 0x80000
setup_memory: max_low_pfn: 0xb0000
setup_memory: max_pfn: 0xfffff
Zone ranges:
  DMA      [mem 0x0000000080000000-0x00000000afffffff]
  Normal   empty
  HighMem  [mem 0x00000000b0000000-0x00000000ffffefff]
Movable zone start for each node
Early memory node ranges
  node   0: [mem 0x0000000080000000-0x00000000ffffefff]
Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffefff]
setup_cpuinfo: initialising cpu 0
setup_cpuinfo: Using full CPU PVR support
wt_msr_noirq
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0 
Built 1 zonelists, mobility grouping on.  Total pages: 522751
Kernel command line: earlycon
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
mem auto-init: stack:off, heap alloc:off, heap free:off
Memory: 1538692K/2097148K available (5185K kernel code, 565K rwdata, 5152K rodata, 165K init, 154K bss, 34168K reserved, 524288K cma-reserved, 1310716K highmem)
Kernel virtual memory layout:
  * 0xfffea000..0xfffff000  : fixmap
  * 0xff800000..0xffc00000  : highmem PTEs
  * 0xff7ff000..0xff800000  : early ioremap
  * 0xb0000000..0xff7ff000  : vmalloc & ioremap
NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
irq-xilinx: mismatch in kind-of-intr param
irq-xilinx: /amba_pl/interrupt-controller@41200000: num_irq=16, sw_irq=0, edge=0xffff05f0
xilinx_timer_init: Timer base: 0xb0002000, Clocksource base: 0xb0002010
clocksource: xilinx_clocksource: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns
sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns
/amba_pl/timer@41c00000: irq=1, cpu_id 0
xilinx_timer_shutdown
xilinx_timer_set_periodic
Calibrating delay loop... 49.35 BogoMIPS (lpj=246784)
pid_max: default: 4096 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
devtmpfs: initialized
random: get_random_u32 called from bucket_table_alloc.isra.24+0x13c/0x170 with crng_init=0
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 16 (order: -4, 448 bytes, linear)
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic allocations
PCI: Probing PCI hardware
vgaarb: loaded
jesd204: created con: id=0, topo=0, link=0, /amba_pl/axi_quad_spi@44a70000/hmc7044@1 <-> /amba_pl/axi-adxcvr-tx@44b60000
jesd204: created con: id=1, topo=0, link=2, /amba_pl/axi_quad_spi@44a70000/hmc7044@1 <-> /amba_pl/axi-adxcvr-rx@44a60000
jesd204: created con: id=2, topo=0, link=0, /amba_pl/axi-adxcvr-tx@44b60000 <-> /amba_pl/axi-jesd204-tx@44b90000
jesd204: created con: id=3, topo=0, link=2, /amba_pl/axi-adxcvr-rx@44a60000 <-> /amba_pl/axi-jesd204-rx@44a90000
jesd204: created con: id=4, topo=0, link=0, /amba_pl/axi-jesd204-tx@44b90000 <-> /amba_pl/axi-ad9081-tx-hpc@44b10000
jesd204: created con: id=5, topo=0, link=2, /amba_pl/axi-jesd204-rx@44a90000 <-> /amba_pl/axi-ad9081-rx-hpc@44a10000
jesd204: created con: id=6, topo=0, link=2, /amba_pl/axi-ad9081-rx-hpc@44a10000 <-> /amba_pl/axi_quad_spi@44a70000/ad9081@0
jesd204: created con: id=7, topo=0, link=0, /amba_pl/axi-ad9081-tx-hpc@44b10000 <-> /amba_pl/axi_quad_spi@44a70000/ad9081@0
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0: JESD204[2] transition uninitialized -> initialized
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0: JESD204[0] transition uninitialized -> initialized
jesd204: found 8 devices and 1 topologies
clocksource: Switched to clocksource xilinx_clocksource
NET: Registered protocol family 2
tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 12288 bytes, linear)
TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)
TCP bind hash table entries: 8192 (order: 5, 163840 bytes, linear)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 24576 bytes, linear)
UDP-Lite hash table entries: 512 (order: 2, 24576 bytes, linear)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PCI: CLS 0 bytes, default 32
random: fast init done
workingset: timestamp_bits=30 max_order=19 bucket_order=0
Key type cifs.idmap registered
jffs2: version 2.2. (NAND) (SUMMARY)  �© 2001-2006 Red Hat, Inc.
romfs: ROMFS MTD (C) 2007 Red Hat, Inc.
bounce: pool size: 64 pages
io scheduler mq-deadline registered
io scheduler kyber registered
Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
40600000.serial: ttyUL0 at MMIO 0x40600000 (irq = 5, base_baud = 0) is a uartlite
printk: console [ttyUL0] enabled
printk: console [ttyUL0] enabled
printk: bootconsole [uartlite_a0] disabled
printk: bootconsole [uartlite_a0] disabled
uartlite 41400000.serial: IRQ index 0 not found
brd: module loaded
Xilinx SystemACE device driver, major=254
libphy: Fixed MDIO Bus: probed
xilinx_axienet 40c00000.ethernet: TX_CSUM 2
xilinx_axienet 40c00000.ethernet: RX_CSUM 2
xilinx_axienet 40c00000.ethernet: Failed to get clock: -2
xilinx_axienet 40c00000.ethernet (unnamed net_device) (uninitialized): Setting assumed host clock to 100000000
libphy: Xilinx Axi Ethernet MDIO: probed
i2c /dev entries driver
i2c i2c-0: Added multiplexed i2c bus 1
i2c i2c-0: Added multiplexed i2c bus 2
i2c i2c-0: Added multiplexed i2c bus 3
at24 4-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
i2c i2c-0: Added multiplexed i2c bus 4
i2c i2c-0: Added multiplexed i2c bus 5
i2c i2c-0: Added multiplexed i2c bus 6
i2c i2c-0: Added multiplexed i2c bus 7
i2c i2c-0: Added multiplexed i2c bus 8
pca954x 0-0075: registered 8 multiplexed busses for I2C switch pca9548
i2c i2c-0: Added multiplexed i2c bus 9
i2c i2c-0: Added multiplexed i2c bus 10
i2c i2c-0: Added multiplexed i2c bus 11
i2c i2c-0: Added multiplexed i2c bus 12
i2c i2c-0: Added multiplexed i2c bus 13
i2c i2c-0: Added multiplexed i2c bus 14
i2c i2c-0: Added multiplexed i2c bus 15
i2c i2c-0: Added multiplexed i2c bus 16
pca954x 0-0074: registered 8 multiplexed busses for I2C switch pca9548
jesd204: /amba_pl/axi_quad_spi@44a70000/hmc7044@1,jesd204:0,parent=spi0.1: Using as SYSREF provider
axi_adxcvr 44a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using CPLL on GTY4 at 0x44A60000. Number of lanes: 4.
axi_adxcvr 44b60000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using QPLL on GTY4 at 0x44B60000. Number of lanes: 4.
axi-jesd204-rx 44a90000.axi-jesd204-rx: AXI-JESD204-RX (1.07.a) at 0x44A90000. Encoder 8b10b, width 4/4, lanes 4, jesd204-fsm.
axi-jesd204-tx 44b90000.axi-jesd204-tx: AXI-JESD204-TX (1.06.a) at 0x44B90000. Encoder 8b10b, width 4/4, lanes 4, jesd204-fsm.
axi_sysid 45000000.axi-sysid-0: AXI System ID core version (1.01.a) found
axi_sysid 45000000.axi-sysid-0: [ad9081_fmca_ebz] on [vcu118] git branch <(HEAD> git <e2a111d74bdcc055cc78409074346977a0f8452b> clean [2021-03-08 11:47:34] UTC
NET: Registered protocol family 17
Key type encrypted registered
ad9081 spi0.0: AD9081 Rev. 3 Grade 10 (API 1.1.0) probed
cf_axi_dds 44b10000.axi-ad9081-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x44B10000 mapped to 0x(ptrval), probed DDS AD9081
cf_axi_adc 44a10000.axi-ad9081-rx-hpc: ADI AIM (10.01.b) at 0x44A10000 mapped to 0x(ptrval), probed ADC AD9081 as MASTER
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition initialized -> probed
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition initialized -> probed
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition probed -> idle
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition probed -> idle
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition idle -> device_init
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition idle -> device_init
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition device_init -> link_init
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition device_init -> link_init
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition link_init -> link_supported
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition link_init -> link_supported
hmc7044 spi0.1: hmc7044_jesd204_link_pre_setup: Link2 forcing continuous SYSREF mode
hmc7044 spi0.1: hmc7044_jesd204_link_pre_setup: Link0 forcing continuous SYSREF mode
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition link_supported -> link_pre_setup
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition link_supported -> link_pre_setup
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition link_pre_setup -> clk_sync_stage1
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition link_pre_setup -> clk_sync_stage1
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition clk_sync_stage1 -> clk_sync_stage2
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage3
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition clk_sync_stage3 -> link_setup
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition clk_sync_stage3 -> link_setup
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition link_setup -> opt_setup_stage1
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition link_setup -> opt_setup_stage1
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition opt_setup_stage1 -> opt_setup_stage2
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition opt_setup_stage1 -> opt_setup_stage2
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition opt_setup_stage2 -> opt_setup_stage3
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition opt_setup_stage2 -> opt_setup_stage3
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition opt_setup_stage3 -> opt_setup_stage4
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition opt_setup_stage3 -> opt_setup_stage4
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition opt_setup_stage4 -> opt_setup_stage5
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition opt_setup_stage4 -> opt_setup_stage5
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition opt_setup_stage5 -> clocks_enable
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition opt_setup_stage5 -> clocks_enable
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition clocks_enable -> link_enable
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition clocks_enable -> link_enable
ad9081 spi0.0: JESD RX (JTX) Link2 in DATA, SYNC deasserted, PLL locked, PHASE established, MODE valid
ad9081 spi0.0: JESD TX (JRX) Link0 0xF lanes in DATA
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition link_enable -> link_running
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition link_enable -> link_running
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[2] transition link_running -> opt_post_running_stage
jesd204: /amba_pl/axi_quad_spi@44a70000/ad9081@0,jesd204:1,parent=spi0.0: JESD204[0] transition link_running -> opt_post_running_stage
Freeing unused kernel memory: 164K
This architecture does not have kernel memory protection.
Run /init as init process
Starting syslogd: OK
Starting klogd: OK
Running sysctl: OK
Saving random seed: random: dd: uninitialized urandom read (512 bytes read)
OK
Starting network: udhcpc: started, v1.31.1
net eth0: Promiscuous mode disabled.
xilinx_axienet 40c00000.ethernet eth0: Setting assumed host clock to 100000000
net eth0: Promiscuous mode disabled.
net eth0: Speed other than 10, 100 
net eth0: or 1Gbps is not supported
xilinx_axienet 40c00000.ethernet eth0: Link is Down
udhcpc: sending discover
xilinx_axienet 40c00000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
udhcpc: sending discover
udhcpc: sending select for 10.44.3.51
udhcpc: lease of 10.44.3.51 obtained, lease time 43200
deleting routers
adding dns 10.32.51.110
adding dns 10.64.53.110
Starting dropbear sshd: random: dropbear: uninitialized urandom read (32 bytes read)
OK
Starting IIO Server Daemon

Welcome to Buildroot
buildroot login: root
Password: 
# 


Login Information

  • user: root
  • password: analog

The following devices should be present:

This specifies any shell prompt running on the target

# iio_info | grep iio:device
        iio:device0: hmc7044
        iio:device1: axi-ad9081-tx-hpc (buffer capable)
        iio:device2: axi-ad9081-rx-hpc (buffer capable)

All links should be in DATA without errors:

This specifies any shell prompt running on the target

# jesd_status -s
  (DEVICES) Found 2 JESD204 Link Layer peripherals

  (0): axi-jesd204-rx/44a90000.axi-jesd204-rx  [*]
  (1): axi-jesd204-tx/44b90000.axi-jesd204-tx

  (STATUS)
  Link is                      enabled
  Link Status                  DATA
  Measured Link Clock (MHz)    249.998
  Reported Link Clock (MHz)    250.000
  Measured Device Clock (MHz)  250.000
  Reported Device Clock (MHz)  250.000
  Desired Device Clock (MHz)   250.000
  Lane rate (MHz)              10000.000
  Lane rate / 40 (MHz)         250.000
  LMFC rate (MHz)              7.812
  SYSREF captured              Yes
  SYSREF alignment error       No
  SYNC~

  (LANE STATUS)
  Lane#                             0      1      2      3
  Errors                            0      0      0      0
  Latency (Multiframes/Octets)      1/22   1/20   1/25   1/21
  CGS State                         DATA   DATA   DATA   DATA        
  Initial Frame Sync                Yes    Yes    Yes    Yes                           
  Initial Lane Alignment Sequence   Yes    Yes    Yes    Yes

4. Connect to board with IIO Scope

From the UART console find out the board IP address that was allocated by the DHCP server. If you do not use a DHCP server manually assign an IP to the board Ethernet port.

5. Capture data with IIO Scope

IIO Oscilloscope Remote

Please see also here:Oscilloscope

The IIO Oscilloscope application can be used locally on FPGA platforms featuring a graphical desktop environment such as ZCU102 or ZC706, however for VCU118 we must use the remote network connection.

When using the remote option, once you logged in to the Linux terminal you need to check the IP address of the using the ifconfig command to see if there was any address assigned by a DHCP server. If not, you need to manually set an address with ifconfig in the same address space your PC is using.

Once the IIO Osc application is launched goto Settings → Connect and enter the IP address of the target in the popup window.

IIO OSC AD9081 Capture Window
Introduction

Main receivers are handled by the axi-ad9081-rx-hpc IIO device, The number of channels depend on the JESD mode (M) parameter and can vary from case to case. When using complex IQ, two channels index by _i and _q from a receiver.

Screenshots
Time Domain View

Frequency Domain View

AD9081 Plugin Description

The AD9081 plugin works with the IIO Oscilloscope. You always use the latest version if possible. Changing any field will immediately write changes which have been made to the AD9081 settings to the hardware, and then read it back to make sure the setting is valid. If you want to set something that the GUI changes to a different number, that either means that GUI is rounding (sorry), or the hardware (either the AD9081 or the FPGA fabric) does not support that mode/precision.

If you want to go play with /sys/bus/iio/devices/…. and manipulate the devices behind the back of the GUI, it's still possible to see the settings by clicking the Reload Settings button at the bottom of the GUI.

The AD9081 view is divided in three sections:

  • Receive Chain
  • Transmit Chain
  • FPGA Settings

Receive Chain

  • ADC Rate(MHz): Displays the ADC Sample Rate. Read More
  • ADC Nyquist Zone Control: Selects the Nyquist Zone. Read More
  • RX Main NCO Frequency Control: Controls the Main NCO. Frequency Read More
  • RX Main NCO Phase Control: Controls the Main NCO Phase. Read More
  • RX Channel NCO Frequency Control: Controls the Channel NCO Frequency. Read More
  • RX Channel NCO Phase Control: Controls the Channel NCO Phase. Read More

Transmit Chain

  • DAC Rate(MHz): Displays the DAC Sample Rate. Read More
  • TX Main NCO Frequency Control: Controls the Main NCO Frequency. Read More
  • TX Main NCO Phase Control: Controls the Main NCO Phase. Read More
  • TX Channel NCO Frequency Control: Controls the Channel. NCO Frequency Read More
  • TX Channel NCO Phase Control: Controls the Channel NCO Phase. Read More
  • TX NCO Channel Digital Gain: Controls the Channel NCO digital gain. Read More
  • TX NCO Test Tone Modes: Controls the Test Tone generation. Read More

FPGA Settings
Transmit/DDS

The plugin provides several options on how the transmitted data is generated.

It is possible to either use the built-in two tone Direct Digital Synthesizer (DDS) to transmit a bi-tonal signal on channels I and Q of the DAC. Or it is possible to use the Direct Memory Access (DMA) facility to transmit custom data that you have stored in a file.

This can be achieved by selecting one of the following options listed by the DDS Mode:

One CW Tone

In One CW Tone mode one continuous wave (CW) tone will be outputted. The plugin displays the controls to set the Frequency, Amplitude and Phase for just one tone and makes sure that the amplitude of the other tone is set to 0. The resulting signal will be outputted on the Channel I of the DAC and the exact same signal but with a difference in phase of 90 degrees will be outputted on the Channel Q of the DAC.

Two CW Tone

In Two CW Tone mode two continuous wave (CW) tones will be outputted. The plugin displays the controls to set the frequencies F1 and F2, amplitudes A1 and A2, phases P1 and P2 for the two tones. The resulting signal will be outputted on the Channel I of the DAC and the exact same signal but with a difference in phase of 90 degrees will be outputted on the Channel Q of the DAC.

Independent I/Q Control

In Independent I/Q Control the plugin displays the controls to set the frequencies, amplitudes and phases for the two tones that will be outputted on channel I and additionally it allows for the two tones that will be outputted on channel Q of the DAC to be configured independently.

Note: The bi-tonal signal (T) is defined as the sum of two tones:
T(t) = A1 * sin(2 * p * F1 * t + P1) + A2 * sin(2 * p * F2 * t + P2),
where A-amplitude, F-frequency, P-phase of a tone.

DAC Buffer Output

The file selector under the File Selection section is used to locate and choose the desired data file. Under the DAC Channels section the enabled channels will be used to transmit the data stored in the file. To finalize the process, a click on the Load button is required.

Restrictions:

  • There are two types of files than can be loaded: .txt or .mat. The IIO-Oscilloscope comes with several data files that can be used. If you want to create your own data files please take a look at the Basic IQ Data Files documentation first.
  • Due to hardware limitation only specific combinations of enabled channels are possible. You can enable a total of 1, 2, 4, etc. channels. If 1 channel is enabled then it can be any of them. If two channels are enabled then channels 0, 1 or channels 2, 3 can be enabled and so on.
Disable

In this mode both DDS and DMA are disabled causing the DAC channels to stop transmitting any data.

Upon pressing Reload Settings button the values will be reloaded with the corresponding driver values. Useful in scenarios where the diver values get changed outside this plugin and a refresh on plugin's values is needed.

Some plugin values will be rounded to the nearest value supported by the hardware.

Support

Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.

resources/eval/user-guides/ad9081_fmca_ebz/quickstart/microblaze.txt · Last modified: 07 Jul 2022 08:45 by Michael Hennerich