This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad9081_fmca_ebz:ad9081_fmca_ebz_hdl [28 Jul 2021 13:06] – [DAC - crossbar config] Laszlo Nagy | resources:eval:user-guides:ad9081_fmca_ebz:ad9081_fmca_ebz_hdl [25 Nov 2021 07:02] – [AD9081-FMCA-EBZ/AD9082-FMCA-EBZ (Single MxFE) HDL Reference Design] Laszlo Nagy | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD9081-FMCA-EBZ (Single MxFE) HDL Reference Design ====== | + | ====== AD9081-FMCA-EBZ / AD9082-FMCA-EBZ (Single MxFE) HDL Reference Design ====== |
===== Functional Overview ===== | ===== Functional Overview ===== | ||
- | The AD9081-FMCA-EBZ reference design is a processor based (e.g. Microblaze) embedded system. The design consists from a receive and a transmit chain. | + | The AD9081-FMCA-EBZ / AD9082-FMCA-EBZ reference design is a processor based (e.g. Microblaze) embedded system. The design consists from a receive and a transmit chain. |
The receive chain transports the captured samples from ADC to the system memory (DDR). Before transferring the data to DDR the samples are stored in a buffer implemented on block rams from the FPGA fabric (util_adc_fifo). | The receive chain transports the captured samples from ADC to the system memory (DDR). Before transferring the data to DDR the samples are stored in a buffer implemented on block rams from the FPGA fabric (util_adc_fifo). |